v5.10.72-2.2.3_images_IMX6QPDLSOLOX Desktop view

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

v5.10.72-2.2.3_images_IMX6QPDLSOLOX Desktop view

560件の閲覧回数
B_Prabhu
Contributor III

Hello,

I am using i.MX6DLSABRE_AI and flashed 5.10.72-2.2.3 BSP files, it is booting up there is no issue. My doubt is i can see only the terminal window in the HDMI monitor (see attachement), is that only option available in this BSP files? or something i have missed? how the windows look like in this version?

To enable frame buffer i have used below command in boot environment "setenv mmcargs 'setenv bootargs console=${console},${baudrate} root=/dev/mmcblk2p2 rootwait rw video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24'"

Could you please support me.

0 件の賞賛
返信
3 返答(返信)

519件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

did you use prebuit images? if yes, which image do you use?

0 件の賞賛
返信

513件の閲覧回数
B_Prabhu
Contributor III
0 件の賞賛
返信

475件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

this demo images are built wayland as backend, if you need other backend, you need build by yourself, more detailed information, pls refer to the ycoto user guide

0 件の賞賛
返信