Could you give me some advice on android 9.0 download imx8qxp mek?
I want to download images on imx8qxp mek using uuu tool, the error is Wait for Known USB Device Appear...
(1) SW2 set 0001 serial download mode.
(2) Connecting J39 to PC USB by a USB OTG cable.
(3) Connecting J10(usb type c) to PC USB by a USB 3.0 cable.
(4) Power on I.MX8qxp mek board via J9
E:\imx8qxp_android9\android_p9.0.0_2.0.0-ga_image_8qmek>uuu_imx_android_flash.bat -f imx8qxp -a -e
This script is validated with uuu 1.2.91 version, please align with this version.
dtbo is supported
dual slot is supported
generate lines to flash partition-table.img to the partition of gpt
generate lines to flash u-boot-imx8qxp.imx to the partition of bootloader0
generate lines to flash dtbo-imx8qxp.img to the partition of dtbo_a
generate lines to flash boot.img to the partition of boot_a
generate lines to flash system.img to the partition of system_a
generate lines to flash vendor.img to the partition of vendor_a
generate lines to flash vbmeta-imx8qxp.img to the partition of vbmeta_a
uuu script generated, start to invoke uuu with the generated uuu script
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.2.135-0-gacaf035
Your console don't support VT mode, fail back to verbose mode
Build in config:
Pctl Chip Vid Pid BcdVersion
==================================================
SDPS: MX8QXP 0x1fc9 0x012f [0x0002..0xffff]
SDPS: MX8QM 0x1fc9 0x0129 [0x0002..0xffff]
SDPS: MX28 0x15a2 0x004f
SDPS: MX815 0x1fc9 0x013e
SDP: MX7D 0x15a2 0x0076
SDP: MX6Q 0x15a2 0x0054
SDP: MX6D 0x15a2 0x0061
SDP: MX6SL 0x15a2 0x0063
SDP: MX6SX 0x15a2 0x0071
SDP: MX6UL 0x15a2 0x007d
SDP: MX6ULL 0x15a2 0x0080
SDP: MX6SLL 0x1fc9 0x0128
SDP: MX7ULP 0x1fc9 0x0126
SDP: MXRT106X 0x1fc9 0x0135
SDP: MX8MM 0x1fc9 0x0134
SDP: MX8MQ 0x1fc9 0x012b
SDPU: SPL 0x0525 0xb4a4 [0x0000..0x04ff]
SDPV: SPL1 0x0525 0xb4a4 [0x0500..0x9998]
SDPU: SPL 0x0525 0xb4a4 [0x9999..0x9999]
FBK: 0x066f 0x9afe
FBK: 0x066f 0x9bff
FB: 0x0525 0xa4a5
FB: 0x18d1 0x0d02
Wait for Known USB Device Appear...
i use win7 when detect the devices, i need to pull out then pull in the type C wire. linux don't need to do it. you can try it.
win7 enviroment , i can download images successfully. Thanks
my win10 doesn't work either, so I download under linux by "sudo ./uuu_imx_android_flash.sh -f imx8mq -a -e" successfully
imx8qxp mek have three usb interface:usb debug, usb type c and usb otg. i want to enter serial download mode. which interface i shoud connect? what devices can be see in "device manager" ?
use type C for downloading, you should find new devices under "Human Interface Device" of device manager
should i install the fastboot tool? after output the following log, it stop
1:6>Start Cmd:SDPS: boot -f u-boot-imx8qm-mek-uuu.imx.link
100%1:6>Okay
it should be USB compatibility issue, you can try to use another USB port or try to use usb hub to connect your board
refer to the settings in the board, for serial download mode, should be 1000, not 0001 pls double check it
Thanks for your reply, maybe just understood differently, should be from 4 to 1, is 0001
if you set the SW2 correctly, pls check if your "device manager" detect your board or not, it seems your PC doesn't detect your board
Thanks, Could you show "device manager " detect device successfully , we can see what device? I don't know wether my imx8qxp mek using ic type PIMX8QX6AVLFZAA , i can not detect device. i will chang ic to PIMX8QX6AVLFZAB