uuu can't burn the linux images into eMMC on the iMX8qxp-mek

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

uuu can't burn the linux images into eMMC on the iMX8qxp-mek

2,597件の閲覧回数
先生孟
Contributor II

Hi Team:

    I want to write the images including Image、dtb、rootfs、bootloader etc files into the eMMC on the iMX8QXP-MEK by uuu mfgtool, therefore I strictly execute following documents:

(1)uuu.pdf (how to operate the uuu tool)

(2)yocto Linux User Guide.pdf (how to boot the linux and use the uuu)

(3)One training document about uuu from FAE 

Excepting above documents, I execute following procedure:

(1)downloading the imx-imx8qxp-mek-images-L4.14.78_1.0.0_ga.zip from nxp website

(2)downloading the rececently uuu.exe from github

(3)connecting the PC and MEK usb type C with USB3 cable

(4)connecting the MEK debug miniUSB and PC with miniUSB cable

(5)Open the PC super-terminal 

(6)Get the flash.bin、fsl-imx8qxp-mek.dtb、uramdisk-rootfs.uboot、Image etc files by decompressing (1) procedure zip file

(7)Modified the uuu.lst script file according with mfgtool script example file

(8)Power on the IMX8QXP-MEK

(9)Execute the uuu program in the windows Command windows

  $uuu uuu.lst 

Then, all files including the flash.bin、dtb、uramdisk rootfs、Image etc are downloaded into the iMX8QXP-MEK ddr memeory, 

Wait for Known USB Device Appear
New USB Device Attached at 1:8
1:8>Start Cmd:SDPS: boot -f flash_mfg.bin
100%1:8>Okay
New USB Device Attached at 1:8
1:8>Start Cmd:FB: ucmd setenv fastboot_dev mmc
1:8>Okay
1:8>Start Cmd:FB: ucmd setenv mmcdev 0
1:8>Okay
1:8>Start Cmd:FB: ucmd mmc dev 0
1:8>Okay
1:8>Start Cmd:FB: ucmd setenv fastboot_buffer ${loadaddr}
1:8>Okay
1:8>Start Cmd:FB: download -f Image
1:8>Okay
1:8>Start Cmd:FB: ucmd setenv fastboot_buffer ${fdt_addr}
1:8>Okay
1:8>Start Cmd:FB: download -f fsl-imx8qxp-mek.dtb
1:8>Okay
1:8>Start Cmd:FB: ucmd setenv fastboot_buffer ${initrd_addr}
1:8>Okay
1:8>Start Cmd:FB: download -f fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.gz.u-boot
1:8>Okay
1:8>Start Cmd:FB: acmd ${kboot} ${loadaddr} ${initrd_addr} ${fdt_addr}
1:8>Okay

the PC supre-terminal shows following scripts:

4.996886: xhci-cdns3: USB bus 1 deregistered 

Sh-4.4# Can't support > 32 dma

.5.139795] hub 1-0:1`.0: usb hub found

5.143595] hub 1-0: 1:0: 1 port detected

5.147805] xhci-cdns3: xHCI host controller

5.152195] xhci-cdns3: new USB bus registered, assigned bus

...

then above scripts always be printed (I take the picture with the attached file)

But uuu can't download the files (include mksdcard.sh.tar、Image、flash.bin、rootfs.tar.bz2、dtb files) into  the eMMC 

by FBK command

I don't know what's the reason, all files come from the imx-imx8qxp-mek_L4.14.78_1.0.0_ga.zip,

Could you could give me the solution?

Thank you very much

Meng

2019-04-10

 

0 件の賞賛
返信
2 返答(返信)

1,770件の閲覧回数
inigovicentewal
Contributor III

Hi 先生孟

Did you get the board started?

Where did you get _flash.bin, _Image, _board.dtb, _rootfs.tar.bz2 ?

Is L4.14.98_2.0.0_ga_images_MX8MMEVK sufficient?

Thanks.

0 件の賞賛
返信

1,770件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

There is example_kernel_emmc.uuu in the demo image.

You can take this for reference.

0 件の賞賛
返信