Hello,
recently insatlled this ltib to buld linux for a sabrelite board. Build went ok after a few hicups. Now with everything built I wanted to prep some packages, like boot_stream, u_boot, and kernel to examine sources. This is something I was doing a few months ago with L2.6.35_1.1.0_130130 ltib. Here is what I see:
$ ./ltib -p boot_stream.spec -m prep
defined(@array) is deprecated at /home/csc/csc_projects/imx6_project1/ltib/bin/Ltibutils.pm line 362.
(Maybe you should just omit the defined()?)
Processing: boot_stream
=========================
Build path taken because: build key set, no prebuilt rpm,
Testing network connectivity
OK GPP:
Try imx-bootlets-src-3.0.35-4.1.0.tar.gz.md5 from the GPP
http://bitshrine.org/gpp/imx-bootlets-src-3.0.35-4.1.0.tar.gz.md5:
11:09:51 ERROR 404: Not Found.
Try imx-bootlets-src-3.0.35-4.1.0.tar.gz from the GPP
http://bitshrine.org/gpp/imx-bootlets-src-3.0.35-4.1.0.tar.gz:
11:09:51 ERROR 404: Not Found.
Can't get: imx-bootlets-src-3.0.35-4.1.0.tar.gz at ./ltib line 802.
f_prep() returned an error, exiting
traceback:
main:572
Exiting on error or interrupt
The network is working of course.
Thanks
已解决! 转到解答。
Hi Roger,
It's great you have solved the problem. If you have no other questions, would you please help click correct answer or helpful answer? Thanks a lot . If any questions contact us :smileyhappy:
Best Regards
Dan