using ltib L3.0.35_4.1.0_130816 unable to prep packages

cancel
Showing results for 
Search instead for 
Did you mean: 

using ltib L3.0.35_4.1.0_130816 unable to prep packages

Jump to solution
777 Views
Contributor II

Hello,

recently insatlled this ltib to buld linux for a sabrelite board.  Build went ok after a few hicups.  Now with everything built I wanted to prep some packages, like boot_stream, u_boot, and kernel to examine sources.  This is something I was doing a few months ago with L2.6.35_1.1.0_130130 ltib.  Here is what I see:

$ ./ltib -p boot_stream.spec -m prep

defined(@array) is deprecated at /home/csc/csc_projects/imx6_project1/ltib/bin/Ltibutils.pm line 362.

        (Maybe you should just omit the defined()?)

Processing: boot_stream

=========================

Build path taken because: build key set, no prebuilt rpm,

Testing network connectivity

OK GPP:

Try imx-bootlets-src-3.0.35-4.1.0.tar.gz.md5 from the GPP

http://bitshrine.org/gpp/imx-bootlets-src-3.0.35-4.1.0.tar.gz.md5:

11:09:51 ERROR 404: Not Found.

Try imx-bootlets-src-3.0.35-4.1.0.tar.gz from the GPP

http://bitshrine.org/gpp/imx-bootlets-src-3.0.35-4.1.0.tar.gz:

11:09:51 ERROR 404: Not Found.

Can't get: imx-bootlets-src-3.0.35-4.1.0.tar.gz at ./ltib line 802.

f_prep() returned an error, exiting

traceback:

main:572

Exiting on error or interrupt

The network is working of course.

Thanks

Tags (1)
0 Kudos
1 Solution
60 Views
NXP TechSupport
NXP TechSupport

Hi Roger,

Have you installed LTIB and build linux BSP succeed sabrelite board yet?

Best Regards

Dan

View solution in original post

0 Kudos
3 Replies
61 Views
NXP TechSupport
NXP TechSupport

Hi Roger,

Have you installed LTIB and build linux BSP succeed sabrelite board yet?

Best Regards

Dan

View solution in original post

0 Kudos
60 Views
Contributor II

yes its fine now, the bootlets source tarball is not in the /pkgs so I guess something is wrong with the URL, but I don't need bootlets now anyway so ....

0 Kudos
60 Views
NXP TechSupport
NXP TechSupport

Hi Roger,

It's great you have solved the problem. If you have no other questions, would you please help click correct answer or helpful answer? Thanks a lot . If any questions contact us :smileyhappy:

Best Regards

Dan

0 Kudos