I download L3.0.35_4.1.0_130816_images_MX6 from freescale website. I copied u-boot, uImage and rootfs into a SD card accroding to i.MX_6Dual6Quad_SABRE-SD-Linux_User's_Guide.pdf. After that I set up Ubuntu roots oneiric.tgz to the SD card.
Then I boot the board. There are some errors but it still be booted and in the root@linaro-ubuntu-desktop:~# . I attached the boot log file.
I can't see any display on the LCD on the board. I have checked the video setting in the boot env.
bootargs_mmc=setenv bootargs ${bootargs} root=/dev/mmcblk1p1 rootwait rw video=mxcfb1:dev=ldb,LDB-XGA,if=RGB666 video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24
Does anyone can help me if my ubunto image is correct according to the log?
Why there is no any display on the LCD on the board?
Thanks.
Original Attachment has been moved to: log_Mar_26_2014.txt.zip
已解决! 转到解答。
Hi wenjing,
Are you using i.mx6q-sdp board? And which LCD are you using ? If you are using CLAA-WVGA LCD, you just need to modify the u-boot "video=mxcfb0:dev=lcd,CLAA-WVGA,if=RGB565". If not , you need to modify the lcd driver and adding the LCD information you are using. So that the LCD can display.
Hope this can help you~~
Have a great day
Best Regards
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Yao,
Here you can download it and more document from freescale official website. Here I can attached it for you, hope this can help you.
Have a great day,
Best Regards
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi, all
Thanks for your help.Today I realized my problem was in ubuntu image burning. I tried these commands on a SD card with good ubuntu. Everything is fine.
My problem maybe caused by error‘connect to socket /var/run/dbus/system_bus_socket’ during reboot.
Hi wenjing,
It's great that your problem have been solved. If no any problems, would you please help closing this thread by click on Correct Answer and helpful answer.
Thanks a lot~~
Have a nice day
Best Regards
Dan
Wally,
Thanks for your replay
I didn't use HDMI. I just want to get display on the LCD on the sabreSD board.
1. cat /proc/cmdline
console=ttymxc0,115200 root=/dev/mmcblk1p1 rootwait rw video=mxcfb1:dev=ldb,LDB-XGA,if=RGB666 video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24
2.xrandr
Can't open display :smileylaugh:
if you export DISPLAY=:0 first, but still can't get xrandr output.
that indicate Xorg may not started yet, try "ps aux | grep Xorg" and check your Xorg is running or not.
if Xorg is running but you still get no output, you might get wrong device when you start the system.
I use the this board to attach HDMI LCD monitor, here is my /proc/cmdline:
console=ttymxc0,115200 root=/dev/mmcblk0p2 rootwait rw fbmem=64M video=mxcfb0:dev=vga,1920x1080M@60,if=RGB24,bpp=32
you can see my device argument: "video=mxcfb0:dev=vga,1920x1080M@60,if=RGB24,bpp=32"
I not sure what device is needed using in-board LCD panel.
Wally
After I try "ps aux | grep Xorg", I get.
root 14409 0.0 0.0 2960 704 ttymxc0 S+ 00:04 0:00 grep --color=auto Xorg
Then I tried this one
setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/mmcblk1p1 rootfstype=ext4 rootwait video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666,bpp=32 ldb=sin1 fbmem=10M'
I can see a only dash flash on the lcd.
I tried
export DISPLAY=:0 & xrandr.
Can't open display : 0
I don't know which is the right command to start display in in-board LCD.
Hi wenjing,
Are you using i.mx6q-sdp board? And which LCD are you using ? If you are using CLAA-WVGA LCD, you just need to modify the u-boot "video=mxcfb0:dev=lcd,CLAA-WVGA,if=RGB565". If not , you need to modify the lcd driver and adding the LCD information you are using. So that the LCD can display.
Hope this can help you~~
Have a great day
Best Regards
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
wenjing:
So your Xorg not started yet, you only grep one process contains "Xorg" string, and that's you "ps aux | grep Xorg" command.
Since Xorg not started, you will never get xrandr output.
unfortunately I don't know the correct device either.
I noticed that your u-boot args "bootargs_mmc=setenv bootargs ${bootargs} root=/dev/mmcblk1p1 rootwait rw video=mxcfb1:dev=ldb,LDB-XGA,if=RGB666 video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24"
you might need to changed it.
you can refer PDF file "i.MX_6Dual6Quad_Sabre-SD_Linux_User_Guide.pdf", search string "video", you need to test all bootargs_mmc yourself to fit in your case.