Can i.MX6DL use nandwrite command to program a boot image to NAND?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can i.MX6DL use nandwrite command to program a boot image to NAND?

Jump to solution
1,877 Views
satoshishimoda
Senior Contributor I

Hi community,

Our partner tried programing a boot image to NAND (/dev/mtd0) by i.MX6DL with "nandwrite" command, but it was failed.

So they tried also programing with "kobs-ng", and it was succeeded.

On the other hand, i.MX51 could progam a boot image to NAND with "nandwrite" command.

So we want to know is there some restrict to use "nandwrite" with i.MX6DL.

Could you let me know it?

Or there is no restrict and some procedure of our partner was wrong?

Best Regards,

Satoshi Shimoda

Labels (2)
Tags (1)
0 Kudos
Reply
1 Solution
1,622 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi,

unfortunately can not, "nandwrite" command is used for jffs2 file system.

Freescale i.MX6 BSPs support only ubifs, while i.MX51  - jffs2.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,623 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi,

unfortunately can not, "nandwrite" command is used for jffs2 file system.

Freescale i.MX6 BSPs support only ubifs, while i.MX51  - jffs2.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply