uboot logo color is not normal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

uboot logo color is not normal

Jump to solution
55,459 Views
fulinux
Contributor IV

Dear Community,

board: imx6q;

version: u-boot-2009.08;

i did what this doc said: https://community.nxp.com/docs/DOC-98109

but the logo color is not normal, it si green like this:

P60512-190156.jpg

what is wrong? and this is my head file:

    //#define IPU_OUTPUT_MODE_HDMI

    #define IPU_OUTPUT_MODE_LVDS

//  #define IPU_OUTPUT_MODE_LCD

#ifdef IPU_OUTPUT_MODE_LVDS

    // For LVDS, 1920*1080 resolution, dual channel

    #define DISPLAY_WIDTH   1920

    #define DISPLAY_HEIGHT  1080

    #define DISPLAY_BPP     32

    #define DISPLAY_IF_BPP  24  // RGB24 interface

    #define DISPLAY_HSYNC_START 80

    #define DISPLAY_HSYNC_END       68

    #define DISPLAY_HSYNC_WIDTH 12

    #define DISPLAY_VSYNC_START 15

    #define DISPLAY_VSYNC_END   15

    #define DISPLAY_VSYNC_WIDTH 8

#define DISPLAY_PIX_CLOCK   139526400  //(DISPLAY_HSYNC_START + DISPLAY_HSYNC_END + DISPLAY_HSYNC_WIDTH + DISPLAY_WIDTH) *   

(DISPLAY_VSYNC_START + DISPLAY_VSYNC_END + DISPLAY_VSYNC_WIDTH + DISPLAY_HEIGHT) * refresh rate (60Hz)

    #define LVDS_SPLIT_MODE  // For dual channel split mode.

    #define DISPLAY_VSYNC_POLARITY          1

    #define DISPLAY_HSYNC_POLARITY          1

    #define DISPLAY_CLOCK_POLARITY          1

    #define DISPLAY_DATA_POLARITY               0

    #define DISPLAY_DATA_ENABLE_POLARITY        1

    #define IPU_NUM         1  // 1 for IPU1, 2 for IPU2.

    #define DI_NUM          0  // 0 for DI0, 1 for DI1.

    #define LVDS_PORT       0  // 0 for LVDS0, 1 for LVDS1.

    #define DI_CLOCK_EXTERNAL_MODE  //When clock external mode was defined, the DI clock root will be PLL3 PFD1,

                                //without this macro, the DI root clock is IPU internal clock.

nothing changed, just above, can you help me? what should i do? what is info do you need? tell me.

wating for your reply?

thank you.

fulinux.

Labels (1)
Tags (2)
1 Solution
51,167 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

I had identified the issue, please apply the attached uboot patch to fix it.

it is based on JB4.3_1.1.1_uboot_logo_keep_patch_2015-09-18.zip

View solution in original post

0 Kudos
46 Replies
48,201 Views
fulinux
Contributor IV

kernel logo can show ppm file not bmp file, it is not logo file's problem, when i write 0x00 to fb memory is also little white. i have told you above. it is very strange.

0 Kudos
48,201 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

In linux, you can use dd command to show the bmp file to frame buffer:

dd if=logo.bmp of=/dev/fb0 bs=1 skip=54

You'd better find out the different display setting in your kernel and uboot.

0 Kudos
48,201 Views
jiejia
Contributor III

Dear Qiang,

I have the same problem. It may have some problem with the 0001-Enable-uboot-logo-for-HDMI-LCD-and-LVDS.patchThe LVDS CLK  is about 75M no matter what the DISPLAY_PIX_CLOCK is. Woud you mind testing for what I said?

0 Kudos
48,201 Views
fulinux
Contributor IV

Dear Qiang,

i did as you said, i shows well:

P60516-154851.jpg

do you need any information? pls tell me.

thank you,

fulinux.

0 Kudos
48,201 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

Maybe there is some wrong porting code in your uboot.

0 Kudos
48,201 Views
fulinux
Contributor IV

Hi, do you need my uboot code?

0 Kudos
48,201 Views
fulinux
Contributor IV

OK, i will test as you said;

and look at this:

pData = (unsigned char *)CONFIG_FB_BASE; CONFIG_FB_BASE = 0x27B00000

and i have write 0x00000 from 0x27B00000 to 0x27B00000 + bmp file size. and read memory by "md" command it shows right:

MX6Q SABRESD U-Boot > md 0x27B00000

27b00000: 00000000 00000000 00000000 00000000    ................

27b00010: 00000000 00000000 00000000 00000000    ................

27b00020: 00000000 00000000 00000000 00000000    ................

27b00030: 00000000 00000000 00000000 00000000    ................

....

but now, the lcd panel is still litte white:

P60513-154733.jpg

but it is not more white than when i write 0xfffffff to fb memory. i don't know if you know what i mean.

thank you,

fulinux.

0 Kudos
48,201 Views
fulinux
Contributor IV

Hi Qiang,

with my kernel attach file

0 Kudos
48,204 Views
fulinux
Contributor IV

hi Qiang,

is it wrong with my backlight and lcd power settings of gpios, this is my settings:

at setup_lvds_iomux() function in board/freescale/mx6q_sabresd/mx6q_sabresd.c:

#if defined CONFIG_MX6Q

    /* GPIO backlight */

    //mxc_iomux_v3_setup_pad(MX6Q_PAD_SD1_DAT3__PWM1_PWMO);

    mxc_iomux_v3_setup_pad(MX6Q_PAD_GPIO_9__PWM1_PWMO);

    /* LVDS panel CABC_EN */

    mxc_iomux_v3_setup_pad(MX6Q_PAD_NANDF_CS2__GPIO_6_15);

    mxc_iomux_v3_setup_pad(MX6Q_PAD_NANDF_CS3__GPIO_6_16);

    mxc_iomux_v3_setup_pad(MX6Q_PAD_GPIO_2__GPIO_1_2);

    mxc_iomux_v3_setup_pad(MX6Q_PAD_GPIO_7__GPIO_1_7);

    mxc_iomux_v3_setup_pad(MX6Q_PAD_GPIO_19__GPIO_4_5);

    reg = readl(GPIO6_BASE_ADDR + GPIO_DR);

    reg &= ~(1 << 16);

    writel(reg, GPIO6_BASE_ADDR + GPIO_DR);

#if 1

    gpio_direction_output(IMX_GPIO_NR(1, 2), 1);

    udelay(10 * 1000);

    gpio_set_value(IMX_GPIO_NR(1, 2), 0);

    udelay(10 * 1000);

    gpio_set_value(IMX_GPIO_NR(1, 2), 1);

    gpio_direction_output(IMX_GPIO_NR(4, 5), 1);

    udelay(10 * 1000);

    gpio_set_value(IMX_GPIO_NR(4, 5), 1);

    gpio_direction_output(IMX_GPIO_NR(1, 7), 0);

    udelay(10 * 1000);

    gpio_set_value(IMX_GPIO_NR(1, 7), 0);

#endif

at board_late_init() function:

    ipu_display_setup();

    gpio_set_value(IMX_GPIO_NR(1, 7), 1);

    udelay(10 * 1000);

    gpio_set_value(IMX_GPIO_NR(4, 5), 0);

Do you think that was right?

with my attach file.

0 Kudos
48,212 Views
fulinux
Contributor IV

Hi,

when i modified this:

    #define DISPLAY_WIDTH  1920

    #define DISPLAY_HEIGHT  1080

    #define DISPLAY_BPP    32

    #define DISPLAY_IF_BPP  24  // RGB24 interface

    #define DISPLAY_HSYNC_START 80

    #define DISPLAY_HSYNC_END  68

    #define DISPLAY_HSYNC_WIDTH 12

    #define DISPLAY_VSYNC_START 15

    #define DISPLAY_VSYNC_END  15

    #define DISPLAY_VSYNC_WIDTH 8

    #define DISPLAY_PIX_CLOCK  139526400  //(DISPLAY_HSYNC_START + DISPLAY_HSYNC_END + DISPLAY_HSYNC_WIDTH + DISPLAY_WIDTH) *    

(DISPLAY_VSYNC_START + DISPLAY_VSYNC_END + DISPLAY_VSYNC_WIDTH + DISPLAY_HEIGHT) * refresh rate (60Hz)

    #define LVDS_SPLIT_MODE  1  // For dual channel split mode.

#endif

    #define DISPLAY_VSYNC_POLARITY          0

    #define DISPLAY_HSYNC_POLARITY          0

    #define DISPLAY_CLOCK_POLARITY          1

    #define DISPLAY_DATA_POLARITY              0

    #define DISPLAY_DATA_ENABLE_POLARITY        1

    #define IPU_NUM        1  // 1 for IPU1, 2 for IPU2.

    #define DI_NUM          0  // 0 for DI0, 1 for DI1.

    #define LVDS_PORT      1  // 0 for LVDS0, 1 for LVDS1.

    #define DI_CLOCK_EXTERNAL_MODE  //When clock external mode was defined, the DI clock root will be PLL3 PFD1,

                                //without this macro, the DI root clock is IPU internal clock.

and

    bmpReady = 0;

    if (bmpReady == 0) {

        // Fill RGB frame buffer

        // Red

        for (i = 0; i < (DISPLAY_WIDTH * DISPLAY_HEIGHT * (DISPLAY_BPP / 8) / 3); i += (DISPLAY_BPP / 8)) {

#if (DISPLAY_BPP == 16)

            pData[i + 0] = 0x00;

            pData[i + 1] = 0xF8;

#else

and the lcd panel screen display like this:

P60513-152541.jpg

you can look at this, the color is lighter;

when i change code like this, change "pData[] = 0x FF" to 0x00:

        // Red

        for (i = 0; i < (DISPLAY_WIDTH * DISPLAY_HEIGHT * (DISPLAY_BPP / 8) / 3); i += (DISPLAY_BPP / 8)) {

#if (DISPLAY_BPP == 16)

            pData[i + 0] = 0x00;

            pData[i + 1] = 0xF8;

#else

            pData[i + 0] = 0x00;

            pData[i + 1] = 0x00;

            pData[i + 2] = 0x00;

            pData[i + 3] = 0x00;

#endif

        }

        // Green

        for (; i < (DISPLAY_WIDTH * DISPLAY_HEIGHT * (DISPLAY_BPP / 8) / 3) * 2; i += (DISPLAY_BPP / 8)) {

#if (DISPLAY_BPP == 16)

            pData[i + 0] = 0xE0;

            pData[i + 1] = 0x07;

#else

            pData[i + 0] = 0x00;

            pData[i + 1] = 0x00;

            pData[i + 2] = 0x00;

            pData[i + 3] = 0x00;

#endif

        }

        // Blue

        for (; i < DISPLAY_WIDTH * DISPLAY_HEIGHT * (DISPLAY_BPP / 8); i += (DISPLAY_BPP / 8)) {

#if (DISPLAY_BPP == 16)

            pData[i + 0] = 0x1F;

            pData[i + 1] = 0x00;

#else

            pData[i + 0] = 0x00;

            pData[i + 1] = 0x00;

            pData[i + 2] = 0x00;

            pData[i + 3] = 0x00;

then like this:

P60513-154733.jpg

it should be black,but it is whilt!

0 Kudos
48,212 Views
huaweiyu
Contributor I

hi,

could you tell me the path of file where you insert  bmpReady = 0;

thank you

0 Kudos
48,212 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

Yes, from your kernel setting, the DE is high active, so it should be "#define DISPLAY_DATA_ENABLE_POLARITY  1"

For black to white issue, you can change DISPLAY_DATA_POLARITY from 0 to 1 to invert the data line.

I think all these informations should be found from your panel's datasheet.

0 Kudos
48,212 Views
fulinux
Contributor IV

when it should be black it shows white, but when it should be whilt it shows more white, so it can't shows black.

when i change "#define IPU_NUM 1" to 2,it shows white, red and blue looply, why

0 Kudos
48,212 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

Another thing can be tried: invert the clock polarity, change DISPLAY_CLOCK_POLARITY from 1 to 0.

The display shows white, red and blue looply, that means the panel hasn't found valid input signal and show its test pattern.

0 Kudos
48,212 Views
fulinux
Contributor IV

it dosen't change anything when i change DISPLAY_CLOCK_POLARITY from 1 to 0. this is logo picture(original picture):

254-1401010Z511.jpg

this is the screen shows:

P60513-163732.jpg

0 Kudos
48,212 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

Can you attach your bmp file and panel datasheet here?

0 Kudos
48,212 Views
fulinux
Contributor IV

Yes ^_^ !

ps.

logo.bmp-bak file: this file i have skiped 54bytes from logo.bmp;

0 Kudos
48,212 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

From the datasheet, the setting should be followed, no other issues found.

#define DISPLAY_VSYNC_POLARITY   0

#define DISPLAY_HSYNC_POLARITY   0

#define DISPLAY_CLOCK_POLARITY   0

#define DISPLAY_DATA_POLARITY    0

#define DISPLAY_DATA_ENABLE_POLARITY  1

0 Kudos
48,212 Views
fulinux
Contributor IV

Hi,

it doesn't change anything when i did as what you said. it still like this:

P60513-163732.jpg

i am trying uboot-2015.04(on branch imx_v2015.04_4.1.15_1.0.0_ga), how can i enable split mode in uboot-2015.04?

0 Kudos
48,212 Views
fulinux
Contributor IV

Dear all,

can anybody help me? how can i solve this problem?

fulinux.

0 Kudos
48,212 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

How about your hardware connection?

Do you just used three pair of LVDS data lane? If so, you should set "#define DISPLAY_IF_BPP  24 " to 18.

0 Kudos