uboot imx8 agl error: u-boot-fslc_2017.11.bb:do_compile

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

uboot imx8 agl error: u-boot-fslc_2017.11.bb:do_compile

851件の閲覧回数
manizillion
Contributor IV

Hi,

i am getting this following error, any inputs regarding this ? ..


Build Configuration:
BB_VERSION           = "1.40.0"
BUILD_SYS            = "x86_64-linux"
NATIVELSBSTRING      = "universal"
TARGET_SYS           = "aarch64-agl-linux"
MACHINE              = "imx8mqevk"
DISTRO               = "poky-agl"
DISTRO_VERSION       = "8.90.0+snapshot-20190913"
TUNE_FEATURES        = "aarch64"
TARGET_FPU           = ""
meta-qt5             = "HEAD:1520d5b2b2beec5e1c3209d3178219e93ef08bca"
meta-agl-profile-graphical-qt5
meta-agl-profile-graphical = "HEAD:f7c7f376caefa9a788eee191220a4a424d0dad0c"
meta-pipewire        = "HEAD:5abdfef072e961c9922f6da3594fb2561735407c"
meta-agl-demo        = "HEAD:abe2d9282954936e222c2989c1d6bbbbead939fc"
meta-freescale_nxp   
meta-freescale-distro = "<unknown>:<unknown>"
meta-freescale       = "HEAD:f5c932229c31b612cba38c2ed6f3c3ec6b800e92"
meta-oe              
meta-multimedia      
meta-networking      
meta-python          
meta-filesystems     = "HEAD:9b3b907f30b0d5b92d58c7e68289184fda733d3e"
meta-agl-profile-core
meta-agl-distro      
meta-agl-bsp         = "HEAD:f7c7f376caefa9a788eee191220a4a424d0dad0c"
meta-security        = "HEAD:31dc4e7532fa7a82060e0b50e5eb8d0414aa7e93"
meta-perl            = "HEAD:9b3b907f30b0d5b92d58c7e68289184fda733d3e"
meta-security        
meta-app-framework   = "HEAD:f7c7f376caefa9a788eee191220a4a424d0dad0c"
meta                 
meta-poky            = "HEAD:d43a86de1a37ce9daede726a49231547a21429a5"

Initialising tasks: 100% |######################################################################################################| Time: 0:00:03
Sstate summary: Wanted 579 Found 51 Missed 528 Current 1337 (8% match, 72% complete)
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
ERROR: u-boot-fslc-v2017.11+gitAUTOINC+ca0c3f3fac-r0 do_compile: oe_runmake failed
ERROR: u-boot-fslc-v2017.11+gitAUTOINC+ca0c3f3fac-r0 do_compile: Function failed: do_compile (log file is located at /home/imx8/master-agl/build/tmp/work/imx8mqevk-agl-linux/u-boot-fslc/v2017.11+gitAUTOINC+ca0c3f3fac-r0/temp/log.do_compile.6126)
ERROR: Logfile of failure stored in: /home/imx8/master-agl/build/tmp/work/imx8mqevk-agl-linux/u-boot-fslc/v2017.11+gitAUTOINC+ca0c3f3fac-r0/temp/log.do_compile.6126
Log data follows:
| DEBUG: Executing shell function do_compile
| NOTE: make -j 8 CROSS_COMPILE=aarch64-agl-linux- CC=aarch64-agl-linux-gcc  --sysroot=/home/imx8/master-agl/build/tmp/work/imx8mqevk-agl-linux/u-boot-fslc/v2017.11+gitAUTOINC+ca0c3f3fac-r0/recipe-sysroot V=1 HOSTCC=gcc  -isystem/home/imx8/master-agl/build/tmp/work/imx8mqevk-agl-linux/u-boot-fslc/v2017.11+gitAUTOINC+ca0c3f3fac-r0/recipe-sysroot-native/usr/include -O2 -pipe -L/home/imx8/master-agl/build/tmp/work/imx8mqevk-agl-linux/u-boot-fslc/v2017.11+gitAUTOINC+ca0c3f3fac-r0/recipe-sysroot-native/usr/lib -L/home/imx8/master-agl/build/tmp/work/imx8mqevk-agl-linux/u-boot-fslc/v2017.11+gitAUTOINC+ca0c3f3fac-r0/recipe-sysroot-native/lib -Wl,-rpath-link,/home/imx8/master-agl/build/tmp/work/imx8mqevk-agl-linux/u-boot-fslc/v2017.11+gitAUTOINC+ca0c3f3fac-r0/recipe-sysroot-native/usr/lib -Wl,-rpath-link,/home/imx8/master-agl/build/tmp/work/imx8mqevk-agl-linux/u-boot-fslc/v2017.11+gitAUTOINC+ca0c3f3fac-r0/recipe-sysroot-native/lib -Wl,-rpath,/home/imx8/master-agl/build/tmp/work/imx8mqevk-agl-linux/u-boot-fslc/v2017.11+gitAUTOINC+ca0c3f3fac-r0/recipe-sysroot-native/usr/lib -Wl,-rpath,/home/imx8/master-agl/build/tmp/work/imx8mqevk-agl-linux/u-boot-fslc/v2017.11+gitAUTOINC+ca0c3f3fac-r0/recipe-sysroot-native/lib -Wl,-O1 -Wl,--allow-shlib-undefined -Wl,--dynamic-linker=/home/imx8/master-agl/build/tmp/sysroots-uninative/x86_64-linux/lib/ld-linux-x86-64.so.2 PYTHON=nativepython STAGING_INCDIR=/home/imx8/master-agl/build/tmp/work/imx8mqevk-agl-linux/u-boot-fslc/v2017.11+gitAUTOINC+ca0c3f3fac-r0/recipe-sysroot-native/usr/include STAGING_LIBDIR=/home/imx8/master-agl/build/tmp/work/imx8mqevk-agl-linux/u-boot-fslc/v2017.11+gitAUTOINC+ca0c3f3fac-r0/recipe-sysroot-native/usr/lib HOSTCC=gcc  -isystem/home/imx8/master-agl/build/tmp/work/imx8mqevk-agl-linux/u-boot-fslc/v2017.11+gitAUTOINC+ca0c3f3fac-r0/recipe-sysroot-native/usr/include HOSTLDFLAGS=-L/home/imx8/master-agl/build/tmp/work/imx8mqevk-agl-linux/u-boot-fslc/v2017.11+gitAUTOINC+ca0c3f3fac-r0/recipe-sysroot-native/usr/lib -L/home/imx8/master-agl/build/tmp/work/imx8mqevk-agl-linux/u-boot-fslc/v2017.11+gitAUTOINC+ca0c3f3fac-r0/recipe-sysroot-native/lib -Wl,-rpath-link,/home/imx8/master-agl/build/tmp/work/imx8mqevk-agl-linux/u-boot-fslc/v2017.11+gitAUTOINC+ca0c3f3fac-r0/recipe-sysroot-native/usr/lib -Wl,-rpath-link,/home/imx8/master-agl/build/tmp/work/imx8mqevk-agl-linux/u-boot-fslc/v2017.11+gitAUTOINC+ca0c3f3fac-r0/recipe-sysroot-native/lib -Wl,-rpath,/home/imx8/master-agl/build/tmp/work/imx8mqevk-agl-linux/u-boot-fslc/v2017.11+gitAUTOINC+ca0c3f3fac-r0/recipe-sysroot-native/usr/lib -Wl,-rpath,/home/imx8/master-agl/build/tmp/work/imx8mqevk-agl-linux/u-boot-fslc/v2017.11+gitAUTOINC+ca0c3f3fac-r0/recipe-sysroot-native/lib -Wl,-O1 -Wl,--allow-shlib-undefined -Wl,--dynamic-linker=/home/imx8/master-agl/build/tmp/sysroots-uninative/x86_64-linux/lib/ld-linux-x86-64.so.2 HOSTSTRIP=true -C /home/imx8/master-agl/build/tmp/work/imx8mqevk-agl-linux/u-boot-fslc/v2017.11+gitAUTOINC+ca0c3f3fac-r0/git O=/home/imx8/master-agl/build/tmp/work/imx8mqevk-agl-linux/u-boot-fslc/v2017.11+gitAUTOINC+ca0c3f3fac-r0/build/imx8mq_evk_config imx8mq_evk_config
| make: Entering directory '/home/imx8/master-agl/build/tmp/work/imx8mqevk-agl-linux/u-boot-fslc/v2017.11+gitAUTOINC+ca0c3f3fac-r0/git'
| make -C /home/imx8/master-agl/build/tmp/work/imx8mqevk-agl-linux/u-boot-fslc/v2017.11+gitAUTOINC+ca0c3f3fac-r0/build/imx8mq_evk_config KBUILD_SRC=/home/imx8/master-agl/build/tmp/work/imx8mqevk-agl-linux/u-boot-fslc/v2017.11+gitAUTOINC+ca0c3f3fac-r0/git \
| -f /home/imx8/master-agl/build/tmp/work/imx8mqevk-agl-linux/u-boot-fslc/v2017.11+gitAUTOINC+ca0c3f3fac-r0/git/Makefile imx8mq_evk_config
| make[1]: Entering directory '/home/imx8/master-agl/build/tmp/work/imx8mqevk-agl-linux/u-boot-fslc/v2017.11+gitAUTOINC+ca0c3f3fac-r0/build/imx8mq_evk_config'
| make -f /home/imx8/master-agl/build/tmp/work/imx8mqevk-agl-linux/u-boot-fslc/v2017.11+gitAUTOINC+ca0c3f3fac-r0/git/scripts/Makefile.build obj=scripts/basic
| ln -fsn /home/imx8/master-agl/build/tmp/work/imx8mqevk-agl-linux/u-boot-fslc/v2017.11+gitAUTOINC+ca0c3f3fac-r0/git source
| /bin/bash /home/imx8/master-agl/build/tmp/work/imx8mqevk-agl-linux/u-boot-fslc/v2017.11+gitAUTOINC+ca0c3f3fac-r0/git/scripts/mkmakefile \
|     /home/imx8/master-agl/build/tmp/work/imx8mqevk-agl-linux/u-boot-fslc/v2017.11+gitAUTOINC+ca0c3f3fac-r0/git . 2017 11
|   GEN     ./Makefile
| rm -f .tmp_quiet_recordmcount
| make -f /home/imx8/master-agl/build/tmp/work/imx8mqevk-agl-linux/u-boot-fslc/v2017.11+gitAUTOINC+ca0c3f3fac-r0/git/scripts/Makefile.build obj=scripts/kconfig imx8mq_evk_config
| scripts/kconfig/conf  --defconfig=arch/../configs/imx8mq_evk_defconfig Kconfig
| ***
| *** Can't find default configuration "arch/../configs/imx8mq_evk_defconfig"!
| ***
| /home/imx8/master-agl/build/tmp/work/imx8mqevk-agl-linux/u-boot-fslc/v2017.11+gitAUTOINC+ca0c3f3fac-r0/git/scripts/kconfig/Makefile:121: recipe for target 'imx8mq_evk_defconfig' failed
| make[2]: *** [imx8mq_evk_defconfig] Error 1
| /home/imx8/master-agl/build/tmp/work/imx8mqevk-agl-linux/u-boot-fslc/v2017.11+gitAUTOINC+ca0c3f3fac-r0/git/Makefile:479: recipe for target 'imx8mq_evk_config' failed
| make[1]: *** [imx8mq_evk_config] Error 2
| make[1]: Leaving directory '/home/imx8/master-agl/build/tmp/work/imx8mqevk-agl-linux/u-boot-fslc/v2017.11+gitAUTOINC+ca0c3f3fac-r0/build/imx8mq_evk_config'
| ERROR: oe_runmake failed
| Makefile:150: recipe for target 'sub-make' failed
| make: *** [sub-make] Error 2
| make: Leaving directory '/home/imx8/master-agl/build/tmp/work/imx8mqevk-agl-linux/u-boot-fslc/v2017.11+gitAUTOINC+ca0c3f3fac-r0/git'
| WARNING: exit code 1 from a shell command.
| ERROR: Function failed: do_compile (log file is located at /home/imx8/master-agl/build/tmp/work/imx8mqevk-agl-linux/u-boot-fslc/v2017.11+gitAUTOINC+ca0c3f3fac-r0/temp/log.do_compile.6126)
ERROR: Task (/home/imx8/master-agl/bsp/meta-freescale/recipes-bsp/u-boot/u-boot-fslc_2017.11.bb:do_compile) failed with exit code '1'

Second Keyboard Interrupt, stopping...


Summary: 1 task failed:
  /home/imx8/master-agl/bsp/meta-freescale/recipes-bsp/u-boot/u-boot-fslc_2017.11.bb:do_compile
Summary: There were 7 WARNING messages shown.
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.

0 件の賞賛
返信
1 返信

711件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Manivannan s,

The AGL demo has been tested with the i.MX6Q so there is no much documentation on running it on the i.MX8. Perhaps the AGL forums may provide more insights.

I see that there has been some follow up on the Jira AGL Development. Hopefully they may provide further help.

https://jira.automotivelinux.org/browse/SPEC-2748?page=com.atlassian.jira.plugin.system.issuetabpane...

My apologies for the inconvenience.

Regards,

0 件の賞賛
返信