Hi All,
I have two boards:
I would like to create a unified u-boot that could setup/config the RAM in SPL stage.
My question is: there is a way to know if the board have a QUAD or DUAL?
The function "get_cpu_rev" does not help too much. Additionally, the current header definitions seems no have the dual:
#define MXC_CPU_MX51 | 0x51 | |
#define MXC_CPU_MX53 | 0x53 | |
#define MXC_CPU_MX6SL | 0x60 | |
#define MXC_CPU_MX6DL | 0x61 | |
#define MXC_CPU_MX6SOLO | 0x62 | |
#define MXC_CPU_MX6Q | 0x63 |
Thanks
已解决! 转到解答。
Hi Julio
i.MX6 Quad versus Dual differentiated by fuse NUM_CORES (0x430)
Table 5-10 Fusemap Descriptions IMX6DQRM
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Julio
i.MX6 Quad versus Dual differentiated by fuse NUM_CORES (0x430)
Table 5-10 Fusemap Descriptions IMX6DQRM
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------