Hi ,
Can anyone let me know what are below tuples used in "pins-imx8mq.h" file?
"<mux_reg conf_reg input_reg mux_mode input_val>"
I have understood that mux_reg is offset of mux reg and conf_reg is offset of pad reg, and also mux_mode is alt-mode used.
But what are input_reg and input_val?
Also let me know how values to particular pins are given in dts?
for example in below pins how 82 is decided?
MX8MQ_IOMUXC_ECSPI1_SCLK_ECSPI1_SCLK 0x82
Thanks and Regards,
Yashavantha
已解决! 转到解答。
Hi Yashavantha
these are input daisy register, for example
#define MX8MQ_IOMUXC_GPIO1_IO11_CCMSRCGPCMIX_PMIC_READY 0x054 0x2BC 0x4BC 0x5 0x1
nput_reg = 0x4BC - INPUT DAISY Register
input_val = 0x1
sect.8.2.4.299 CCM_PMIC_READY_SELECT_INPUT DAISY Register
(IOMUXC_CCM_PMIC_READY_SELECT_INPUT) i.MX8MDQ Reference Manual
https://www.nxp.com/docs/en/reference-manual/IMX8MDQLQRM.pdf
>for example in below pins how 82 is decided?
>MX8MQ_IOMUXC_ECSPI1_SCLK_ECSPI1_SCLK 0x82
this is setting for IOMUXC_SW_PAD_CTL_PAD_ECSPI1_SCLK described in
sect.8.2.4.275 SW_PAD_CTL_PAD_ECSPI1_SCLK SW PAD Control
Register (IOMUXC_SW_PAD_CTL_PAD_ECSPI1_SCLK) i.MX8MDQ Reference Manual
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Yashavantha
these are input daisy register, for example
#define MX8MQ_IOMUXC_GPIO1_IO11_CCMSRCGPCMIX_PMIC_READY 0x054 0x2BC 0x4BC 0x5 0x1
nput_reg = 0x4BC - INPUT DAISY Register
input_val = 0x1
sect.8.2.4.299 CCM_PMIC_READY_SELECT_INPUT DAISY Register
(IOMUXC_CCM_PMIC_READY_SELECT_INPUT) i.MX8MDQ Reference Manual
https://www.nxp.com/docs/en/reference-manual/IMX8MDQLQRM.pdf
>for example in below pins how 82 is decided?
>MX8MQ_IOMUXC_ECSPI1_SCLK_ECSPI1_SCLK 0x82
this is setting for IOMUXC_SW_PAD_CTL_PAD_ECSPI1_SCLK described in
sect.8.2.4.275 SW_PAD_CTL_PAD_ECSPI1_SCLK SW PAD Control
Register (IOMUXC_SW_PAD_CTL_PAD_ECSPI1_SCLK) i.MX8MDQ Reference Manual
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------