u-boot imx8mm does not boot from sdcard neither from e-mmc

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

u-boot imx8mm does not boot from sdcard neither from e-mmc

ソリューションへジャンプ
1,961件の閲覧回数
mariusoctavian
Contributor III



I have imx8mm evk

I am using this u-boot.

git clone https://github.com/nxp-imx/uboot-imx

I installed aarch64-linux-gnu- /usr/bin (ubuntu 22.04),
and I also have the aarch64--glibc--stable-2022.08-1 (I tried both compilers)

I am building like this.

COMPILER=aarch64-linux-gnu-  # from apt
##COMPILER=aarch64-linux-

export PATH=/path/to/tc/bin:$PATH

ARCH=arm CROSS_COMPILE=$COMPILER make imx8mm_evk_defconfig
ARCH=arm CROSS_COMPILE=COMPILER make clean
ARCH=arm CROSS_COMPILE=COMPILER make

after building I have these files

 

 

 

find -name '*.bin' -o -name '*.img'
./u-boot-dtb.img
./u-boot-nodtb.bin
./spl/u-boot-spl-nodtb.bin
./spl/u-boot-spl.bin
./tools/binman/test/descriptor.bin
./u-boot-dtb.bin
./u-boot.img
./u-boot.bin

 

 

 

I tried to dd the u-boot and/or spl as all kinds of combinations I've could find in scripts.

 

 

 

sudo dd if=./u-boot-*.bin<img> of=/dev/mmcblk0 bs=1k seek=XX=33/69
 

 

 

 


What is the right dd command and what u-boot files and what seek (ofsets) are correct ones for IMX8MM
sdcard and emmc?

I also tried all these

 

 

$ sudo dd if=<U-Boot image> of=/dev/sdx bs=1k seek=<offset> conv=fsync
Where offset is:
• 1 - for i.MX 6 or i.MX 7
• 33 - for i.MX 8QuadMax A0, i.MX 8QuadXPlus A0, and i.MX 8M Quad, and i.MX 8M Mini
• 32 - for i.MX 8QuadXPlus B0, i.MX 8QuadMax B0, i.MX 8DualX, i.MX 8DXL, i.MX 8M Nano, i.MX 8M Plus,
i.MX 8ULP, and i.MX 9

 

 

 

 

Thank you

 

 

 

 

 

 

0 件の賞賛
返信
1 解決策
1,894件の閲覧回数
mariusoctavian
Contributor III

Thank you,

I skipped the yocto thing. I will try with yocto, as looks like there is no escape from it.
I will reply as soon I get some positive results.

 

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
1,902件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

Hi @mariusoctavian 

I'd suggest you refer to the <4.5.12 How to build U-Boot and Kernel in standalone environment> and <4.5.13 How to build imx-boot image by using imx-mkimage> of i.MX Linux User's Guide (nxp.com)

 

Best regards

Harvey

0 件の賞賛
返信
1,892件の閲覧回数
mariusoctavian
Contributor III
 
0 件の賞賛
返信
1,895件の閲覧回数
mariusoctavian
Contributor III

Thank you,

I skipped the yocto thing. I will try with yocto, as looks like there is no escape from it.
I will reply as soon I get some positive results.

 

0 件の賞賛
返信
1,877件の閲覧回数
mariusoctavian
Contributor III
lol, i start yocto build yesterday, still building after 7 hours, octo core i7 2.7ghz ram 32gb
0 件の賞賛
返信
1,898件の閲覧回数
mariusoctavian
Contributor III

 

スポイラ
as per: user_guide


Right from host: using gcc


make distclean
make imx8mm_evk_defconfig
make
...
cc1: warning: unknown register name: x18
cc1: error: bad value (‘armv8-a+crc’) for ‘-march=’ switch​


and for arch64 with latest bootlin 2022 compiler

export PATH=/opt/tc/aarch64--glibc--stable-2022.08-1/bin:${PATH}
ARCH=arm64 CROSS_COMPILE=aarch64-linux-gnu- && make distclean
ARCH=arm64 CROSS_COMPILE=aarch64-linux-gnu- && make imx8mm_evk_defconfig
ARCH=arm64 CROSS_COMPILE=aarch64-linux-gnu- && make 


  CLEAN   spl/u-boot.cfg
  CLEAN   include/generated/env.in u-boot.cfg
  CLEAN   scripts/basic
  CLEAN   scripts/kconfig
  CLEAN   include/config include/generated spl
  CLEAN   .config .config.old include/autoconf.mk include/autoconf.mk.dep include/config.h
  HOSTCC  scripts/basic/fixdep
  HOSTCC  scripts/kconfig/conf.o
  YACC    scripts/kconfig/zconf.tab.c
  LEX     scripts/kconfig/zconf.lex.c
  HOSTCC  scripts/kconfig/zconf.tab.o
  HOSTLD  scripts/kconfig/conf
#
# configuration written to .config
#
scripts/kconfig/conf  --syncconfig Kconfig
  UPD     include/config.h
  CFG     u-boot.cfg
cc1: warning: unknown register name: x18
  GEN     include/autoconf.mk
  GEN     include/autoconf.mk.dep
cc1: warning: unknown register name: x18
  CFG     spl/u-boot.cfg
cc1: warning: unknown register name: x18
  GEN     spl/include/autoconf.mk
  UPD     include/config/uboot.release
  UPD     include/generated/version_autogenerated.h
  UPD     include/generated/timestamp_autogenerated.h
  UPD     include/generated/dt.h
  ENVC    include/generated/env.txt
  ENVP    include/generated/env.in
  ENVT    include/generated/environment.h
  CC      lib/asm-offsets.s
cc1: warning: unknown register name: x18
cc1: error: bad value (‘armv8-a+crc’) for ‘-march=’ switch
cc1: note: valid arguments to ‘-march=’ switch are: nocona core2 nehalem corei7 westmere sandybridge corei7-avx ivybridge core-avx-i haswell core-avx2 broadwell skylake skylake-avx512 cannonlake icelake-client icelake-server cascadelake tigerlake bonnell atom silvermont slm goldmont goldmont-plus tremont knl knm x86-64 eden-x2 nano nano-1000 nano-2000 nano-3000 nano-x2 eden-x4 nano-x4 k8 k8-sse3 opteron opteron-sse3 athlon64 athlon64-sse3 athlon-fx amdfam10 barcelona bdver1 bdver2 bdver3 bdver4 znver1 znver2 btver1 btver2 native
make[1]: *** [scripts/Makefile.build:143: lib/asm-offsets.s] Error 1
make: *** [Makefile:1954: prepare0] Error 2
/sdaone/PEG_PROJ/Kohler_wc/ICP_u_boot










 

 

0 件の賞賛
返信
1,937件の閲覧回数
mariusoctavian
Contributor III

I found that I need the imx-atf as well.
I cloned this:
https://github.com/nxp-imx/imx-atf
I Have gcc/c++ 9..to 11
git checkout imx_4.9.123_imx8mm_ga
ARCH=arm64 CROSS_COMPILE=aarch64-linux- && make PLAT=imx8mm CFG_ARM64_core=y

I tried all of them and I cannot pass

gcc: error: unrecognized command line option ‘-mstrict-align’; did you mean ‘-Wstrict-aliasing’?
gcc: error: unrecognized command line option ‘-mfix-cortex-a53-835769’

I tried to comment those then The errors goes deeper.

cc1: error: bad value (‘armv8-a’) for ‘-march=’ switch


Any help would be appreciated


0 件の賞賛
返信
1,642件の閲覧回数
mariusoctavian
Contributor III

RESOLVED WITH:

https://github.com/varigit/imx-atf.git
7575633e03ff952a18c0a2c0aa543dee793fda5f

https://github.com/nxp-imx/imx-mkimage.git
6745ccdcf15384891639b7ced3aa6ce938682365

https://github.com/varigit/uboot-imx.git
9458fd59dd6d69230438350c3aeb8ac803ff1b1c

and

aarch64--glibc--stable-2022.08-1


 

0 件の賞賛
返信