Hello support team,
we have developed a proprietary board derived from the NXP evaboard imx8mqevk.
The DDR memory format has changed to 2GB but u-boot always states 3GB of memory (the same size of the evaboard).
Yocto version is Zeus (imx-5.4.24-2.1.0)
The boot output:
------------------------------------------------------------------------------------------
U-Boot 2020.04-5.4.24-2.1.0+g4979a99482 (Apr 26 2021 - 10:03:28 +0000)
CPU: i.MX8MD rev2.1 1500 MHz (running at 1000 MHz)
CPU: Commercial temperature grade (0C to 95C) at 42C
Reset cause: POR
Model: NXP i.MX8MQ EVK
DRAM: 3 GiB
TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C0 0x50]
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... *** Warning - bad CRC, using default environment
<snip>
------------------------------------------------------------------------------------------
Still no luck, what else are we missing?
已解决! 转到解答。
Hi Giacomo
just for test one can try to build without OPTee, as described in sect.5.6.10 OP-TEE enablement
Yocto Guide included in Documentation
Also i.MX8M Mini EVK has 2GB configuration and one can look at its configs for comparison.
Best regards
igor
Hi Giacomo
just for test one can try to build without OPTee, as described in sect.5.6.10 OP-TEE enablement
Yocto Guide included in Documentation
Also i.MX8M Mini EVK has 2GB configuration and one can look at its configs for comparison.
Best regards
igor