hi,this is my modified base on the branch imx_v2015.04_4.1.15_1.0.0_ga patch:
diff --git a/arch/arm/lib/board.c b/arch/arm/lib/board.c
index 1f2bab1..faa938b 100644
--- a/arch/arm/lib/board.c
+++ b/arch/arm/lib/board.c
@@ -578,7 +578,7 @@ void board_init_r(gd_t *id, ulong dest_addr)
#endif
#ifdef CONFIG_GENERIC_MMC
- puts("MMC: ");
+ puts("fulinux MMC: ");
mmc_initialize(gd->bd);
#endif
@@ -592,6 +592,7 @@ void board_init_r(gd_t *id, ulong dest_addr)
dataflash_print_info();
#endif
+ printf ("fulinux xxxx\n");
/* initialize environment */
if (should_load_env())
env_relocate();
diff --git a/board/freescale/mx6sabresd/mx6sabresd.c b/board/freescale/mx6sabresd/mx6sabresd.c
index ee2b67b..8be2b10 100644
--- a/board/freescale/mx6sabresd/mx6sabresd.c
+++ b/board/freescale/mx6sabresd/mx6sabresd.c
@@ -58,9 +58,14 @@ DECLARE_GLOBAL_DATA_PTR;
PAD_CTL_SPEED_MED | PAD_CTL_DSE_40ohm | \
PAD_CTL_SRE_FAST | PAD_CTL_HYS)
+#define USDHC_PAD_CTRL (PAD_CTL_PKE | PAD_CTL_PUE | \
+ PAD_CTL_PUS_47K_UP | PAD_CTL_SPEED_HIGH | \
+ PAD_CTL_DSE_40ohm | PAD_CTL_SRE_FAST | PAD_CTL_HYS)
+#if 0
#define USDHC_PAD_CTRL (PAD_CTL_PUS_47K_UP | \
PAD_CTL_SPEED_LOW | PAD_CTL_DSE_80ohm | \
PAD_CTL_SRE_FAST | PAD_CTL_HYS)
+#endif
#define ENET_PAD_CTRL (PAD_CTL_PUS_100K_UP | \
PAD_CTL_SPEED_MED | PAD_CTL_DSE_40ohm | PAD_CTL_HYS)
@@ -129,6 +134,19 @@ static void setup_iomux_enet(void)
gpio_set_value(IMX_GPIO_NR(1, 25), 1);
}
+static iomux_v3_cfg_t const usdhc1_pads[] = {
+ MX6_PAD_SD1_CLK__SD1_CLK | MUX_PAD_CTRL(USDHC_PAD_CTRL),
+ MX6_PAD_SD1_CMD__SD1_CMD | MUX_PAD_CTRL(USDHC_PAD_CTRL),
+ MX6_PAD_SD1_DAT0__SD1_DATA0 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
+ MX6_PAD_SD1_DAT1__SD1_DATA1 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
+ MX6_PAD_SD1_DAT2__SD1_DATA2 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
+ MX6_PAD_SD1_DAT3__SD1_DATA3 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
+ MX6_PAD_NANDF_D0__SD1_DATA4 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
+ MX6_PAD_NANDF_D1__SD1_DATA5 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
+ MX6_PAD_NANDF_D2__SD1_DATA6 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
+ MX6_PAD_NANDF_D3__SD1_DATA7 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
+};
+
static iomux_v3_cfg_t const usdhc2_pads[] = {
MX6_PAD_SD2_CLK__SD2_CLK | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_SD2_CMD__SD2_CMD | MUX_PAD_CTRL(USDHC_PAD_CTRL),
@@ -140,7 +158,6 @@ static iomux_v3_cfg_t const usdhc2_pads[] = {
MX6_PAD_NANDF_D5__SD2_DATA5 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_NANDF_D6__SD2_DATA6 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_NANDF_D7__SD2_DATA7 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
- MX6_PAD_NANDF_D2__GPIO2_IO02 | MUX_PAD_CTRL(NO_PAD_CTRL), /* CD */
};
static iomux_v3_cfg_t const usdhc3_pads[] = {
@@ -154,7 +171,6 @@ static iomux_v3_cfg_t const usdhc3_pads[] = {
MX6_PAD_SD3_DAT5__SD3_DATA5 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_SD3_DAT6__SD3_DATA6 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_SD3_DAT7__SD3_DATA7 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
- MX6_PAD_NANDF_D0__GPIO2_IO00 | MUX_PAD_CTRL(NO_PAD_CTRL), /* CD */
};
static iomux_v3_cfg_t const usdhc4_pads[] = {
@@ -311,7 +327,8 @@ static void setup_iomux_uart(void)
}
#ifdef CONFIG_FSL_ESDHC
-struct fsl_esdhc_cfg usdhc_cfg[3] = {
+struct fsl_esdhc_cfg usdhc_cfg[4] = {
+ {USDHC1_BASE_ADDR},
{USDHC2_BASE_ADDR},
{USDHC3_BASE_ADDR},
{USDHC4_BASE_ADDR},
@@ -346,14 +363,16 @@ int mmc_map_to_kernel_blk(int dev_no)
return dev_no + 1;
}
-#define USDHC2_CD_GPIO IMX_GPIO_NR(2, 2)
-#define USDHC3_CD_GPIO IMX_GPIO_NR(2, 0)
+//#define USDHC2_CD_GPIO IMX_GPIO_NR(1, 4)
+//#define USDHC3_CD_GPIO IMX_GPIO_NR(7, 0)
int board_mmc_getcd(struct mmc *mmc)
{
struct fsl_esdhc_cfg *cfg = (struct fsl_esdhc_cfg *)mmc->priv;
int ret = 0;
+ return -1;
+#if 0
switch (cfg->esdhc_base) {
case USDHC2_BASE_ADDR:
ret = !gpio_get_value(USDHC2_CD_GPIO);
@@ -367,6 +386,7 @@ int board_mmc_getcd(struct mmc *mmc)
}
return ret;
+#endif
}
int board_mmc_init(bd_t *bis)
@@ -386,20 +406,23 @@ int board_mmc_init(bd_t *bis)
switch :smileyinfo: {
case 0:
imx_iomux_v3_setup_multiple_pads(
- usdhc2_pads, ARRAY_SIZE(usdhc2_pads));
- gpio_direction_input(USDHC2_CD_GPIO);
- usdhc_cfg[0].sdhc_clk = mxc_get_clock(MXC_ESDHC2_CLK);
+ usdhc1_pads, ARRAY_SIZE(usdhc1_pads));
+ usdhc_cfg[0].sdhc_clk = mxc_get_clock(MXC_ESDHC_CLK);
break;
case 1:
imx_iomux_v3_setup_multiple_pads(
- usdhc3_pads, ARRAY_SIZE(usdhc3_pads));
- gpio_direction_input(USDHC3_CD_GPIO);
- usdhc_cfg[1].sdhc_clk = mxc_get_clock(MXC_ESDHC3_CLK);
+ usdhc2_pads, ARRAY_SIZE(usdhc2_pads));
+ usdhc_cfg[1].sdhc_clk = mxc_get_clock(MXC_ESDHC2_CLK);
break;
case 2:
imx_iomux_v3_setup_multiple_pads(
+ usdhc3_pads, ARRAY_SIZE(usdhc3_pads));
+ usdhc_cfg[2].sdhc_clk = mxc_get_clock(MXC_ESDHC3_CLK);
+ break;
+ case 3:
+ imx_iomux_v3_setup_multiple_pads(
usdhc4_pads, ARRAY_SIZE(usdhc4_pads));
- usdhc_cfg[2].sdhc_clk = mxc_get_clock(MXC_ESDHC4_CLK);
+ usdhc_cfg[3].sdhc_clk = mxc_get_clock(MXC_ESDHC4_CLK);
break;
default:
printf("Warning: you configured more USDHC controllers"
diff --git a/common/board_r.c b/common/board_r.c
index b1ad605..59d0feb 100644
--- a/common/board_r.c
+++ b/common/board_r.c
@@ -400,7 +400,7 @@ static int initr_onenand(void)
#ifdef CONFIG_GENERIC_MMC
static int initr_mmc(void)
{
- puts("MMC: ");
+ puts("fulinux 1 MMC: ");
mmc_initialize(gd->bd);
return 0;
}
@@ -439,6 +439,7 @@ static int should_load_env(void)
static int initr_env(void)
{
+ printf ("fulinux initr_env()\n");
/* initialize environment */
if (should_load_env())
env_relocate();
diff --git a/common/env_common.c b/common/env_common.c
index af59c72..91c347a 100644
--- a/common/env_common.c
+++ b/common/env_common.c
@@ -251,6 +251,7 @@ int env_export(env_t *env_out)
void env_relocate(void)
{
+ printf ("fulinux env_relocate()\n");
#if defined(CONFIG_NEEDS_MANUAL_RELOC)
env_reloc();
env_htab.change_ok += gd->reloc_off;
diff --git a/common/env_mmc.c b/common/env_mmc.c
index fb006bd..33f9068 100644
--- a/common/env_mmc.c
+++ b/common/env_mmc.c
@@ -98,7 +98,7 @@ static inline int mmc_set_env_part(struct mmc *mmc) {return 0; };
static int init_mmc_for_env(struct mmc *mmc)
{
if (!mmc) {
- puts("No MMC card found\n");
+ puts("fulinux No MMC card found\n");
return -1;
}
@@ -303,11 +303,13 @@ void env_relocate_spec(void)
u32 offset;
int ret;
int dev = mmc_get_env_devno();
+ printf ("fulinux dev=%d\n", dev);
#ifdef CONFIG_SPL_BUILD
dev = 0;
#endif
+ printf ("fulinux env_relocate_spec\n");
mmc = find_mmc_device(dev);
if (init_mmc_for_env(mmc)) {
diff --git a/drivers/mmc/mmc.c b/drivers/mmc/mmc.c
index 830d9ae..f387be2 100644
--- a/drivers/mmc/mmc.c
+++ b/drivers/mmc/mmc.c
@@ -182,7 +182,7 @@ struct mmc *find_mmc_device(int dev_num)
}
#if !defined(CONFIG_SPL_BUILD) || defined(CONFIG_SPL_LIBCOMMON_SUPPORT)
- printf("MMC Device %d not found\n", dev_num);
+ printf("fuliux MMC Device %d not found\n", dev_num);
#endif
return NULL;
diff --git a/include/configs/mx6sabresd.h b/include/configs/mx6sabresd.h
index 153799e..ab8fd50 100644
--- a/include/configs/mx6sabresd.h
+++ b/include/configs/mx6sabresd.h
@@ -12,7 +12,7 @@
#include <asm/arch/imx-regs.h>
#include <asm/imx-common/gpio.h>
-#undef DEBUG
+#define DEBUG
#ifdef CONFIG_SPL
#define CONFIG_SPL_LIBCOMMON_SUPPORT
@@ -31,7 +31,7 @@
#define PHYS_SDRAM_SIZE (1u * 1024 * 1024 * 1024)
#elif defined(CONFIG_MX6Q)
#define CONFIG_DEFAULT_FDT_FILE "imx6q-sabresd.dtb"
-#define PHYS_SDRAM_SIZE (1u * 1024 * 1024 * 1024)
+#define PHYS_SDRAM_SIZE (2u * 1024 * 1024 * 1024)
#elif defined(CONFIG_MX6DL)
#define CONFIG_DEFAULT_FDT_FILE "imx6dl-sabresd.dtb"
#define PHYS_SDRAM_SIZE (1u * 1024 * 1024 * 1024)
@@ -42,8 +42,8 @@
#include "mx6sabre_common.h"
-#define CONFIG_SYS_FSL_USDHC_NUM 3
-#define CONFIG_SYS_MMC_ENV_DEV 1 /* SDHC3 */
+#define CONFIG_SYS_FSL_USDHC_NUM 4
+#define CONFIG_SYS_MMC_ENV_DEV 2 /* SDHC2 */
#define CONFIG_SYS_MMC_ENV_PART 0 /* user partition */
#ifdef CONFIG_SYS_USE_SPINOR
this is log when it runs on board:
U-Boot 2015.04-14468-g19b5506-dirty (Apr 20 2016 - 02:23:42)
initcall: 17805f44
U-Boot code: 17800000 -> 17864494 BSS: -> 178B20B4
initcall: 17801928
CPU: Freescale i.MX6Q rev1.5 at 792 MHz
uclass_find_device_by_seq: 0 -1
uclass_find_device_by_seq: 0 0
- -1 -1
- not found
CPU: Temperature 36 C
Reset cause: POR
initcall: 178063f4
Board: MX6-SabreSD
initcall: 17805f88
I2C: ready
initcall: 17805f70
DRAM: initcall: 17803168
initcall: 17806160
Monitor len: 000B20B4
Ram size: F0000000
Ram top: 00000000
initcall: 17805d00
initcall: 17805eec
TLB table from ffff0000 to ffff4000
initcall: 17805d18
initcall: 17805ea0
Reserving 712k for U-Boot at: fff3d000
initcall: 17805e70
Reserving 16392k for malloc() at: fef3b000
initcall: 17806040
Reserving 80 Bytes for Board Info at: fef3afb0
initcall: 17805d20
initcall: 17805e3c
Reserving 248 Bytes for Global Data at: fef3aeb8
initcall: 17805dd8
initcall: 17805d34
initcall: 178061d0
initcall: 1780613c
initcall: 17806098
RAM Configuration:
Bank #0: 10000000 3.8 GiB
DRAM: 3.8 GiB
initcall: 17805dbc
New Stack Pointer is: fef3ae90
initcall: 17805d3c
initcall: 17805d6c
Relocation Offset is: e873d000
Relocating to fff3d000, new gd at fef3aeb8, sp at fef3ae90
initcall: fff4321c
initcall: fff433a8
initcall: 17806398 (relocated to fff43398)
dram_bank_mmu_setup: bank: 0
mmu_set_region_dcache_behaviour: start=0x00000000, size=1048575, option=30
mmu_set_region_dcache_behaviour: start=0x00000009, size=262144, option=30
initcall: 17806224 (relocated to fff43224)
initcall: 1780624c (relocated to fff4324c)
initcall: 1780635c (relocated to fff4335c)
Pre-reloc malloc() used 0xd4 bytes (0 KB)
using memory 0xfef3b000-0xfff3d000 for malloc()
initcall: 17806214 (relocated to fff43214)
initcall: 17806348 (relocated to fff43348)
uclass_find_device_by_seq: 0 -1
uclass_find_device_by_seq: 0 0
- -1 -1
- not found
Bound device imx_thermal to root_driver
initcall: 178035d4 (relocated to fff405d4)
initcall: 17819388 (relocated to fff56388)
initcall: 17806338 (relocated to fff43338)
initcall: 178062c0 (relocated to fff432c0)
Now running in RAM - U-Boot at: fff3d000
initcall: 17803650 (relocated to fff40650)
initcall: 17806318 (relocated to fff43318)
fulinux 1 MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2, FSL_SDHC: 3
initcall: 178062dc (relocated to fff432dc)
fulinux initr_env()
fulinux env_relocate()
fulinux dev=-1
fulinux env_relocate_spec
fuliux MMC Device -1 not found
fulinux No MMC card found
Using default environment
I enable "#define DEBUG"
my question is "No MMC card found",What is the reason for this problem,Do you need any other information。
The problem has been bothering me for a week, i need help.
thanks.
Solved! Go to Solution.
Hi Chen
seems you are adding SD1 support in uboot, it is enabled in :
../mx6qsabreauto/mx6qsabreauto.c
please recheck these codes.
Aslo please check signals with oscilloscope.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Chen
seems you are adding SD1 support in uboot, it is enabled in :
../mx6qsabreauto/mx6qsabreauto.c
please recheck these codes.
Aslo please check signals with oscilloscope.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi, it's ok,sd0(emmc) seems like no card detect, so it's wrong when get cd status.