too hih fps in imx8mm

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

too hih fps in imx8mm

820 Views
reyhanehyazdani
Contributor II

Hello everyone,

Our image is built based on boot2qt Yocto and the display output is a LVDS display which is connected to the imx8mm MIPI through SN65DSI84 convertor.

The issue is:

Currently we achieve 180fps while using EGLFS as backend, which is too high and makes our animation moves 3 times faster. If we use Wayland as backend it will be 60fps.

Do you have any idea what should we do to reach to the frame rate of 60fps?

0 Kudos
Reply
2 Replies

814 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello reyhanehyazdani,

You should play with QT_QPA_EGLFS_WIDTH and QT_QPA_EGLFS_HEIGHT and see how much down is your fps, maybe QT_QPA_FB_FORCE_FULLSCREEN.

With wayland the fps will down, I do not know is it going to be a 60fps but you should try.

 

Regards

 

0 Kudos
Reply

799 Views
reyhanehyazdani
Contributor II

Thank you for your reply.

I have done it and set width and height, but no changes.

Actually what is not clear for me is whether the EGLFS in imx8mm boot2qt image is real or emulator?

How can I understand that EGLFS is real?

in /unit_tests/Dispay there is a test regarding vsync: mxc_fb_vsync. When I run this test as its example, I got 180fps as a result. At the same time, E-Bike application is running under boot2qt, which has a feature that shows frame rate. This value is 60fps!! I am realy confused. Which one is correct and why there are two different values?

Thanks

Reyhaneh

0 Kudos
Reply