i.mx8QuadxPlus ,how to compile the emmc firmware downloaded based on UUU in yocto configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx8QuadxPlus ,how to compile the emmc firmware downloaded based on UUU in yocto configuration

ソリューションへジャンプ
1,116件の閲覧回数
783435100
Contributor III

Dear technical support:
    I received the i.mx8QuadxPlus development board, how to compile the emmc firmware downloaded based on UUU in yocto configuration
   I am developing based on imx-yocto-L5.4.47_2.2.0,
   I configure local.conf: UBOOT_CONFIG = "emmc" and imx8qxpmek.conf: UBOOT_CONFIG ?? = "emmc",
  but they have no effect. How to configure and compile correctly What?
  Thank you!

0 件の賞賛
返信
1 解決策
1,100件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi 783435100

 

uboot configurations are described in sect.5.5 U-Boot configuration

i.MX Yocto Project User’s Guide​

seems one can use the same configuration as for sd.

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,101件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi 783435100

 

uboot configurations are described in sect.5.5 U-Boot configuration

i.MX Yocto Project User’s Guide​

seems one can use the same configuration as for sd.

 

Best regards
igor

0 件の賞賛
返信