systemd with ttymxc0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,614件の閲覧回数
kunyichen
Contributor IV

hi,

    I try the below on v3.14.52_v1.1.0qa bsp,

because I need to use connman with WIFI

so add 'systemd' into DISTRO_FEATURES

currently connman work well with WIFI

but I can't use serial console (ttymxc0) to login my system now after add systemd

I have try this systemd for Administrators, Part XVI , but still failed

have anyone can tell me, how to login by ttymxc0?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,913件の閲覧回数
kunyichen
Contributor IV

okay, currently workable when to enable CONFIG_FHANDLE of kernel

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,913件の閲覧回数
kunyichen
Contributor IV

when I booting into system then open a terminal to run below command will work,

systemctl enable serial-getty@ttymxc0.service

but system booting still failed, check boot status

systemctl status serial-getty@ttymxc0.service

will show Active: inactive(dead)

Dependency failed for Serial Getty on ttymxc0

Job serial-getty@ttymxc0.service start failed with result 'dependency'

0 件の賞賛
返信
1,914件の閲覧回数
kunyichen
Contributor IV

okay, currently workable when to enable CONFIG_FHANDLE of kernel

0 件の賞賛
返信