supporting UHS-I in imx6 board by yocto L4.1.15

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

supporting UHS-I in imx6 board by yocto L4.1.15

1,639 Views
qi908542785
Contributor I

Hi,

We are using a Sabresd board (i.MX6Q) with YOCTO 4.1.15 kernel. The host supports UHS-I SDR 50 and 104 modes. However when we plug in a UHS-I SD card to usdhc3, we see that it gets detected as a "High speed device" rather than a 'ultra high speed device'. Browsing through the sources, we found that to for the SD card to work in UHS mode, the host needs to switch to 1.8v from 3.3v.

Looks like Sabresd does not support this voltage level and hence restricts this switch over.

Then, I found the following posts talk about 1.8V SD/MMC.But I failed.

What need to modify the support UHS-I mode,Also need to make some changes in u-boot.Hope to get your help.

supporting SDR104 in imx6 board by yocto

Regards,

QI.

0 Kudos
Reply
4 Replies

924 Views
igorpadykov
NXP Employee
NXP Employee

Hi

Sabresd board has not 1.8V switch, depicted on mentioned link

as AI board schematic. So it does not support SDR104.

For SDR104 testing one can use Sabre AI board which has such switch.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

924 Views
qi908542785
Contributor I

Hi

Our products use Sabresd board,On the basis of Sabresd board, do your own board.

On the basis of Sabresd board,Whether can do some modification on the hardware to support UHS-I mode

Do you have any good ways to make Sabresd board support UHS-I mode?

Best regards

igor

0 Kudos
Reply

924 Views
jan_spurek
NXP Employee
NXP Employee

Hi,

to enable SDR50/SDR104 mode, you need to acces BOOT_CFG1[3:2] and choose either value 10 (SDR50) or 11 (SDR104). Refference manual, page 345. BOOT_CFG1[3:2] can be accesed via EIM_DA2 (BOOT_CFG1[2]) and EIM_DA3  (BOOT_CFG1[3])  pins.

0 Kudos
Reply

924 Views
igorpadykov
NXP Employee
NXP Employee

Hi

please implement on custom board switch which uses Sabre AI board.

Best regards

igor

0 Kudos
Reply