Hello,
I am trying capture a stream from local video and show it to local display as well as want to stream the same on RTMP server.
I am expecting no latency (at least, on a local display).
Issue is when I use streaming to only local it's working fine with below pipe:
gst-launch-1.0 imxv4l2videosrc device=/dev/video1 imx-capture-mode=4 fps-n=30 ! video/x-raw,width=1280,height=720,framerate=30/1 ! timeoverlay ! imxipuvideosink
When I want to stream it to local + rtmp server, I could see lot of latency and frame drops on local as well. Here is the pipeline that I am using:
gst-launch-1.0 imxv4l2videosrc device=/dev/video1 imx-capture-mode=4 fps-n=30 ! video/x-raw,width=1280,height=720,framerate=30/1 ! timeoverlay ! tee name="local" local. ! queue ! imxipuvideosink local. ! queue ! imxipuvideotransform ! imxvpuenc_h264 bitrate=8000 ! h264parse ! flvmux ! rtmpsink location=rtmp://192.168.0.56/live
Any suggestions/clue?
Hi Harshal
seems gstreamer-imx used in the case, it is not supported by nxp, issue can be posted on
gstreamer-imx github page
Issues · Freescale/gstreamer-imx · GitHub
Alternatively one can try nxp plugins using attached Linux Guide sect.7.3.14 RTSP
streaming server, more documentation can be found on
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------