Hi Sir,
I have iMX8M Mini EVK and I am able to run AOSP 9.0 on it.
But after booting when I connect debug port to my laptop and open it using putty then I see lots of unwanted messages
These messages always keeps coming at frequent interval.
It become very annoying while debugging. I want to stop/hide these message but not sure hot to do that.
below is the common message which keep coming -
[11111.056000] healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400 fc=4000000 cc=32 chg=a
[11170.765718] healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400 fc=4000000 cc=32 chg=a
[11171.056032] healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400 fc=4000000 cc=32 chg=a
[11230.765728] healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400 fc=4000000 cc=32 chg=a
[11231.056056] healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400 fc=4000000 cc=32 chg=a
Is there any way i can hide or stop these messages ?
Thanks,
Maneesh
解決済! 解決策の投稿を見る。
As first (easiest) option you can use "dmesg -D" to disable printing messages to console, later you can use "dmesg -E" to enable them back if required.
Also you can tune log level with "dmesg -l"
Hi Victor,
Thanks for your reply.
But on iMX8M mini EVK when I booted AOSP 9.0 and when I checked dmesg --help options
there is no -D or -E flags available.
Also If I try to do sudo or su then it give permission denied or invalid error msg.
Please check the logs which I collected after booting iMX8M Mini EVK ->
NOTE : - I am using iMX8M Mini EVK and running Android AOSP 9.0 provided by NXP
evk_8mm:/ $
evk_8mm:/ $
evk_8mm:/ $ dmesg --help
usage: dmesg [-Cc] [-r|-t|-T] [-n LEVEL] [-s SIZE] [-w]
Print or control the kernel ring buffer.
-C Clear ring buffer without printing
-c Clear ring buffer after printing
-n Set kernel logging LEVEL (1-9)
-r Raw output (with <level markers>)
-S Use syslog(2) rather than /dev/kmsg
-s Show the last SIZE many bytes
-T Show human-readable timestamps
-t Don't print timestamps
-w Keep waiting for more output (aka --follow)
evk_8mm:/ $
[ 131.759090] healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400 fc=4000000 cc=32 chg=a
[ 132.050218] healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400 fc=4000000 cc=32 chg=a
1|evk_8mm:/ $
1|evk_8mm:/ $ su dmesg -C
su: invalid uid/gid 'dmesg'
1|evk_8mm:/ $
1|evk_8mm:/ $ sudo dmesg -C
/system/bin/sh: sudo: not found
127|evk_8mm:/ $
127|evk_8mm:/ $ root
/system/bin/sh: root: not found
127|evk_8mm:/ $ cd /
evk_8mm:/ $
Thanks,
Maneesh
Please try to play with logging level. I mean "-n" option.
Hi Victor Linnik,
I am facing some issue during AOSP OTA and I have already asked this question in this forum
If you can provide any solutions or suggestion then it will be of great help.
Thanks,
Maneesh
Hi Victor Linnik,
Thanks for your suggestions.
It solved my problem.
I did -
evk_8mm:/ $ su
evk_8mm:/ $
evk_8mm:/ $ dmesg -n 1
evk_8mm:/ $
And now I am not receiving any debug messages.
Thanks,
Maneesh