spi: can't get the TX DMA channel, error -517!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

spi: can't get the TX DMA channel, error -517!

4,417件の閲覧回数
mahendrasondaga
Contributor III

Hi.. community 
Hope all are doing well 

I'm dealing with the i.MX6 SOM from variscite 

For the instance, I'm using Yocto BSP hardknott 

My intend is to get the ecspi1 working, and that's how i have configure the kernel as follows 

 

1. Activated all necessary drivers from the menuconfig 
For ex

CONFIG_SPI=y

CONFIG_SPI_MASTER=y

CONFIG_SPI_IMX=y

CONFIG_SPI_IMX_DMA=y



2. configured the device tree source file on the dedicated PADS as follows 

 

&ecspi1 {
	fsl,spi-num-chipselects = <1>;
	cs-gpios = <&gpio4 26 0>;
	pinctrl-names = "default";
	pinctrl-0 = <&pinctrl_ecspi1_1>;
	status = "okay";

        chip1: spidev@0 {
               compatible = "var,spidev";
               spi-max-frequency = <12000000>;
               reg = <0>;
        };
};


	pinctrl_ecspi1_1: ecspi1grp {
		fsl,pins = <
			MX6UL_PAD_CSI_DATA07__ECSPI1_MISO       0x100b1
			MX6UL_PAD_CSI_DATA06__ECSPI1_MOSI       0x100b1
			MX6UL_PAD_CSI_DATA04__ECSPI1_SCLK       0x100b1
			MX6UL_PAD_CSI_DATA05__GPIO4_IO26        0x100b1
		>;
	};

 

3. Installed the imx-sdma firmware with the custom image 
which is appearing in /lib/firmware/imx/sdma directory in my custom image 

CORE_IMAGE_EXTRA_INSTALL += " firmware-imx-sdma"

 

Problem statement 

ecspi not getting activate, as /dev/spi* directory is not populating!

In kernel boot logs, i found some error logs for the SPI, which is mentioned here 

 

[    2.216962] spi_imx 2008000.spi: can't get the TX DMA channel, error -517!
[    3.538836] spi_imx 2008000.spi: can't get the TX DMA channel, error -517!
[    3.558381] spi_imx 2008000.spi: can't get the TX DMA channel, error -517!
[    3.564509] spi_imx 2008000.spi: can't get the TX DMA channel, error -517!


From where,  i got to know that the TX DMA channel is not allocated to SPI

For your reference , i have attached the full kernel boot logs, defconfig file and .dts file 

I need some support from the community 

All suggestions and comments welcome 

 

 

Thanks 

Mahendra Sondagar 

ラベル(3)
0 件の賞賛
21 返答(返信)

4,072件の閲覧回数
mahendrasondaga
Contributor III

Hi.. @kef2 & @Sanket_Parekh 
here is the update from my side

1. verified the menuconfigs settings from my side as follows

 

CONFIG_SPI=y
CONFIG_SPI_MASTER=y
CONFIG_SPI_IMX=y
CONFIG_SPI_IMX_DMA=y
CONFIG_SPI_FSL_LPSPI=y
CONFIG_SPI_FSL_QUADSPI=y
CONFIG_SPI_NXP_FLEXSPI=y
CONFIG_SPI_SPIDEV=y

CONFIG_EXTRA_FIRMWARE="imx/sdma/sdma-imx6q.bin"
CONFIG_EXTRA_FIRMWARE_DIR="/lib/firmware/"

 

2. updated DT by applying the patch to enable the SPI & sdma as follows

 

&ecspi1 {
	fsl,spi-num-chipselects = <1>;
	cs-gpios = <&gpio4 26 0>;
	pinctrl-names = "default";
	pinctrl-0 = <&pinctrl_ecspi1_1>;
	status = "okay";

      spidev@0 {
               compatible = "var,spidev";
               spi-max-frequency = <12000000>;
               reg = <0>;
               status = "okay";
        };



pinctrl_ecspi1_1: ecspi1grp {
		fsl,pins = <
			MX6UL_PAD_CSI_DATA07__ECSPI1_MISO       0x100b1
			MX6UL_PAD_CSI_DATA06__ECSPI1_MOSI       0x100b1
			MX6UL_PAD_CSI_DATA04__ECSPI1_SCLK       0x100b1
			MX6UL_PAD_CSI_DATA05__GPIO4_IO26        0x100b1
		>;
	};


&sdma {
    status = "okay";
};

 

3. After building the images with the above changes and loading with the target, here are the observations

(i) The DMA error gone from the dmesg logs

spi_imx 2008000.spi: can't get the TX DMA channel, error -517!

 
(ii) still  /dev/spi* unable to populate!

(iii) device tree configuration & observations at target board are as follows

root@imx6ul-var-dart:~# find /sys/firmware | grep sdma
/sys/firmware/devicetree/base/soc/bus@2000000/sdma@20ec000
/sys/firmware/devicetree/base/soc/bus@2000000/sdma@20ec000/#dma-cells
/sys/firmware/devicetree/base/soc/bus@2000000/sdma@20ec000/compatible
/sys/firmware/devicetree/base/soc/bus@2000000/sdma@20ec000/clocks
/sys/firmware/devicetree/base/soc/bus@2000000/sdma@20ec000/fsl,sdma-ram-script-name
/sys/firmware/devicetree/base/soc/bus@2000000/sdma@20ec000/clock-names
/sys/firmware/devicetree/base/soc/bus@2000000/sdma@20ec000/interrupts
/sys/firmware/devicetree/base/soc/bus@2000000/sdma@20ec000/phandle
/sys/firmware/devicetree/base/soc/bus@2000000/sdma@20ec000/reg
/sys/firmware/devicetree/base/soc/bus@2000000/sdma@20ec000/name

 

root@imx6ul-var-dart:~# find /sys/firmware | grep spi@2008000/dma
/sys/firmware/devicetree/base/soc/bus@2000000/spba-bus@2000000/spi@2008000/dma-names
/sys/firmware/devicetree/base/soc/bus@2000000/spba-bus@2000000/spi@2008000/dmas

 

 

0 件の賞賛

4,006件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @mahendrasondaga ,

I hope you are doing well.

->It should confirm via the command you shared & if the status is okay then it should be enabled.
->It looks like the initial loading of the SDMA firmware fails. This usually happens when the imx-sdma driver is built into the kernel. Please try building it as a kernel module.
->It may happen because SDMA firmware is outdated, Please make sure to use the latest Linux BSP as it has the latest updated drivers as well as firmware.

I hope it helps!

Thanks & Regards,

Sanket Parekh

0 件の賞賛

3,966件の閲覧回数
mahendrasondaga
Contributor III

Hi.. @Sanket_Parekh 

after activating from the kernel module, it has been loaded

 

root@imx6ul-var-dart:~# dmesg | grep sdma
[    1.339421] imx-sdma 20ec000.sdma: no event needs to be remapped
[    1.339461] imx-sdma 20ec000.sdma: WARN: Device release is not defined so it is not safe to unbind this driver while in use
[    1.345584] imx-sdma 20ec000.sdma: firmware found.
[    1.346064] imx-sdma 20ec000.sdma: loaded firmware 3.5
[    2.245635] imx-sdma 20ec000.sdma: private_candidate: dma0chan0 busy
[    3.281665] imx-sdma 20ec000.sdma: private_candidate: dma0chan0 busy
[    3.281699] imx-sdma 20ec000.sdma: private_candidate: dma0chan1 busy
[    3.282203] imx-sdma 20ec000.sdma: private_candidate: dma0chan0 busy
[    3.282228] imx-sdma 20ec000.sdma: private_candidate: dma0chan1 busy
[    3.282248] imx-sdma 20ec000.sdma: private_candidate: dma0chan2 busy
root@imx6ul-var-dart:~# dmesg | grep spi
[    2.245820] spidev@0 enforce active low on chipselect handle
[    2.252011] spi_imx 2008000.spi: registered master spi0
[    2.252436] spi spi0.0: spi_imx_setup: mode 0, 8 bpw, 12000000 hz
[    2.252479] spi spi0.0: setup mode 0, 8 bits/w, 12000000 Hz max --> 0
[    2.253746] spi_imx 2008000.spi: registered child spi0.0

 

root@imx6ul-var-dart:/dev# spidev_test -D /dev/spidev0.0
spi mode: 0x4
bits per word: 8
max speed: 500000 Hz (500 kHz)

 

Many Thanks @Sanket_Parekh & @kef2 
Appreciate both of you

0 件の賞賛

3,936件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @mahendrasondaga ,

I hope you are doing well.

I'm glad that issue is solved.
Hence can I close this thread?

Thanks & Regards,

Sanket Parekh

0 件の賞賛

3,908件の閲覧回数
mahendrasondaga
Contributor III

yes, you may

0 件の賞賛

3,989件の閲覧回数
mahendrasondaga
Contributor III

Hi.. @Sanket_Parekh 

Thanks, let me try this

0 件の賞賛

4,057件の閲覧回数
kef2
Senior Contributor IV

If you have this

&sdma {
    status = "okay";
};

 then this

find /sys/firmware | grep sdma

should confirm it! I guess you failed to deploy new dtb to target. SDMA driver has to trigger in dmesg message about firmware loading.

0 件の賞賛

3,995件の閲覧回数
mahendrasondaga
Contributor III

Hi.. @kef2 
Yes, you're right
By mistake, i have loaded the older DTB file

here is the update after enabling the sdma

root@imx6ul-var-dart:~# find /sys/firmware | grep sdma
/sys/firmware/devicetree/base/soc/bus@2000000/sdma@20ec000
/sys/firmware/devicetree/base/soc/bus@2000000/sdma@20ec000/#dma-cells
/sys/firmware/devicetree/base/soc/bus@2000000/sdma@20ec000/compatible
/sys/firmware/devicetree/base/soc/bus@2000000/sdma@20ec000/clocks
/sys/firmware/devicetree/base/soc/bus@2000000/sdma@20ec000/fsl,sdma-ram-script-name
/sys/firmware/devicetree/base/soc/bus@2000000/sdma@20ec000/clock-names
/sys/firmware/devicetree/base/soc/bus@2000000/sdma@20ec000/status
/sys/firmware/devicetree/base/soc/bus@2000000/sdma@20ec000/interrupts
/sys/firmware/devicetree/base/soc/bus@2000000/sdma@20ec000/phandle
/sys/firmware/devicetree/base/soc/bus@2000000/sdma@20ec000/reg
/sys/firmware/devicetree/base/soc/bus@2000000/sdma@20ec000/name
root@imx6ul-var-dart:~# 

 

status contents seems to be "okay^@"
Yes, its activated now

root@imx6ul-var-dart:~# find /sys/firmware | grep spi@2008000/dma
/sys/firmware/devicetree/base/soc/bus@2000000/spba-bus@2000000/spi@2008000/dma-names
/sys/firmware/devicetree/base/soc/bus@2000000/spba-bus@2000000/spi@2008000/dmas

 

root@imx6ul-var-dart:~# dmesg | grep sdma                                    
root@imx6ul-var-dart:~# 


Still result remains the same!

root@imx6ul-var-dart:~# dmesg | grep spi 
[    2.222540] spi_imx 2008000.spi: can't get the TX DMA channel, error -517!
[    3.553153] spi_imx 2008000.spi: can't get the TX DMA channel, error -517!
[    3.572671] spi_imx 2008000.spi: can't get the TX DMA channel, error -517!
[    3.578818] spi_imx 2008000.spi: can't get the TX DMA channel, error -517!

 

The complete dmesg logs is attached here

Any suggestions pl. ?

0 件の賞賛

4,209件の閲覧回数
kef2
Senior Contributor IV

Then perhaps SDMA is not enabled in DT. Try adding

 

&sdma {
	status = "okay";
};

 

Or verify what you have after Linux boots:

#  find /sys/firmware | grep sdma

/sys/firmware/devicetree/base/soc/bus@2000000/dma-controller@20ec000/fsl,sdma-ram-script-name

# ls -l /sys/firmware/devicetree/base/soc/bus@2000000/dma-controller@20ec000/
-r--r--r-- 1 root root 4 May 23 07:03 #dma-cells
-r--r--r-- 1 root root 8 May 23 07:03 clock-names
-r--r--r-- 1 root root 16 May 23 07:03 clocks
-r--r--r-- 1 root root 46 May 23 07:03 compatible
-r--r--r-- 1 root root 24 May 23 07:03 fsl,sdma-ram-script-name
-r--r--r-- 1 root root 12 May 23 07:03 interrupts
-r--r--r-- 1 root root 15 May 23 07:03 name
-r--r--r-- 1 root root 4 May 23 07:03 phandle
-r--r--r-- 1 root root 8 May 23 07:03 reg
-r--r--r-- 1 root root 5 May 23 07:03 status

# cat /sys/firmware/devicetree/base/soc/bus@2000000/dma-controller@20ec000/status
okay#

As well check if ecspi1 doesn't miss dmas and dma-names

# find /sys/firmware | grep spi@2008000/dma
/sys/firmware/devicetree/base/soc/bus@2000000/spba-bus@2000000/spi@2008000/dma-names
/sys/firmware/devicetree/base/soc/bus@2000000/spba-bus@2000000/spi@2008000/dmas

# hexdump /sys/firmware/devicetree/base/soc/bus@2000000/spba-bus@2000000/spi@2008000/dmas

0000000 0000 0a00 0000 0300 0000 0700 0000 0100
0000010 0000 0a00 0000 0400 0000 0700 0000 0200
0000020

#  cat /sys/firmware/devicetree/base/soc/bus@2000000/spba-bus@2000000/spi@2008000/dma-names
rxtx#

 

On success you should get this on your iMX6ULL

# dmesg | grep sdma
[ 0.344638] imx-sdma 20ec000.dma-controller: firmware found.
[ 0.344972] imx-sdma 20ec000.dma-controller: loaded firmware 3.5

4,204件の閲覧回数
mahendrasondaga
Contributor III

Hi.. @kef2 
here is the test results 

find /sys/firmware | grep sdma                           
/sys/firmware/devicetree/base/soc/bus@2000000/sdma@20ec000
/sys/firmware/devicetree/base/soc/bus@2000000/sdma@20ec000/#dma-cells
/sys/firmware/devicetree/base/soc/bus@2000000/sdma@20ec000/compatible
/sys/firmware/devicetree/base/soc/bus@2000000/sdma@20ec000/clocks
/sys/firmware/devicetree/base/soc/bus@2000000/sdma@20ec000/fsl,sdma-ram-script-name
/sys/firmware/devicetree/base/soc/bus@2000000/sdma@20ec000/clock-names
/sys/firmware/devicetree/base/soc/bus@2000000/sdma@20ec000/interrupts
/sys/firmware/devicetree/base/soc/bus@2000000/sdma@20ec000/phandle
/sys/firmware/devicetree/base/soc/bus@2000000/sdma@20ec000/reg
/sys/firmware/devicetree/base/soc/bus@2000000/sdma@20ec000/name

 

-r--r--r-- 1 root root  4 Mar 25 08:24 #dma-cells
-r--r--r-- 1 root root  8 Mar 25 08:24 clock-names
-r--r--r-- 1 root root 16 Mar 25 08:24 clocks
-r--r--r-- 1 root root 46 Mar 25 08:24 compatible
-r--r--r-- 1 root root 24 Mar 25 08:24 fsl,sdma-ram-script-name
-r--r--r-- 1 root root 12 Mar 25 08:24 interrupts
-r--r--r-- 1 root root  5 Mar 25 08:24 name
-r--r--r-- 1 root root  4 Mar 25 08:24 phandle
-r--r--r-- 1 root root  8 Mar 25 08:24 reg

 

 

find /sys/firmware | grep spi@2008000/dma
/sys/firmware/devicetree/base/soc/bus@2000000/spba-bus@2000000/spi@2008000/dma-names
/sys/firmware/devicetree/base/soc/bus@2000000/spba-bus@2000000/spi@2008000/dmas

 

root@imx6ul-var-dart:~# dmesg | grep sdma
root@imx6ul-var-dart:~# 


Yes, you're right 
sdma seems not to be activated in DT 

however, my host PC is in trouble
Once, It will  get recover, I'll also verify the DT and update here 

Many Thanks 

0 件の賞賛

4,135件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @mahendrasondaga ,

I hope you are doing well.

->Please make sure to check the sdma-related DT configuration, I have shared an example for reference.

sdma3: dma-controller@30e00000 {
                                compatible = "fsl,imx8mp-sdma", "fsl,imx7d-sdma";
                                reg = <0x30e00000 0x10000>;
                                interrupts = <GIC_SPI 34 IRQ_TYPE_LEVEL_HIGH>;
                                clocks = <&audio_blk_ctrl IMX8MP_CLK_AUDIO_BLK_CTRL_SDMA3_ROOT>,
                                         <&audio_blk_ctrl IMX8MP_CLK_AUDIO_BLK_CTRL_SDMA3_ROOT>;
                                clock-names = "ipg", "ahb";
                                #dma-cells = <3>;
                                fsl,sdma-ram-script-name = "imx/sdma/sdma-imx7d.bin";
                                fsl,ratio-1-1;
                                power-domains = <&audiomix_pd>;
                                status = "okay";
                        };

->One should always set the status to "okay" to enable it.

Please share the observation.

Thanks & Regards,

Sanket Parekh

0 件の賞賛

4,088件の閲覧回数
mahendrasondaga
Contributor III

Hi.. @Sanket_Parekh 

here is the sdma node in my case

You can see, the status property is not written, but i guess it's seems to be activated

 

sdma: sdma@20ec000 {
				compatible = "fsl,imx6ul-sdma", "fsl,imx6q-sdma",
					     "fsl,imx35-sdma";
				reg = <0x020ec000 0x4000>;
				interrupts = <GIC_SPI 2 IRQ_TYPE_LEVEL_HIGH>;
				clocks = <&clks IMX6UL_CLK_IPG>,
					 <&clks IMX6UL_CLK_SDMA>;
				clock-names = "ipg", "ahb";
				#dma-cells = <3>;
				fsl,sdma-ram-script-name = "imx/sdma/sdma-imx6q.bin";
			};

 

 

タグ(1)
0 件の賞賛

4,267件の閲覧回数
mahendrasondaga
Contributor III

Hi.. @kef2 
I have configured the kernel configuration options into the menuconfig as follows 

CONFIG_EXTRA_FIRMWARE="imx/sdma/sdma-imx6q.bin"
CONFIG_EXTRA_FIRMWARE_DIR="/lib/firmware/"

After compiling and installing the target board, I also verified for the same via below command 

zcat /proc/config.gz | grep CONFIG_EXTRA_FIRMWARE
CONFIG_EXTRA_FIRMWARE="imx/sdma/sdma-imx6q.bin"
CONFIG_EXTRA_FIRMWARE_DIR="/lib/firmware/"


However, still, the issue remains the same!
As I believe the sdma-imx6q.bin lies in my /lib/firmware directory of the rootfs  and that's how I have configured CONFIG_EXTRA_FIRMWARE_DIR accordingly 

during the CONFIG_EXTRA_FIRMWARE_DIR="firmware" configuration, and compiling the Makefile unable to finds it!

Any suggestions pl. ?

0 件の賞賛

4,257件の閲覧回数
kef2
Senior Contributor IV

You forgot to provide updated dmesg output

0 件の賞賛

4,214件の閲覧回数
mahendrasondaga
Contributor III

Hi.. @kef2 
pl. find the kernel boot log & dmesg logs file from here 

Thanks 

0 件の賞賛

4,338件の閲覧回数
kef2
Senior Contributor IV

Since you have 'y' for 

 

CONFIG_SPI_IMX=y

 

SDMA as well should be compiled as 'y'. No matter 'y' or 'm', you should see message about loading SDMA FW. Perhaps you have SDMA disabled in kernel. 

So 'y' for SPI_IMX means 'y' for SDMA. 'y' for SDMA means SDMA FW has to be included in kernel as blob. Unless it's done, no matter is there FW in /lib/firmare or not, SDMA will fail.

 

CORE_IMAGE_EXTRA_INSTALL += " firmware-imx-sdma"

 

This seems only instructing Yocto to populate FW in rootfs. It doesn't let FW blob to be attached in zImage. To include FW in zImage, kernel has to be compiled with 

CONFIG_EXTRA_FIRMWARE="imx/sdma/sdma-imx6q.bin"
CONFIG_EXTRA_FIRMWARE_DIR="firmware"

Where FIRMWARE_DIR is path visible to kernel Makefile. It could be either relative or absolute. Above "firmware" is folder in the same path as kernel Makefile. And there's a FW file in firmware/imx/sdma/sdma-imx6q.bin. 

 

CONFIG_EXTRA_FIRMWARE_DIR="firmware"

should be set to /lib/firmware. sdma-*.bin files come populated with host OS, as well with Yocto?

0 件の賞賛

4,309件の閲覧回数
mahendrasondaga
Contributor III

Hi.. @kef2 
Thanks for the feedback 

Yes, i agreed!
That i can also check from the kernel logs as well that kernel is not linking with the sdma drivers as, the directory is missing 

Let me try this remedy

Many Thanks 

0 件の賞賛

4,297件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @mahendrasondaga 

I hope you are doing well.

->One can also check by enabling the below-given macros in the def config.
CONFIG_SPI_FSL_LPSPI=y
CONFIG_SPI_FSL_QUADSPI=y
CONFIG_SPI_NXP_FLEXSPI=y
CONFIG_SPI_SPIDEV=y

->Please also enable the below option also in the kernel configuration.
CONFIG_IMX_SCU=y

Please share the observation.

Thanks & Regards,

Sanket Parekh

0 件の賞賛

4,277件の閲覧回数
mahendrasondaga
Contributor III

Hi.. @Sanket_Parekh 
Thanks , Surely will add it and update it here after testing 

0 件の賞賛

4,271件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @mahendrasondaga ,

I hope you are doing well.

OK, Sure Please share the observation and the updates if any.

Thanks & Regards,

Sanket Parekh

0 件の賞賛