DDR configurations for iMX8M Plus

cancel
Showing results for 
Search instead for 
Did you mean: 

DDR configurations for iMX8M Plus

Jump to solution
527 Views
xueyf
Contributor II

Hi,

I am planning to use Nanya DDR part NT6AN512T32AV with iMx8m plus processor. I have filled the XLS sheet MX8M_Plus_LPDDR4_RPA_v9.xlsx with required details. Can anyone review the configuration and confirm if the filled details are correct.

Tags (1)
0 Kudos
1 Solution
416 Views
xueyf
Contributor II

You're welcome!

I have completed the calibration, but I'm experiencing abnormal behavior with the network interface after calibration.

xueyf_0-1685505622550.png

How can I resolve this issue?

View solution in original post

0 Kudos
5 Replies
498 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @xueyf,

I hope you are doing well.

The below-mentioned parameter needs to be changed in the RPA file for NT6AN512T32AV part.

Density per channel per chip select (Gb)1: 16

Please change Density per channel per chip select to 8Gb.

NT6AN512T32AV is a dual channel DRAM (8 Gb density per channel)

Thanks & Regards,
Dhruvit Vasavada.

0 Kudos
446 Views
xueyf
Contributor II

Thank you for your response.

However, when I press the calibration button, the interface keeps getting stuck at STEP 1. What should I do to resolve this issue?

xueyf_0-1685429363168.png

 

0 Kudos
431 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @xueyf,

I hope you are doing well.

From the RPA file, It seems that the DDR clock frequency is changed from the default configuration.

Please note that RPA file only supports 1500Mhz and 2000Mhz clock frequency 

For frequencies other than these two, it is up to the user to create the appropriate register setting for the desired frequency. (DRAM_PLL_FDIV_CTL0 ).

Please refer to the below document for more information.

iMX 8M Mini Register Programming Aid DRAM PLL setting

Thanks & Regards,
Dhruvit Vasavada

0 Kudos
417 Views
xueyf
Contributor II

You're welcome!

I have completed the calibration, but I'm experiencing abnormal behavior with the network interface after calibration.

xueyf_0-1685505622550.png

How can I resolve this issue?

0 Kudos
397 Views
xueyf
Contributor II
I'm glad to hear that the issue has been resolved!
0 Kudos