Hi again,
I noticed, that my Linux-Installation only recognizes two cpu-cores of the installed i.MX6Q, but I don't know why
Here is the configuration in my Device-Tree (copied from FSL SabreSD)
[CODE]
cpus {
#address-cells = <1>;
#size-cells = <0>;
cpu@0 {
compatible = "arm,cortex-a9";
device_type = "cpu";
reg = <0>;
next-level-cache = <&L2>;
operating-points = <
/* kHz uV */
1200000 1275000
996000 1250000
852000 1250000
792000 1150000
396000 975000
>;
fsl,soc-operating-points = <
/* ARM kHz SOC-PU uV */
1200000 1275000
996000 1250000
852000 1250000
792000 1175000
396000 1175000
>;
clock-latency = ; /* two CLK32 periods */
clocks = <&clks IMX6QDL_CLK_ARM>,
<&clks IMX6QDL_CLK_PLL2_PFD2_396M>,
<&clks IMX6QDL_CLK_STEP>,
<&clks IMX6QDL_CLK_PLL1_SW>,
<&clks IMX6QDL_CLK_PLL1_SYS>;
clock-names = "arm", "pll2_pfd2_396m", "step",
"pll1_sw", "pll1_sys";
arm-supply = <®_arm>;
pu-supply = <®_pu>;
soc-supply = <®_soc>;
};
cpu@1 {
compatible = "arm,cortex-a9";
device_type = "cpu";
reg = ;
next-level-cache = <&L2>;
};
cpu@2 {
compatible = "arm,cortex-a9";
device_type = "cpu";
reg = ;
next-level-cache = <&L2>;
};
cpu@3 {
compatible = "arm,cortex-a9";
device_type = "cpu";
reg = ;
next-level-cache = <&L2>;
};
}; [/CODE]
Why does Linux see only two cores?
已解决! 转到解答。
Well, I'm very sorry to say that, but it was a hardware-failure. The Voltage supply was configured for a i.MX6D. By this way, two of the Cores weren't able to start.
I fixed it, and now we have the foll Quad-Core Performance.
Again, sorry for that.
Well, I'm very sorry to say that, but it was a hardware-failure. The Voltage supply was configured for a i.MX6D. By this way, two of the Cores weren't able to start.
I fixed it, and now we have the foll Quad-Core Performance.
Again, sorry for that.
Hi Steffen
Is it possible that you might have set the number
of CPUs to only 2 in while configuring the kernel.
You might want to verify that CONFIG_NR_CPUS is 4.
Hope this helps
Sinan Akman
Hello Steffen,
It is weird that you’re not seeing all four cores if these are set on the kernel configuration and the device tree. Which machine configuration did you use in Yocto and what kernel version are you using? Perhaps you can attach the defconfig file as well.