shorten pins

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

shorten pins

903 Views
sapirbuz
Contributor IV

Hi,

MIMXRT1051CVL5B.

We want to support Jtag (bit-bang) and UART (dedicated), which will be routed from the NXP MCU to the same connector in our design. The user will choose by FW, on the fly, the interface he wants to use- UART/Jtag.

We will do HW shorts from the NXP Jtag pins to the NXP UART pins (see picture below):

GPIO_EMC_17 (UART CTS) will be shorten to GPIO_EMC_16 (bit-bang Jtag DO)

GPIO_EMC_18 (UART RTS) will be shorten to GPIO_EMC_15 (bit-bang Jtag DI)

GPIO_EMC_19 (UART TX) will be shortened to GPIO_EMC_13 (bit-bang Jtag Clk)

GPIO_EMC_20 (UART RX) will be shorten to GPIO_EMC_27 (bit-bang Jtag SS)

 

Is it possible to support that function in the NXP MCU? Do you see any constraint to keeping that? Will the pin that is not in use affect the pin that is used? 

For example, when we use GPIO_EMC_17, migth GPIO_EMC_16 affect the GPIO_EMC_17 interface?

sapirbuz_0-1655558279214.png

 

0 Kudos
Reply
4 Replies

874 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is it possible to support that function in the NXP MCU? Do you see any constraint to keeping that? Will the pin that is not in use affect the pin that is used?
-- To be honest, I'm not 100% sure, as the pin that is not in use definitely affects the pin that is used, as every pin has its electrical attribution configuration, further, I'm confused with the above Jtag pins, they shouldn't work as the JTAG pins actually.

jeremyzhou_0-1655791290771.png


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

870 Views
sapirbuz
Contributor IV

Hi,

The JTAG we will use is not the dedicated Jtag, it is GPIO pins that will act as Jtag using bit bang.

Can you please ask someone who knows the answer to this ticket?

0 Kudos
Reply

860 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
After discussing with my co-workers, we both think the short-connected pins will affect each other, even if one is not used, as every pin has its electrical attribution configuration.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

889 Views
sapirbuz
Contributor IV

kindly reminder

0 Kudos
Reply