setting repo

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

setting repo

4,012 次查看
zhangbaobing
Contributor II

pastedImage_1.png

I do it as up following,but always fault,

i wander why.

标签 (1)
标记 (1)
0 项奖励
32 回复数

2,815 次查看
iris_wen
NXP Employee
NXP Employee

Please try the following steps:

1. Save the attachment in ~/bin

2. $ chmod a+x ~/bin/repo

3. Add the following line to the ~/.bashrc file

   export PATH=~/bin:$PATH

4.$ source ~/.bashrc

0 项奖励

2,815 次查看
zhangbaobing
Contributor II

pastedImage_1.png

Executeing this instruction which is fault

pastedImage_2.png

so the back instructon still fault.

0 项奖励

2,815 次查看
iris_wen
NXP Employee
NXP Employee

Do you really follow the steps I provided? 

The first step is to save the attachment in ~/bin. Then the repo is already in your computer. You don't need to download again.

Remember to unzip the attachment...ONLY copy the file repo in ~/bin...

0 项奖励

2,810 次查看
zhangbaobing
Contributor II

first ,what is attachment?

pastedImage_1.png

0 项奖励

2,810 次查看
zhangbaobing
Contributor II

where is the attachment?

and can you give me specfications ?

0 项奖励

2,810 次查看
zhangbaobing
Contributor II

pastedImage_1.png

pastedImage_2.png

pastedImage_3.png

0 项奖励

2,810 次查看
joanxie
NXP TechSupport
NXP TechSupport

maybe you can refer to the link as below, get the repo from tsinghua

"https://mirrors.tuna.tsinghua.edu.cn/help/git-rep"

I suggest that you can update to the latest version, some packages in the git.freescale.com are removed, if you build the 3.14.28, maybe you will get the connection error even if you can repo sync successfully, I have built 4.14.52 successfully before, but I don't know if you can get 3.14.28 source package or not

0 项奖励

2,810 次查看
zhangbaobing
Contributor II

pastedImage_1.png

0 项奖励

2,810 次查看
joanxie
NXP TechSupport
NXP TechSupport
0 项奖励

2,810 次查看
zhangbaobing
Contributor II

pastedImage_1.png

i download L4.1.15 still fault

0 项奖励

2,810 次查看
zhangbaobing
Contributor II

pastedImage_1.png

0 项奖励

2,810 次查看
joanxie
NXP TechSupport
NXP TechSupport

as I mentioned before, the source code was removed from git.freescale.com, maybe you can refer to my another document

https://community.nxp.com/docs/DOC-346089 

0 项奖励

2,810 次查看
zhangbaobing
Contributor II

still fault

pastedImage_1.png

0 项奖励

2,810 次查看
joanxie
NXP TechSupport
NXP TechSupport

do you mind reading my document again? as I mentioned,  you couldn't use git.freescale.com, try to use the new command as my document mentions

0 项奖励

2,810 次查看
zhangbaobing
Contributor II

pastedImage_1.pngstill fault

0 项奖励

2,810 次查看
joanxie
NXP TechSupport
NXP TechSupport

I don't find any error according to the pic you attached

0 项奖励

2,815 次查看
iris_wen
NXP Employee
NXP Employee

Hi Baobing,

Did you reboot or source the .bashrc file by the following command? 

$ source ~/.bashrc

0 项奖励

2,815 次查看
iris_wen
NXP Employee
NXP Employee

If the instruction in user guide is not detailed enough, please follow this link.

https://blog.csdn.net/xuanwolanxue/article/details/104678027?ops_request_misc=%257B%2522request%255F...

0 项奖励

2,815 次查看
zhangbaobing
Contributor II

hi ,that is still false

0 项奖励

2,815 次查看
iris_wen
NXP Employee
NXP Employee

Could you please share the log?

0 项奖励