salve-spi ss Interrupt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

salve-spi ss Interrupt

907件の閲覧回数
leihe
Contributor I

            hello,I have a problem,I need Interrupt signal to tell me when the data  transmission is complete ,my machine is a slave spi device,so master control when the transmission is over,I want's to check chip select Interrupt,I can't find it,is it exists in imx6D?

thank you!

ラベル(4)
タグ(2)
0 件の賞賛
返信
3 返答(返信)

761件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi lei he,

You can look at chapters 21.4.6 Interrupts and 21.7.5 Interrupt Control Register (ECSPIx_INTREG) in IMX6D Reference Manual


Regards,
Carlos
NXP Technical Support

0 件の賞賛
返信

761件の閲覧回数
leihe
Contributor I

thankyou

0 件の賞賛
返信

761件の閲覧回数
leihe
Contributor I

if i set the bit of sion,can I use gpio interrupt?

0 件の賞賛
返信