rootfs with vivante support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

rootfs with vivante support

2,668 Views
srinivasaporam
Contributor II

Hi,

We have got imx6Q reference board for which we have cross compiled kernel.

We are able to boot to ubuntu with this board but X is giving error that not able to load 'vivante'.

We are using ubuntu-core-14.04.02-core.armhf.tar.gz (rootfs). When we are checking for vivante.so in (./usr/lib/ or ./usr/lib/xorg etc..) vivante driver support files are not there. How to get rootfs which has got vivante support or how i can make this rootfs to have vivante????

Labels (3)
0 Kudos
Reply
2 Replies

1,877 Views
igorpadykov
NXP Employee
NXP Employee

Hi Srinivasa

vivante drivers are : gpu-viv-bin-mx6q-xx, xserver-xorg-video-imx-viv-xx

http://downloads.yoctoproject.org/mirror/sources/kernel-module-imx-gpu-viv-5.0.11.p7.1.tar.gz

http://downloads.yoctoproject.org/mirror/sources/xserver-xorg-video-imx-viv-5.0.11.p7.1.tar.gz

https://community.freescale.com/thread/327339

https://community.freescale.com/thread/376320

http://downloads.yoctoproject.org/mirror/sources/

http://patches.openembedded.org/patch/104949/

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,877 Views
srinivasaporam
Contributor II

Hi Igor,

Can you please explain me how to build these and deploy to the target machine.

We already cross-compiled 3.10.53 or 3.14.14 and board is booting to ubuntu14.04. Now from above links i have got

1.kernel-module-imx-gpu-viv-5.0.11.p7.1.tar.gz

2. xserver-xorg-video-imx-viv-5.0.11.p7.1.tar.gz

is there any document that explains installing above ?????

0 Kudos
Reply