Hi, i need your help with the board i have "SABRE Board for Smart Devices", Part Numbers: MCIMX6Q-SDB.
so, i can boot Linux with using the files from here:
i.MX6 Q/D/DL/S L3.0.35_4.0.0 GA release
more exactly:
* u-boot is: "u-boot-mx6q-sabresd.bin" from L3.0.35_4.0.0_130424_images_MX6.tar.gz
* kernel is: "uImage" from L3.0.35_4.0.0_130424_images_MX6.tar.gz
* rootfs is: rootfs.ext2 from L3.0.35_4.0.0_130424_images_MX6.tar.gz
but it seems there is no HDMI output - on dmesg the only relevant messages i can find are:
mxc_hdmi mxc_hdmi: Read EDID again
mxc_hdmi mxc_hdmi: No modes read from edid
mxc_hdmi mxc_hdmi: create default modelist
so, the only thing from defaults that i changed is the following u-boot settings:
bootargs_mmc=setenv bootargs ${bootargs} ip=none root=/dev/mmcblk1p1 rootwait video=mxcfb0:dev=hdmi,1280x720M@60,if=RGB24 video=mxcfb1:off
i tried with using "1920x1080M@60" too, but with the exact same result. however, any other device i have with HDMI output works connected to the that same HDMI input that is not working with "SABRE Board for Smart Devices", Part Numbers: MCIMX6Q-SDB. so, what's wrong?
thank you,
Stefan