"failed to set clk" and "Kernel panic"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

"failed to set clk" and "Kernel panic"

1,922 Views
weisheng
Contributor III

we use a board copy by freescale sabre-sdl board,when boot the kernel,I meet the error below,I have try to chanded pll2_pfd2_594m to pll2_pfd2_396m or 352, or set maxcpus=1 (nosmp) in kernel (by the way ,how to set the two args correctery by detail? I use setenv nosmp 0)args, I am very confused !someone please help me out! thanks !

U-Boot 2015.04 (Oct 23 2015 - 15:25:09)

CPU:   Freescale i.MX6SOLO rev1.2 at 792 MHz

CPU:   Temperature 39 C

Reset cause: POR

Board: MX6-SabreSD

I2C:   ready

DRAM:  1 GiB

PMIC:  PFUZE100 ID=0x10

MMC:   MMC/SD: Reset never completed.

voltage not supported by controller

FSL_SDHC: 0

*** Warning - bad CRC, using default environment

No panel detected: default to QIMEI-SWVGA

Display: QIMEI-SWVGA (800x600)

In:    serial

Out:   serial

Err:   serial

check_and_clean: reg 0, flag_set 0

Fastboot: Normal

flash target is MMC:0

Net:   FEC [PRIME]

Error: FEC address not set.

Normal Boot

Hit any key to stop autoboot:  0

booti mmc0

kernel   @ 10808000 (6819528)

ramdisk  @ 11800000 (725616)

fdt      @ 11700000 (32597)

kernel cmdline:

        use boot.img command line:

        console=ttymxc0,115200 init=/init rw video=mxcfb0 vmalloc=400M androidboot.serialno=1822a9d4df668b47

switch to ldo_bypass mode!

   Using Device Tree in place at 11700000, end 1170af54

Starting kernel ...

Booting Linux on physical CPU 0x0

Initializing cgroup subsys cpu

Initializing cgroup subsys cpuacct

Linux version 3.10.53-88204-g4f0dd92-dirty (weiss@ubuntu) (gcc version 4.6.x-google 20120106 (prerelease) (GCC) ) #1 SMP PREEMPT Tue Oct 27 17:36:57 CST 2015

CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d

CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache

Machine: Freescale i.MX6 Quad/DualLite (Device Tree), model: Freescale i.MX6 DualLite SABRE Smart Device Board

cma: CMA: reserved 256 MiB at 3a000000

Memory policy: ECC disabled, Data cache writealloc

PERCPU: Embedded 8 pages/cpu @820c3000 s9728 r8192 d14848 u32768

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 259840

Kernel command line: console=ttymxc0,115200 init=/init rw video=mxcfb0 vmalloc=400M androidboot.serialno=1822a9d4df668b47

PID hash table entries: 4096 (order: 2, 16384 bytes)

Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)

Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)

Memory: 959MB 64MB = 1023MB total

Memory: 758744k/758744k available, 289832k reserved, 0K highmem

Virtual kernel memory layout:

    vector  : 0xffff0000 - 0xffff1000   (   4 kB)

    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

    vmalloc : 0xc0800000 - 0xff000000   (1000 MB)

    lowmem  : 0x80000000 - 0xc0000000   (1024 MB)

    pkmap   : 0x7fe00000 - 0x80000000   (   2 MB)

    modules : 0x7f000000 - 0x7fe00000   (  14 MB)

      .text : 0x80008000 - 0x80e7a48c   (14794 kB)

      .init : 0x80e7b000 - 0x80ed0600   ( 342 kB)

      .data : 0x80ed2000 - 0x80f56000   ( 528 kB)

       .bss : 0x80f56000 - 0x80feacf8   ( 596 kB)

SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1

Preemptible hierarchical RCU implementation.

        RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1.

NR_IRQS:16 nr_irqs:16 16

L310 cache controller enabled

l2x0: 16 ways, CACHE_ID 0x410000c8, AUX_CTRL 0x32050000, Cache size: 524288 B

failed to set parent of clk gpu3d_shader_sel to pll2_pfd2_396m: -22

sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms

CPU identified as i.MX6DL, silicon rev 1.2

Console: colour dummy device 80x30

Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)

pid_max: default: 32768 minimum: 301

Security Framework initialized

SELinux:  Initializing.

Mount-cache hash table entries: 512

Initializing cgroup subsys debug

Initializing cgroup subsys freezer

CPU: Testing write buffer coherency: ok

CPU0: thread -1, cpu 0, socket 0, mpidr 80000000

Setting up static identity map for 0x807e23e8 - 0x807e2440

Brought up 1 CPUs

SMP: Total of 1 processors activated (1581.05 BogoMIPS).

CPU: All CPU(s) started in SVC mode.

devtmpfs: initialized

pinctrl core: initialized pinctrl subsystem

regulator-dummy: no parameters

NET: Registered protocol family 16

DMA: preallocated 256 KiB pool for atomic coherent allocations

Use WDOG2 as reset source

syscon 20c8000.anatop: regmap [mem 0x020c8000-0x020c8fff] registered

vdd1p1: 800 <--> 1375 mV at 1100 mV

vdd3p0: 2800 <--> 3150 mV at 3000 mV

vdd2p5: 2000 <--> 2750 mV at 2400 mV

vddarm: 725 <--> 1450 mV

vddpu: 725 <--> 1450 mV

vddsoc: 725 <--> 1450 mV

syscon 20e0000.iomuxc-gpr: regmap [mem 0x020e0000-0x020e0037] registered

syscon 21bc000.ocotp-ctrl: regmap [mem 0x021bc000-0x021bffff] registered

hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.

hw-breakpoint: maximum watchpoint size is 4 bytes.

imx6dl-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver

bio: create slab <bio-0> at 0

mxs-dma 110000.dma-apbh: initialized

usb_otg_vbus: 5000 mV

usb_h1_vbus: 5000 mV

mipi_dsi_pwr_on: no parameters

i2c-core: driver [max17135] using legacy suspend method

i2c-core: driver [max17135] using legacy resume method

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

i2c i2c-0: IMX I2C adapter registered

i2c i2c-1: IMX I2C adapter registered

Linux video capture interface: v2.00

pps_core: LinuxPPS API ver. 1 registered

pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>

PTP clock support registered

imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 driver probed

mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 dphy version is 0x3130302a

MIPI CSI2 driver module loaded

Advanced Linux Sound Architecture Driver Initialized.

Bluetooth: Core ver 2.16

NET: Registered protocol family 31

Bluetooth: HCI device and connection manager initialized

Bluetooth: HCI socket layer initialized

Bluetooth: L2CAP socket layer initialized

Bluetooth: SCO socket layer initialized

imx-gpc 20dc000.gpc: failed to get clk!

imx-gpc: probe of 20dc000.gpc failed with error -2

Switching to clocksource mxc_timer1

NET: Registered protocol family 2

TCP established hash table entries: 8192 (order: 4, 65536 bytes)

TCP bind hash table entries: 8192 (order: 4, 65536 bytes)

TCP: Hash tables configured (established 8192 bind 8192)

TCP: reno registered

UDP hash table entries: 512 (order: 2, 16384 bytes)

UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)

NET: Registered protocol family 1

RPC: Registered named UNIX socket transport module.

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

RPC: Registered tcp NFSv4.1 backchannel transport module.

Trying to unpack rootfs image as initramfs...

Freeing initrd memory: 708K (81800000 - 818b1000)

hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available

of_clk_src_onecell_get: invalid clock index 245

ERROR: could not get clock /soc/busfreq:axi_alt_sel(10)

imx6_busfreq busfreq.13: busfreq_probe: failed to get axi_alt_sel_clk

imx6_busfreq: probe of busfreq.13 failed with error -2

Bus freq driver module loaded

futex hash table entries: 256 (order: 2, 16384 bytes)

audit: initializing netlink socket (disabled)

type=2000 audit(0.270:1): initialized

VFS: Disk quotas dquot_6.5.2

Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)

NFS: Registering the id_resolver key type

Key type id_resolver registered

Key type id_legacy registered

NTFS driver 2.1.30 [Flags: R/W DEBUG].

jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.

fuse init (API version 7.22)

msgmni has been set to 1995

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

imx-weim 21b8000.weim: WEIM driver registered.

pwm-backlight backlight.18: invalid default brightness level: 16, using 7

mxc_mipi_dsi 21e0000.mipi: failed to reset: -2

mxc_mipi_dsi: probe of 21e0000.mipi failed with error -2

MIPI DSI driver module loaded

mxc_sdc_fb fb.16: registered mxc display driver lcd

Console: switching to colour frame buffer device 100x30

imx_epdc_fb 20f4000.epdc: can't get/select pinctrl

imx-sdma 20ec000.sdma: no iram assigned, using external mem

imx-sdma 20ec000.sdma: initialized

imx-sdma 20ec000.sdma: loaded firmware 1.1

pfuze100-regulator 1-0008: Full lay: 2, Metal lay: 1

pfuze100-regulator 1-0008: FAB: 0, FIN: 0

pfuze100-regulator 1-0008: pfuze100 found.

SW1AB: 300 <--> 1875 mV at 1175 mV

SW1C: 300 <--> 1875 mV at 1175 mV

SW2: 800 <--> 3300 mV at 3300 mV

SW3A: 400 <--> 1975 mV at 1500 mV

SW3B: 400 <--> 1975 mV at 1500 mV

SW4: 800 <--> 3300 mV at 3150 mV

SWBST: 5000 <--> 5150 mV at 5000 mV

VSNVS: 1000 <--> 3000 mV at 3000 mV

VREFDDR: 750 mV

VGEN1: 800 <--> 1550 mV at 1500 mV

VGEN2: 800 <--> 1550 mV at 1500 mV

VGEN3: 1800 <--> 3300 mV at 2800 mV

VGEN4: 1800 <--> 3300 mV at 1800 mV

VGEN5: 1800 <--> 3300 mV at 3000 mV

VGEN6: 1800 <--> 3300 mV at 3300 mV

Serial: IMX driver

2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX

console [ttymxc0] enabled

serial: Freescale lpuart driver

imx sema4 driver is registered.

[drm] Initialized drm 1.1.0 20060810

[drm] Initialized vivante 1.0.0 20120216 on minor 0

brd: module loaded

loop: module loaded

of_dma_request_slave_channel: dma-names property missing or empty

spi_imx 2008000.ecspi: cannot get the TX DMA channel!

spi_imx 2008000.ecspi: dma setup error,use pio instead

spi_imx 2008000.ecspi: probed

tun: Universal TUN/TAP device driver, 1.6

tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>

CAN device driver interface

fec 2188000.ethernet (unregistered net_device): Invalid MAC address: 00:00:00:00:00:00

fec 2188000.ethernet (unregistered net_device): Using random MAC address: f6:20:f9:fd:78:7d

libphy: fec_enet_mii_bus: probed

fec 2188000.ethernet eth0: registered PHC device 0

PPP generic driver version 2.4.2

PPP BSD Compression module registered

PPP Deflate Compression module registered

PPP MPPE Compression module registered

NET: Registered protocol family 24

usbcore: registered new interface driver asix

usbcore: registered new interface driver ax88179_178a

usbcore: registered new interface driver cdc_ether

usbcore: registered new interface driver net1080

usbcore: registered new interface driver cdc_subset

usbcore: registered new interface driver zaurus

usbcore: registered new interface driver cdc_ncm

ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

usbcore: registered new interface driver cdc_acm

cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters

usbcore: registered new interface driver usb-storage

usbcore: registered new interface driver usbserial

usbcore: registered new interface driver option

usbserial: USB Serial support registered for GSM modem (1-port)

ci_hdrc ci_hdrc.1: doesn't support gadget

ci_hdrc ci_hdrc.1: EHCI Host Controller

ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1

ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00

usb usb1: New USB device found, idVendor=1d6b, idProduct=0002

usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1

usb usb1: Product: EHCI Host Controller

usb usb1: Manufacturer: Linux 3.10.53-88204-g4f0dd92-dirty ehci_hcd

usb usb1: SerialNumber: ci_hdrc.1

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

mousedev: PS/2 mouse device common for all mice

usbcore: registered new interface driver xpad

usbcore: registered new interface driver usb_acecad

usbcore: registered new interface driver aiptek

usbcore: registered new interface driver gtco

usbcore: registered new interface driver hanwang

usbcore: registered new interface driver kbtab

usbcore: registered new interface driver wacom

i2c-core: driver [isl29023] using legacy suspend method

i2c-core: driver [isl29023] using legacy resume method

snvs_rtc 20cc034.snvs-rtc-lp: rtc core: registered 20cc034.snvs-rtc-lp as rtc0

i2c /dev entries driver

usbcore: registered new interface driver uvcvideo

USB Video Class driver (1.1.1)

gspca_main: v2.14.0 registered

imx2-wdt 20c0000.wdog: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=0)

device-mapper: uevent: version 1.0.3

device-mapper: ioctl: 4.24.0-ioctl (2013-01-15) initialised: dm-devel@redhat.com

Bluetooth: Virtual HCI driver ver 1.3

Bluetooth: HCI UART driver ver 2.2

Bluetooth: HCIATH3K protocol initialized

usbcore: registered new interface driver btusb

cpuidle: using governor ladder

cpuidle: using governor menu

sdhci: Secure Digital Host Controller Interface driver

sdhci: Copyright(c) Pierre Ossman

sdhci-pltfm: SDHCI platform and OF driver helper

mmc1: no vqmmc regulator found

mmc1: no vmmc regulator found

mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA

mmc3: no vqmmc regulator found

mmc3: no vmmc regulator found

mmc3: SDHCI controller on 219c000.usdhc [219c000.usdhc] using ADMA

mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed

mmc1: host does not support reading read-only switch. assuming write-enable.

mxc_asrc 2034000.asrc: failed to get asrck clock

mxc_asrc: probe of 2034000.asrc failed with error -2

mxc_vpu 2040000.vpu: failed to get vpu power

of_clk_src_onecell_get: invalid clock index 248

mmc1: new high speed SDHC card at address e624

ERROR: could not get clock /soc/aips-bus@02100000/caam@2100000:caam_ipg(2)

mmcblk1: mmc1:e624 SU08G 7.40 GiB

caam 2100000.caam: can't identify CAAM ipg clk: -2

Unable to handle kernel NULL pointer dereference at virtual address 00000004

pgd = 80004000

[00000004] *pgd=00000000

Internal error: Oops: 805 [#1] PREEMPT SMP ARM

Modules linked in:

CPU: 0 PID: 1 Comm: swapper/0 Not tainted 3.10.53-88204-g4f0dd92-dirty #1

task: bc06c000 ti: bc06a000 task.ti: bc06a000

PC is at caam_sm_startup+0x68/0x2a4

LR is at caam_sm_startup+0x68/0x2a4

pc : [<805d9468>]    lr : [<805d9468>]    psr: a0000113

sp : bc06bef8  ip : 00000073  fp : 00000000

r10: 0000016f  r9 : 80ecd680  r8 : bc476210

r7 : 80eaf6b0  r6 : bc0e0610  r5 : 00000000  r4 : bc40f780

r3 : bc48ed80  r2 : 00000000  r1 : bc40f780  r0 : 00000000

Flags: NzCv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment kernel

Control: 10c53c7d  Table: 1000404a  DAC: 00000015

PC: 0x805d93e8:

93e8  e1a0a000 eaffff65 80ee1e44 80fb27c0 80ee3af8 80dd9680 e92d4ff8 e2806010

9408  e1a00006 ebf761f2 e59f327c e30810d0 e1a05000 e5930008 ebec01f5 e2504000

9428  0a000094 e3a00000 e59f2260 e1a01000 e5846000 eb00ae0c e59f1254 e1a02006

9448  eb00b895 e3500000 0a000086 e2808010 e5840008 e1a01004 e1a00008 ebf76205

9468  e5858004 e5953010 e5932fd8 f57ff04f e7e53852 e2833001 e5843044 e5953010

9488  e5932fd8 f57ff04f e7e33652 e2833001 e5843048 e5953010 e5932fd8 f57ff04f

94a8  e202303f e2833001 e584304c e5953010 e5932fdc f57ff04f e7e23852 e3a02b01

94c8  e1a03312 e5843050 e3a03080 e5843054 e5953008 e5930000 e2800010 e5840004

LR: 0x805d93e8:

93e8  e1a0a000 eaffff65 80ee1e44 80fb27c0 80ee3af8 80dd9680 e92d4ff8 e2806010

9408  e1a00006 ebf761f2 e59f327c e30810d0 e1a05000 e5930008 ebec01f5 e2504000

9428  0a000094 e3a00000 e59f2260 e1a01000 e5846000 eb00ae0c e59f1254 e1a02006

9448  eb00b895 e3500000 0a000086 e2808010 e5840008 e1a01004 e1a00008 ebf76205

9468  e5858004 e5953010 e5932fd8 f57ff04f e7e53852 e2833001 e5843044 e5953010

9488  e5932fd8 f57ff04f e7e33652 e2833001 e5843048 e5953010 e5932fd8 f57ff04f

94a8  e202303f e2833001 e584304c e5953010 e5932fdc f57ff04f e7e23852 e3a02b01

94c8  e1a03312 e5843050 e3a03080 e5843054 e5953008 e5930000 e2800010 e5840004

SP: 0xbc06be78:

be78  803ae98c 807d3c9c 00000000 807e1de0 bc0e1180 807d3d6c 00000000 807e1b54

be98  bc476210 805d9468 a0000113 ffffffff bc06bee4 8000dc58 00000000 bc40f780

beb8  00000000 bc48ed80 bc40f780 00000000 bc0e0610 80eaf6b0 bc476210 80ecd680

bed8  0000016f 00000000 00000073 bc06bef8 805d9468 805d9468 a0000113 ffffffff

bef8  80812a00 80f56000 bc06a000 80ec2250 80eaf6b0 00000000 80ecd680 0000016f

bf18  00000000 80eaf6f4 00000000 800086ec 00000001 00000003 00000000 ffffffed

bf38  820c0dff 80049394 80db4f38 80e388ec 00000006 00000006 80ee922c 80ec2270

bf58  00000006 80ec2250 80f56000 80e7b428 80ecd680 0000016f 00000000 80e7bb8c

R1: 0xbc40f700:

f700  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

f720  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

f740  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

f760  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

f780  bc0e0610 00000000 bc476200 00000000 00000000 00000000 00000000 00000000

f7a0  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

f7c0  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

f7e0  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

R3: 0xbc48ed00:

ed00  bc478840 bc044140 bc48ea04 bc04414c bc044140 80f03844 bc4788c0 00000001

ed20  00000007 00000000 bc48ed28 bc48ed28 00000000 00000000 bc02f670 bc02f674

ed40  bc48ea3c 00000001 00000000 80f36f28 00000000 00000000 00000000 00000000

ed60  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

ed80  00000000 bc48ed84 bc48ed84 803ae98c 803ae9d4 bc0e1180 bc0e1184 bc0e1184

eda0  00000001 00000000 00000000 00000000 00000000 bc02f65c bc02f660 bc4565b8

edc0  00000001 bc48edc4 bc48edc4 bc40f780 bc476210 00000000 00000000 00000000

ede0  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

R4: 0xbc40f700:

f700  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

f720  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

f740  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

f760  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

f780  bc0e0610 00000000 bc476200 00000000 00000000 00000000 00000000 00000000

f7a0  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

f7c0  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

f7e0  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

R6: 0xbc0e0590:

0590  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

05b0  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

05d0  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

05f0  00000000 00000000 00000000 00000000 bc0e2340 ffffffff 00000000 00000000

0610  bc0e0410 bc0e1180 bc0e2340 bc0e081c bc0e041c bc0e0418 bc0413c0 80f037a0

0630  bc0e23c0 00000009 00000007 00000000 00000000 00000001 00000000 bc0e064c

0650  bc0e064c 00000000 00000000 80f03900 00000000 00000000 00000000 00000020

0670  00030003 bc0e0874 bc0e0474 7fffffff 00010001 bc0e0684 bc0e0684 00000000

R7: 0x80eaf630:

f630  e1a00005 e3a03001 e1a02102 e12fff3c e3a03000 e1a00004 e1a01003 e58430ac

f650  e58430a8 ebe4b7fa e1a00004 e3a01001 ebe4b7f7 e1a00005 e59f1038 ebd3ff61

f670  e59f0034 e28dd008 e8bd4070 ead39687 e3e00012 e28dd008 e8bd8070 80dd9520

f690  80dd9530 80fc9590 80dd95d0 80ee3af8 80ee1e44 80fb27c0 80dd9634 80f392f0

f6b0  e3a00000 e59f2048 e1a01000 e92d4008 ebdd556b e2501000 1a000004 e59f2034

f6d0  ebdd5567 e2501000 03e00012 08bd8008 e1a00001 ebdd5e69 e3500000 0a000002

f6f0  ebdca742 e3a00000 e8bd8008 e3e00012 e8bd8008 80dd9520 80dd9530 e3a00000

f710  e59f2048 e1a01000 e92d4008 ebdd5554 e2501000 1a000004 e59f2034 ebdd5550

R8: 0xbc476190:

6190  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

61b0  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

61d0  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

61f0  00000000 00000000 00000000 00000000 bc478a00 ffffffff 00000000 00000000

6210  bc0e0610 bc48ed80 bc478a00 bc0413c0 bc487c74 bc0e0618 bc0413c0 80f037a0

6230  bc478a80 00000003 00000007 00000000 00000000 00000001 00000000 bc47624c

6250  bc47624c 00000000 00000000 80f03900 00000000 00000000 00000000 00000020

6270  00010001 80f03eec bc487ccc 7fffffff 00010001 bc476284 bc476284 00000000

R9: 0x80ecd600:

d600  80eae314 80eae38c 80eae3bc 80eae3e4 80eae4fc 80eae618 80eae700 80eae70c

d620  80eae718 80eae724 80eae730 80eae88c 80eae8fc 80eae908 80eae9b8 80eaea34

d640  80eaea58 80eaea70 80eaea7c 80eaec34 80eaec60 80eaec6c 80eaece4 80eaede8

d660  80eaedf4 80eaee00 80eaee48 80eaee54 80eaee78 80eaf27c 80eaf49c 80eaf6b0

d680  80eaf70c 80eaf768 80eaf774 80eaf9d8 80eafb08 80eafb14 80eafb2c 80eafb44

d6a0  80eafb5c 80eafb74 80eafb8c 80eafba4 80eafbbc 80eafbd4 80eafbec 80eafc04

d6c0  80eafc1c 80eafc34 80eafc4c 80eafc64 80eafc7c 80eafc94 80eafcac 80eafcc4

d6e0  80eafcdc 80eafcf4 80eafd74 80eafd8c 80eafda4 80eafdbc 80eafdd4 80eafdec

Process swapper/0 (pid: 1, stack limit = 0xbc06a238)

Stack: (0xbc06bef8 to 0xbc06c000)

bee0:                                                       80812a00 80f56000

bf00: bc06a000 80ec2250 80eaf6b0 00000000 80ecd680 0000016f 00000000 80eaf6f4

bf20: 00000000 800086ec 00000001 00000003 00000000 ffffffed 820c0dff 80049394

bf40: 80db4f38 80e388ec 00000006 00000006 80ee922c 80ec2270 00000006 80ec2250

bf60: 80f56000 80e7b428 80ecd680 0000016f 00000000 80e7bb8c 00000006 00000006

bf80: 80e7b428 80053d90 00000000 807d42b0 00000000 00000000 00000000 00000000

bfa0: 00000000 807d42b8 00000000 8000e158 00000000 00000000 00000000 00000000

bfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

bfe0: 00000000 00000000 00000000 00000000 00000013 00000000 c719ef0f c62de1af

[<805d9468>] (caam_sm_startup+0x68/0x2a4) from [<80eaf6f4>] (caam_sm_init+0x44/0x5c)

[<80eaf6f4>] (caam_sm_init+0x44/0x5c) from [<800086ec>] (do_one_initcall+0xf4/0x154)

[<800086ec>] (do_one_initcall+0xf4/0x154) from [<80e7bb8c>] (kernel_init_freeable+0xfc/0x1c8)

[<80e7bb8c>] (kernel_init_freeable+0xfc/0x1c8) from [<807d42b8>] (kernel_init+0x8/0xe4)

[<807d42b8>] (kernel_init+0x8/0xe4) from [<8000e158>] (ret_from_fork+0x14/0x3c)

Code: e5840008 e1a01004 e1a00008 ebf76205 (e5858004)

usb 1-1: new high-speed USB device number 2 using ci_hdrc

---[ end trace d1fbb8c760753e8c ]---

Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b

Rebooting in 5 seconds..

mxc_restart: Watchdog reset failed to assert reset

0 Kudos
Reply
1 Reply

1,135 Views
igorpadykov
NXP Employee
NXP Employee

Hi wei

seems this image was built for wrong proccesor, please check

attached Yocto Guide sect.5.2 Machine Configurations for

"imx6solosabresd" configuration and use appropriate dtb/dts files.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply