I use the imx8qm-mek board and use the rear_view_camera demo in M4 core:
1. Can I change this demo run on M4-core0? I modify the cmakelist but it doesn't work
2. I use board->lvds->it6263->hdmi monitor to display the demo, but I find that after the function APP_InitDisplay called there will be almost 1 second before the nxp logo display on the monitor, I didn't find where this time is consumed in the code, why this take so long?
Thank you!
Hi,
I need some info from your side,
which display connector you are using?
Currently, I am using IMX-LVDS-HDMI ( LVDS to HDMI adaptor card (mini SAS)) and display itself not up in M4.
Do I needs to do any configuration in M4 SDK side (source/vendor/nxp/mcu-sdk-auto/SDK_MEK-MIMX8QM/boards/mekmimx8qm/demo_apps/rear_view_camera) ?
Thanks & Regards,
VinothS,
Hi,
Did your connector is it6263?
Hi Xu Ji ,
Will you please share your RVC cold boot images ?
RVC Cold Boot,
Thanks & Regards,
VInoth S,
Hi Xu hi,
view camera demo is working (Needs to connect HDMI Monitor at J8 connector of LVDS Port as per schematic (SPF-29420_C2.pdf) instead of J7 Connector.)
Thank You,
Vinoth S,