problem building L2.6.35_11.09.01_ER_source

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

problem building L2.6.35_11.09.01_ER_source

Jump to solution
1,557 Views
andrebella
Contributor III

I been trying to build the LTIB but I'm getting this error, it does not tell me much it happens right after I run ./ltib

rpmdb: --force-debian: unknown option

Died at ./ltib line 2340.

traceback:

main::setup_rpmdb:2340

  main::check_rpm_setup:2403

   main::host_checks:1423

    main:542

Started: Mon Oct  8 16:39:53 2012

Ended:   Mon Oct  8 16:39:54 2012

Elapsed: 1 seconds

Build Failed


Labels (1)
0 Kudos
Reply
1 Solution
885 Views
andrebella
Contributor III

I just read it, I found the solution to the error here [ltib] Diff of /ltib/ltib

I'm using ubuntu 12.04, but I dont think this linux image builder has support for it yet, I'm still getting more errors, I will post more solutions if I can find them.

View solution in original post

0 Kudos
Reply
2 Replies
885 Views
RandyKrakora
NXP Employee
NXP Employee

Are you building under Ubuntu? What version?

Did you look here yet?:

https://community.freescale.com/docs/DOC-1442

-Randy

0 Kudos
Reply
886 Views
andrebella
Contributor III

I just read it, I found the solution to the error here [ltib] Diff of /ltib/ltib

I'm using ubuntu 12.04, but I dont think this linux image builder has support for it yet, I'm still getting more errors, I will post more solutions if I can find them.

0 Kudos
Reply