Now I want to design a pad using imx6 solox based on the official development board with Peripherals such as wifi, bluetooth, GPS, PCIE, CAMERA.and 10.1 inch LCD .How do I calculate the power consumption to choose the right lithium battery?
Hi zhang
one can look at sect.4.1.5 Maximum Supply Currents i.MX6SX Datasheet
https://www.nxp.com/docs/en/data-sheet/IMX6SXCEC.pdf
and AN5050 i.MX6SX Power Consumption
https://www.nxp.com/docs/en/application-note/AN5050.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Is there a power consumption calculation tool that I can use? I still need to add the power consumption of the SSD, the power consumption of the wifi module, the power consumption of the Bluetooth module, the power consumption of the LCD liquid crystal, and other peripheral devices.right?
>Is there a power consumption calculation tool that I can use?
no.
Best regards
igor