Hello,
My current version:
Release: android_p11.0.0_2.6.0
Board: i.MX8MQ based custom board
I need to port wm8960 to Android system.
In the Android system, I can play audio files normally with tinyplay:
#tinyplay tinghai-zhanghuimei. wav
I can also use tinycap to record files normally, and the recorded files play normally:
#tinycap /data/rec.wav -D 0 -d 0 –c 2 –r 48000 –b 16 –p 1024 –n 3 -T 10
When I integrated wm8960 into Android, I noticed the following two points according to the description of 8.2.2 supporting a new sound card in 《android_user's_guide.pdf-rev. android-11.0.0_2.6.0-7 January 2022》:
Add the contents in the above red box and turn off the wm8524 sound card
wm8960_config.json file is an original configuration file in the official source code. It has not been modified. The contents of the file are as follows:
I have not made any changes to this file. It is still the official configuration for wm8524.
The current situation is:
When I set the Android volume: settings->sound->medium Volume I can hear the prompt tone of the system, but when I set the volume, the volume progress bar keeps bouncing, as if the volume setting was unsuccessful. And I can't play music through the KuGou music APK.
My question:
1. How to replace the sound card wm8524 with wm8960 and port it to Android 11.0.0? Do I need to modify the device/nxp/imx8m/evk_ 8mq/audio_policy_configuration.xml?
2. If I want to play music in the KuGou music APK, in addition to adding wm8960_rpmsg_config.json, what changes need to be made?
Attachment 1 is a log that the volume progress bar keeps bouncing when the system volume is modified
Attachment 2 is the log when playing music with kugou apk
Looking forward to your reply.
I'm facing the same issue!!
Does your issue got solved?
if yes, then please tell how to play audio through media player application.