I have a RM3 board from bluechip technologies. I've been able to port u-boot and kernel to it, using the boundary devices android builds as a guide. I am using the boundary devices android filesystem images as well with my modified kernel. When booting android 4.0.4, I get the following error:
init: property (null) has no value for writing to /sys/class/android_usb/android0/iManufacturer
init: property (null) has no value for writing to /sys/class/android_usb/android0/iProduct
init: cannot find '/system/bin/sh', disabling 'console'
init: cannot find '/system/bin/servicemanager', disabling 'servicemanager'
init: cannot find '/system/bin/vold', disabling 'vold'
init: cannot find '/system/bin/gpu_init.sh', disabling 'gpu_init'
init: cannot find '/system/bin/netd', disabling 'netd'
init: cannot find '/system/bin/dispd', disabling 'dispd'
init: cannot find '/system/bin/debuggerd', disabling 'debuggerd'
init: cannot find '/system/bin/surfaceflinger', disabling 'surfaceflinger'
init: cannot find '/system/bin/app_process', disabling 'zygote'
init: cannot find '/system/bin/drmserver', disabling 'drm'
init: cannot find '/system/bin/mediaserver', disabling 'media'
init: cannot find '/system/bin/dbus-daemon', disabling 'dbus'
init: cannot find '/system/bin/installd', disabling 'installd'
init: cannot find '/system/etc/install-recovery.sh', disabling 'flash_recovery'
init: cannot find '/system/bin/keystore', disabling 'keystore'
init: cannot find '/system/bin/rild', disabling 'ril-daemon'
init: cannot find '/system/bin/sh', disabling 'console'
From reading online in the forums, it seems I may not be loading the filesystem correctly. Can anyone please guide me on how to tackle this problem?
Here is the full bootlog (note: even though it says Sabre Lite in many places, this is really the RM3 board. I have tweaked u-boot and kernel to accommodate for the RM3):
U-Boot 2009.08-dirty (Jun 28 2014 - 20:32:38)
CPU: Freescale i.MX6 family TO1.2 at 792 MHz
Temperature: 47 C, calibration data 0x5704c47d
mx6q pll1: 792MHz
mx6q pll2: 528MHz
mx6q pll3: 480MHz
mx6q pll8: 50MHz
ipg clock : 66000000Hz
ipg per clock : 66000000Hz
uart clock : 80000000Hz
cspi clock : 60000000Hz
ahb clock : 132000000Hz
axi clock : 264000000Hz
emi_slow clock: 29333333Hz
ddr clock : 528000000Hz
usdhc1 clock : 198000000Hz
usdhc2 clock : 198000000Hz
usdhc3 clock : 198000000Hz
usdhc4 clock : 198000000Hz
nfc clock : 24000000Hz
Board: MX6Q-SABRELITE:[ POR]
Boot Device: NOR
I2C: ready
DRAM: 1 GB
MMC: FSL_USDHC: 0,FSL_USDHC: 1
JEDEC ID: 0xbf:0x25:0x8e
Reading SPI NOR flash 0xc0000 [0x2000 bytes] -> ram 0x27600a18
SUCCESS
In: serial
Out: serial
Err: serial
Net: got MAC address from IIM: 00:c0:46:00:88:f1
FEC0 [PRIME]
Hit any key to stop autoboot: 0
MX6Q SABRELITE U-Boot > mmc dev 0
mmc0 is current device
MX6Q SABRELITE U-Boot > mmc rescan; fatload mmc 0:1 ${loadaddr} uImage && fatload mmc 0:1 12800000 uramdisk.img && bootm 10800000 12800000
reading uImage
4354968 bytes read
reading uramdisk.img
213592 bytes read
## Booting kernel from Legacy Image at 10800000 ...
Image Name: Linux-3.0.35-gb8823c8-dirty
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 4354904 Bytes = 4.2 MB
Load Address: 10008000
Entry Point: 10008000
Verifying Checksum ... OK
## Loading init Ramdisk from Legacy Image at 12800000 ...
Image Name: Initial Ram Disk
Image Type: ARM Linux RAMDisk Image (gzip compressed)
Data Size: 213528 Bytes = 208.5 kB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Initializing cgroup subsys cpuset
Initializing cgroup subsys cpu
Linux version 3.0.35-gb8823c8-dirty (ashwin@ashwin1) (gcc version 4.7.1 20120531 (prerelease) (crosstool-NG linaro-1.13.1-2012.06-20120625 - Linaro GCC 2012.06) ) #13 SMP PREEMPT Sun J
un 29 20:00:55 EDT 2014
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: Freescale i.MX 6Quad Sabre-Lite Board
Memory policy: ECC disabled, Data cache writealloc
CPU identified as i.MX6Q, silicon rev 1.2
PERCPU: Embedded 7 pages/cpu @c1174000 s5760 r8192 d14720 u32768
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 210944
Kernel command line: enable_wait_mode=off console=ttymxc0,115200 vmalloc=400M consoleblank=0 video=mxcfb0:dev=lcd,DTECH,if=RGB666 fbmem=10M androidboot.bootdev=sdhci-esdhc-imx.0 androi
dboot.hardware=freescale androidboot.console=ttymxc0
PID hash table entries: 2048 (order: 1, 8192 bytes)
Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
Memory: 576MB 256MB = 832MB total
Memory: 833424k/833424k available, 215152k reserved, 442368K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
DMA : 0xfbe00000 - 0xffe00000 ( 64 MB)
vmalloc : 0xd9800000 - 0xf2000000 ( 392 MB)
lowmem : 0xc0000000 - 0xd9000000 ( 400 MB)
pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
.init : 0xc0008000 - 0xc0041000 ( 228 kB)
.text : 0xc0041000 - 0xc07cf458 (7738 kB)
.data : 0xc07d0000 - 0xc083a060 ( 425 kB)
.bss : 0xc083a084 - 0xc096a820 (1218 kB)
Preemptible hierarchical RCU implementation.
NR_IRQS:624
MXC GPIO hardware
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms
MXC_Early serial console at MMIO 0x2020000 (options '115200')
bootconsole [ttymxc0] enabled
Console: colour dummy device 80x30
Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512
Initializing cgroup subsys cpuacct
CPU: Testing write buffer coherency: ok
hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
CPU1: Booted secondary processor
Brought up 2 CPUs
SMP: Total of 2 processors activated (3162.11 BogoMIPS).
print_constraints: dummy:
NET: Registered protocol family 16
print_constraints: vddpu: 725 <--> 1300 mV at 1150 mV fast normal
print_constraints: vddcore: 725 <--> 1300 mV at 1150 mV fast normal
print_constraints: vddsoc: 725 <--> 1300 mV at 1200 mV fast normal
print_constraints: vdd2p5: 2000 <--> 2775 mV at 2400 mV fast normal
print_constraints: vdd1p1: 800 <--> 1400 mV at 1100 mV fast normal
print_constraints: vdd3p0: 2625 <--> 3400 mV at 3000 mV fast normal
------------ Board type Sabre Lite
imx_add_mxc_pwm:pdata= (null)
imx_add_mxc_pwm:pdata= (null)
imx_add_mxc_pwm:pdata= (null)
imx_add_mxc_pwm:pdata= (null)
hw-breakpoint: found 6 breakpoint and 1 watchpoint registers.
hw-breakpoint: 1 breakpoint(s) reserved for watchpoint single-step.
hw-breakpoint: maximum watchpoint size is 4 bytes.
L310 cache controller enabled
l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x02070000, Cache size: 1048576 B
IMX usb wakeup probe
bio: create slab <bio-0> at 0
print_constraints: VDDA: 2500 mV
print_constraints: VDDIO: 3300 mV
machine_constraints_voltage: VDDD: unsupportable voltage constraints
reg-fixed-voltage reg-fixed-voltage.2: Failed to register regulator: -22
reg-fixed-voltage: probe of reg-fixed-voltage.2 failed with error -22
print_constraints: vmmc: 3300 mV
vgaarb: loaded
SCSI subsystem initialized
spi_imx imx6q-ecspi.0: probed
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
Freescale USB OTG Driver loaded, $Revision: 1.55 $
add wake up source irq 75
imx-ipuv3 imx-ipuv3.0: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
imx-ipuv3 imx-ipuv3.1: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
mxc_mipi_csi2 mxc_mipi_csi2: i.MX MIPI CSI2 driver probed
mxc_mipi_csi2 mxc_mipi_csi2: i.MX MIPI CSI2 dphy version is 0x3130302a
MIPI CSI2 driver module loaded
Advanced Linux Sound Architecture Driver Version 1.0.24.
Bluetooth: Core ver 2.16
NET: Registered protocol family 31
Bluetooth: HCI device and connection manager initialized
Bluetooth: HCI socket layer initialized
Bluetooth: L2CAP socket layer initialized
Bluetooth: SCO socket layer initialized
cfg80211: Calling CRDA to update world regulatory domain
i2c-core: driver [max17135] using legacy suspend method
i2c-core: driver [max17135] using legacy resume method
Switching to clocksource mxc_timer1
NET: Registered protocol family 2
IP route cache hash table entries: 16384 (order: 4, 65536 bytes)
TCP established hash table entries: 65536 (order: 7, 524288 bytes)
TCP bind hash table entries: 65536 (order: 7, 786432 bytes)
TCP: Hash tables configured (established 65536 bind 65536)
TCP reno registered
UDP hash table entries: 256 (order: 1, 8192 bytes)
UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Unpacking initramfs...
Freeing initrd memory: 208K
Static Power Management for Freescale i.MX6
wait mode is disabled for i.MX6
cpaddr = d9880000 suspend_iram_base=d9918000
PM driver module loaded
IMX usb wakeup probe
i.MXC CPU frequency driver
highmem bounce pool size: 64 pages
ashmem: initialized
JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
msgmni has been set to 764
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
pwm_config: pwm freq = 32786, clk_select=2 clock_rate=6000000
pwm_config: pwm freq = 20000, clk_select=2 clock_rate=6000000
MIPI DSI driver module loaded
mxc_sdc_fb mxc_sdc_fb.0: register mxc display driver lcd
pwm_config: pwm freq = 32786, clk_select=2 clock_rate=6000000
pwm_config: pwm freq = 20000, clk_select=2 clock_rate=6000000
mxc_sdc_fb mxc_sdc_fb.1: register mxc display driver lcd
mxc_sdc_fb mxc_sdc_fb.1: ipu0-di0 already in use
mxc_sdc_fb: probe of mxc_sdc_fb.1 failed with error -16
mxc_sdc_fb mxc_sdc_fb.2: register mxc display driver ldb
_regulator_get: get() with no identifier
imx-ipuv3 imx-ipuv3.1: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)
pwm_config: pwm freq = 32786, clk_select=2 clock_rate=6000000
pwm_config: pwm freq = 20000, clk_select=2 clock_rate=6000000
mxc_sdc_fb mxc_sdc_fb.3: register mxc display driver ldb
pwm_config: pwm freq = 32786, clk_select=2 clock_rate=6000000
pwm_config: pwm freq = 20000, clk_select=2 clock_rate=6000000
imx-sdma imx-sdma: loaded firmware 1.1
imx-sdma imx-sdma: initialized
Serial: IMX driver
imx-uart.0: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX
console [ttymxc0] enabled, bootconsole disabled
console [ttymxc0] enabled, bootconsole disabled
imx-uart.1: ttymxc1 at MMIO 0x21e8000 (irq = 59) is a IMX
loop: module loaded
Can't recover from RESET HBA!
No sata disk.
m25p80 spi0.0: found sst25vf080b, expected sst25vf016b
m25p80 spi0.0: sst25vf080b (1024 Kbytes)
Creating 3 MTD partitions on "m25p80":
0x000000000000-0x0000000c0000 : "bootloader"
0x0000000c0000-0x0000000c2000 : "ubparams"
0x0000000c2000-0x000000100000 : "unused"
vcan: Virtual CAN interface driver
CAN device driver interface
flexcan netdevice driver
FEC Ethernet Driver
fec_enet_mii_bus: probed
PPP generic driver version 2.4.2
PPP Deflate Compression module registered
PPP BSD Compression module registered
PPP MPPE Compression module registered
NET: Registered protocol family 24
PPTP driver version 0.8.5
tun: Universal TUN/TAP device driver, 1.6
tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1
fsl-ehci fsl-ehci.0: irq 75, io base 0x02184000
fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
add wake up source irq 72
fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 2
fsl-ehci fsl-ehci.1: irq 72, io base 0x02184200
fsl-ehci fsl-ehci.1: USB 2.0 started, EHCI 1.00
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
usbcore: registered new interface driver cdc_acm
cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
usbcore: registered new interface driver usbserial
usbserial: USB Serial Driver core
USB Serial support registered for GSM modem (1-port)
usbcore: registered new interface driver option
option: v0.7.2:USB Driver for GSM modems
USB Serial support registered for Qualcomm USB modem
usbcore: registered new interface driver qcserial
ARC USBOTG Device Controller driver (1 August 2005)
android_usb gadget: Mass Storage Function, version: 2009/09/11
android_usb gadget: Number of LUNs=1
lun0: LUN: removable file: (no medium)
Gadget Android: controller 'fsl-usb2-udc' not recognized
android_usb gadget: android_usb ready
Suspend udc for OTG auto detect
fsl-usb2-udc: bind to driver android_usb
mousedev: PS/2 mouse device common for all mice
input: gpio-keys as /devices/platform/gpio-keys/input/input0
tsc2004_prepare_for_reading: write_cmd -5
tsc2004: probe of 2-0048 failed with error -5
egalax_ts 2-0004: egalax_ts: failed to read firmware version
egalax_ts: probe of 2-0004 failed with error -5
ft5x06-ts 2-0038: ft5x06: Could not detect touch screen.
ft5x06: Jun 28 2014
i2c-core: driver [isl29023] using legacy suspend method
i2c-core: driver [isl29023] using legacy resume method
using rtc device, snvs_rtc, for alarms
snvs_rtc snvs_rtc.0: rtc core: registered snvs_rtc as rtc0
i2c /dev entries driver
Linux video capture interface: v2.00
ov5642_read_reg:write reg error:reg=300a
ov5642_probe:cannot find camera
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video16
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video17
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video18
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video19
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video20
usbcore: registered new interface driver uvcvideo
usb 2-1: new high speed USB device number 2 using fsl-ehci
USB Video Class driver (v1.1.0)
i2c-core: driver [mag3110] using legacy suspend method
android_work: did not send uevent (0 0 (null))
i2c-core: driver [mag3110] using legacy resume method
imx2-wdt imx2-wdt.0: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=1)
Bluetooth: HCI UART driver ver 2.2
Bluetooth: HCILL protocol initialized
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
mmc0: no vmmc regulator found
mmc0: SDHCI controller on platform [sdhci-esdhc-imx.0] using DMA
sdhci sdhci-esdhc-imx.2: no write-protect pin available!
sdhci sdhci-esdhc-imx.2: no card-detect pin available!
mmc1: SDHCI controller on platform [sdhci-esdhc-imx.2] using DMA
mxc_vdoa mxc_vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
VPU initialized
mxc_asrc registered
revserved_memory_account:viv_gpu registerd
anatop_thermal anatop_thermal.0: fuse data: 0x5704c47d
Thermal calibration data is 0x5704c47d
anatop_thermal_counting_ratio: raw25c=1392 raw_hot=1220 hot_temp=125
android_work: sent uevent USB_STATE=CONNECTED
android_work: sent uevent USB_STATE=DISCONNECTED
Anatop Thermal registered as thermal_zone0
anatop_thermal_probe: default cooling device is cpufreq!
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
logger: created 256K log 'log_main'
logger: created 256K log 'log_events'
logger: created 256K log 'log_radio'
logger: created 256K log 'log_system'
usbcore: registered new interface driver snd-usb-audio
mxc_hdmi_soc mxc_hdmi_soc.0: MXC HDMI Audio
imx-hdmi-soc-dai: probe of imx-hdmi-soc-dai.0 failed with error -12
sgtl5000 0-000a: Failed to get supply 'VDDD': -19
print_constraints: 0-000a: 850 <--> 1600 mV at 1200 mV normal
sgtl5000 0-000a: Device with ID register 0 is not a sgtl5000
sgtl5000 0-000a: asoc: failed to probe CODEC sgtl5000.0-000a: -19
asoc: failed to instantiate card sgtl5000-audio: -19
ALSA device list:
No soundcards found.
Netfilter messages via NETLINK v0.30.
nf_conntrack version 0.5.0 (13025 buckets, 52100 max)
ctnetlink v0.93: registering with nfnetlink.
mmc0: new high speed SDHC card at address aaaa
NF_TPROXY: Transparent proxy support initialized, version 4.1.0
NF_TPROXY: Copyright (c) 2006-2007 BalaBit IT Ltd.
mmcblk0: mmc0:aaaa SL16G 14.8 GiB (ro)
xt_time: kernel timezone is -0000
IPv4 over IPv4 tunneling driver
GRE over IPv4 demultiplexor driver
ip_tables: (C) 2000-2006 Netfilter Core Team
arp_tables: (C) 2002 David S. Miller
TCP cubic registered
NET: Registered protocol family 10
mmcblk0: p1 p2 p3 < p5 p6 p7 p8 p9 > p4
ip6_tables: (C) 2000-2006 Netfilter Core Team
IPv6 over IPv4 tunneling driver
NET: Registered protocol family 17
NET: Registered protocol family 15
can: controller area network core (rev 20090105 abi 8)
android_work: sent uevent USB_STATE=CONNECTED
NET: Registered protocol family 29
can: raw protocol (rev 20090105)
can: broadcast manager protocol (rev 20090105 t)
android_work: sent uevent USB_STATE=DISCONNECTED
Bluetooth: RFCOMM TTY layer initialized
Bluetooth: RFCOMM socket layer initialized
Bluetooth: RFCOMM ver 1.11
Bluetooth: BNEP (Ethernet Emulation) ver 1.3
Bluetooth: BNEP filters: protocol multicast
Bluetooth: HIDP (Human Interface Emulation) ver 1.2
L2TP core driver, V2.0
PPPoL2TP kernel driver, V2.0
L2TP IP encapsulation support (L2TPv3)
L2TP netlink interface
L2TP ethernet pseudowire support (L2TPv3)
lib80211: common routines for IEEE802.11 drivers
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
Bus freq driver module loaded
Bus freq driver Enabled
mxc_dvfs_core_probe
DVFS driver module loaded
regulator_init_complete: VDDIO: incomplete constraints, leaving on
regulator_init_complete: VDDA: incomplete constraints, leaving on
snvs_rtc snvs_rtc.0: setting system clock to 1970-01-01 00:00:00 UTC (0)
Freeing init memory: 228K
init (1): /proc/1/oom_adj is deprecated, please use /proc/1/oom_score_adj instead.
android_work: sent uevent USB_STATE=CONNECTED
android_work: sent uevent USB_STATE=DISCONNECTED
usb 2-1: device not accepting address 2, error -71
usb 2-1: new high speed USB device number 3 using fsl-ehci
android_work: sent uevent USB_STATE=CONNECTED
init: cannot open '/initlogo.rle'
init: command 'loglevel' r=0
init: command 'export' r=0
init: command 'export' r=0
init: command 'export' r=0
init: command 'export' r=0
init: command 'export' r=0
init: command 'export' r=0
init: command 'export' r=0
init: command 'export' r=0
init: command 'export' r=0
init: command 'export' r=0
init: command 'export' r=0
init: command 'export' r=0
init: command 'export' r=0
init: command 'export' r=0
init: command 'export' r=0
init: command 'export' r=0
init: command 'export' r=0
init: command 'export' r=0
init: command 'export' r=0
init: command 'symlink' r=0
init: command 'symlink' r=0
init: command 'symlink' r=0
hub 2-1:1.0: USB hub found
init: command 'mkdir' r=0
hub 2-1:1.0: 2 ports detected
init: command 'mount' r=0
init: command 'mkdir' r=0
init: command 'mkdir' r=0
init: command 'symlink' r=0
init: command 'mkdir' r=0
init: command 'symlink' r=0
init: command 'mkdir' r=0
init: command 'symlink' r=0
init: command 'mkdir' r=0
init: command 'mkdir' r=0
init: command 'mkdir' r=0
init: command 'mkdir' r=0
init: command 'mkdir' r=0
init: command 'mkdir' r=0
init: command 'mkdir' r=0
init: command 'mkdir' r=0
init: command 'mkdir' r=0
init: command 'mount' r=0
init: command 'mkdir' r=0
init: command 'mount' r=0
init: command 'mkdir' r=0
init: command 'mount' r=0
init: command 'write' r=0
init: command 'write' r=-2
init: command 'write' r=0
init: command 'write' r=-2
init: command 'write' r=-2
init: command 'write' r=-2
init: command 'write' r=0
init: command 'write' r=0
init: command 'mkdir' r=0
init: command 'mount' r=0
init: command 'chown' r=0
init: command 'chown' r=0
init: command 'chmod' r=0
init: command 'write' r=-22
init: command 'mkdir' r=0
init: command 'chown' r=0
init: command 'chmod' r=0
init: command 'write' r=0
init: command 'mkdir' r=0
init: command 'chown' r=0
init: command 'chmod' r=0
init: command 'write' r=0
init: command 'chmod' r=0
init: processing action 0x31fe0 (fs)
init: command 'mount' r=-1
init: command 'mount' r=0
init: command 'mount' r=-1
init: command 'mkdir' r=0
init: command 'mount' r=-1
init: executing '/sbin/ts_calibrator'
init: executed '/sbin/ts_calibrator' done
init: command 'exec' r=0
init: processing action 0x2b080 (post-fs)
init: command 'mount' r=0
init: command 'chown' r=-30
init: command 'chmod' r=-30
init: command 'chown' r=-2
init: command 'chmod' r=-2
init: command 'chown' r=0
init: command 'chmod' r=0
init: command 'chown' r=0
init: command 'chmod' r=0
init: command 'chown' r=0
init: command 'chmod' r=0
init: command 'mkdir' r=-30
init: processing action 0x2b2a0 (post-fs-data)
init: command 'chown' r=0
init: command 'chmod' r=0
init: command 'mkdir' r=0
init: command 'copy' r=-1
init: command 'chown' r=-2
init: command 'chmod' r=-2
init: command 'copy' r=-1
init: command 'chown' r=-2
init: command 'chmod' r=-2
init: command 'write' r=-2
init: command 'mkdir' r=0
init: command 'mkdir' r=0
init: command 'mkdir' r=0
init: command 'mkdir' r=0
init: command 'mkdir' r=0
init: command 'mkdir' r=0
init: command 'mkdir' r=0
init: command 'mkdir' r=0
init: command 'chmod' r=0
init: command 'chmod' r=-2
init: command 'chmod' r=-2
init: command 'chmod' r=-2
init: command 'mkdir' r=0
init: command 'mkdir' r=0
init: command 'mkdir' r=0
init: command 'mkdir' r=0
init: command 'mkdir' r=0
init: command 'mkdir' r=0
init: command 'mkdir' r=0
init: command 'mkdir' r=0
init: command 'mkdir' r=0
init: command 'chmod' r=0
init: command 'mkdir' r=0
init: command 'mkdir' r=0
init: command 'chown' r=0
init: command 'chmod' r=0
init: command 'mkdir' r=0
init: command 'mkdir' r=0
init: command 'chown' r=0
init: command 'chmod' r=0
init: command 'chown' r=0
init: command 'chmod' r=0
init: processing action 0x32438 (property_service_init)
init: Created socket '/dev/socket/property_service' with mode '666', user '0', group '0'
init: command 'property_service_init' r=0
init: processing action 0x32480 (signal_init)
init: command 'signal_init' r=0
init: processing action 0x324c8 (check_startup)
init: command 'check_startup' r=0
init: processing action 0x2ba10 (boot)
init: command 'ifup' r=0
init: command 'hostname' r=0
init: command 'domainname' r=0
init: command 'setrlimit' r=0
init: command 'write' r=0
init: command 'write' r=0
init: command 'chown' r=0
init: command 'chmod' r=0
init: command 'chown' r=0
init: command 'chmod' r=0
init: command 'write' r=0
init: command 'write' r=0
init: command 'write' r=0
init: command 'chown' r=-2
init: command 'chown' r=-2
init: command 'chown' r=-2
init: command 'chown' r=-2
init: command 'chown' r=-2
init: command 'chown' r=0
init: command 'chown' r=0
init: command 'chown' r=0
init: command 'chmod' r=0
init: command 'chmod' r=0
init: command 'chmod' r=0
init: command 'chown' r=-2
init: command 'chown' r=-2
init: command 'chown' r=-2
init: command 'chown' r=-2
init: command 'chown' r=-2
init: command 'chown' r=-2
init: command 'chown' r=-2
init: command 'chown' r=-2
init: command 'chown' r=-2
init: command 'chown' r=-2
init: command 'chown' r=-2
init: command 'chown' r=-2
init: command 'chown' r=-2
init: command 'chown' r=-2
init: command 'chown' r=-2
init: command 'chown' r=-2
init: command 'chown' r=-2
init: command 'chown' r=-2
init: command 'chown' r=-2
init: command 'chown' r=0
init: command 'chown' r=0
init: command 'chown' r=0
init: command 'chown' r=0
init: command 'chown' r=0
init: command 'chown' r=0
init: command 'chown' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'mkdir' r=0
init: command 'mkdir' r=0
init: command 'chown' r=0
init: command 'chmod' r=-2
init: command 'chown' r=-2
init: command 'write' r=-2
init: command 'write' r=0
init: property (null) has no value for writing to /sys/class/android_usb/android0/iManufacturer
init: command 'write' r=-22
init: property (null) has no value for writing to /sys/class/android_usb/android0/iProduct
init: command 'write' r=-22
init: command 'write' r=0
init: command 'mount' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: cannot find '/system/bin/sh', disabling 'console'
init: cannot find '/system/bin/servicemanager', disabling 'servicemanager'
init: cannot find '/system/bin/vold', disabling 'vold'
init: cannot find '/system/bin/gpu_init.sh', disabling 'gpu_init'
init: command 'class_start' r=0
init: cannot find '/system/bin/netd', disabling 'netd'
init: cannot find '/system/bin/dispd', disabling 'dispd'
init: cannot find '/system/bin/debuggerd', disabling 'debuggerd'
init: cannot find '/system/bin/surfaceflinger', disabling 'surfaceflinger'
init: cannot find '/system/bin/app_process', disabling 'zygote'
init: cannot find '/system/bin/drmserver', disabling 'drm'
init: cannot find '/system/bin/mediaserver', disabling 'media'
init: cannot find '/system/bin/dbus-daemon', disabling 'dbus'
init: cannot find '/system/bin/installd', disabling 'installd'
init: cannot find '/system/etc/install-recovery.sh', disabling 'flash_recovery'
init: cannot find '/system/bin/keystore', disabling 'keystore'
init: cannot find '/system/bin/rild', disabling 'ril-daemon'
init: command 'class_start' r=0
init: processing action 0x313b8 (boot)
init: command 'symlink' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'setprop' r=0
init: command 'chown' r=0
init: command 'chown' r=0
init: command 'chown' r=-2
init: command 'chown' r=-2
init: command 'chown' r=0
init: command 'chmod' r=0
init: command 'chmod' r=0
init: command 'chmod' r=0
init: command 'chmod' r=-2
init: command 'chmod' r=-2
init: command 'chmod' r=0
init: command 'chown' r=0
init: command 'chmod' r=0
init: command 'chown' r=0
init: command 'chmod' r=0
init: command 'chown' r=0
init: command 'chown' r=0
init: command 'chmod' r=0
init: command 'chown' r=0
init: command 'chmod' r=0
init: command 'chown' r=0
init: command 'chmod' r=0
init: command 'chown' r=0
init: command 'chmod' r=0
init: command 'chown' r=0
init: command 'chmod' r=0
init: command 'chown' r=-2
init: command 'chmod' r=-2
init: command 'chown' r=-2
init: command 'chmod' r=-2
init: command 'setprop' r=0
init: command 'chown' r=0
init: command 'chmod' r=0
init: command 'chmod' r=0
init: command 'chmod' r=0
init: command 'write' r=0
init: command 'write' r=0
init: command 'write' r=0
init: command 'write' r=0
init: command 'write' r=0
init: command 'write' r=0
init: command 'chmod' r=0
init: command 'chmod' r=0
init: command 'chmod' r=0
init: command 'chmod' r=0
init: command 'chmod' r=0
init: command 'chmod' r=0
init: command 'mkdir' r=-2
init: command 'chmod' r=-2
init: command 'chmod' r=-2
init: command 'chown' r=-2
init: command 'mkdir' r=0
init: command 'mkdir' r=0
init: command 'chmod' r=0
init: command 'chmod' r=-2
init: command 'chown' r=0
init: command 'chown' r=-2
init: command 'setprop' r=0
init: processing action 0x32510 (queue_propety_triggers)
init: command 'queue_propety_triggers' r=0
init: processing action 0x2d120 (property:persist.sys.usb.config=*)
init: command 'setprop' r=0
init: processing action 0x2d3f0 (property:ro.debuggable=1)
init: cannot find '/system/bin/sh', disabling 'console'
init: command 'start' r=0
init: starting 'adbd'
init: command 'start' r=0
adb_open
init: processing action 0x31018 (property:sys.usb.config=mtp,adb)
android_usb: already disabled
init: command 'write' r=0
init: command 'write' r=0
init: command 'write' r=0
init: command 'write' r=0
mtp_bind_config
adb_bind_config
init: command 'write' r=0
init: command 'start' r=0
init: command 'setprop' r=0
android_work: sent uevent USB_STATE=DISCONNECTED
android_work: sent uevent USB_STATE=CONNECTED
android_usb gadget: high speed config #1: android
android_work: sent uevent USB_STATE=CONFIGURED
解決済! 解決策の投稿を見る。
Had to change vold.fstab file to mount the correct sd card device
this line:
dev_mount sdcard /mnt/sdcard 4 /devices/platform/sdhci-esdhc-imx.0/mmc_host/mmc1
where sdhci-esdhc-imx.x is the sd card platform device number
Also, if I adb shell, I get this:
- exec '/system/bin/sh' failed: No such file or directory (2) -
and
adb ls /system gives this:
000041ed 00000000 53b0e158 .
000041fd 00000000 00000001 ..
Had to change vold.fstab file to mount the correct sd card device
this line:
dev_mount sdcard /mnt/sdcard 4 /devices/platform/sdhci-esdhc-imx.0/mmc_host/mmc1
where sdhci-esdhc-imx.x is the sd card platform device number