pca953x 2-0032: failed writing register

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

pca953x 2-0032: failed writing register

6,574 Views
controlx
Contributor I

i tried to build a new image via Yocto. i build base-core-image with iproute2, i2c-tools, libsocketcan and canutils included (same with fsl-image-gui). On Start-Up there is always a failure "pca953x 2-0032: failed writing register". But on the schematic of Sabre AI i can't see any pca953x Controller. The i2c Portexpanders are max7310!

Same failure comes up if i type "ip link set can0 up type can bitrate 125000"

In my opinion it seems like that the Controller will write to a Portexpander but there is an other configurated?!

BB_VERSION = "1.20.0"

BUILD_SYS = "x86:64-linux"

NATIVELSBSTRING = "Ubuntu-14.04"

TARGET_SYS = "arm-poky-linux-gnueabi'

MACHINE = "imx6qsareauto"

DISTRO = "poky"

DISTRO_VERSION = "1.5.3"

I've seen this failure too on posts in the Forum but there were no Solution for it!

Hope anyone can help me

U-Boot 2013.10 (Oct 08 2014 - 16:40:45)

CPU:   Freescale i.MX6Q rev1.2 at 792 MHz

Reset cause: POR

Board: MX6Q-Sabreauto revA

DRAM:  2 GiB

MMC:   FSL_SDHC: 0

*** Warning - bad CRC, using default environment

In:    serial

Out:   serial

Err:   serial

Net:   FEC [PRIME]

Hit any key to stop autoboot:  0                                               

mmc0 is current device                                                         

reading boot.scr                                                               

** Unable to read file boot.scr **                                             

reading uImage                                                                 

4042576 bytes read in 190 ms (20.3 MiB/s)                                      

Booting from mmc ...                                                           

reading imx6q-sabreauto.dtb                                                    

** Unable to read file imx6q-sabreauto.dtb **                                  

## Booting kernel from Legacy Image at 12000000 ...                            

   Image Name:   Linux-3.0.35-4.1.0+yocto+gbdde70                              

   Image Type:   ARM Linux Kernel Image (uncompressed)                         

   Data Size:    4042512 Bytes = 3.9 MiB                                       

   Load Address: 10008000                                                      

   Entry Point:  10008000                                                      

   Verifying Checksum ... OK                                                   

   Loading Kernel Image ... OK                                                 

                                                                               

Starting kernel ...                                                            

                                                                               

Uncompressing Linux... done, booting the kernel.                               

Linux version 3.0.35-4.1.0+yocto+gbdde708 (udcu@udcu-laptop) (gcc version 4.8.14

CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d               

CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache              

Machine: Freescale i.MX 6Quad/DualLite/Solo Sabre Auto Board                   

Memory policy: ECC disabled, Data cache writealloc                             

CPU identified as i.MX6Q, silicon rev 1.2                                      

PERCPU: Embedded 7 pages/cpu @8c80e000 s5792 r8192 d14688 u32768               

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 487424    

Kernel command line: console=ttymxc3,115200 root=/dev/mmcblk0p2 rootwait rw    

PID hash table entries: 4096 (order: 2, 16384 bytes)                           

Dentry cache hash table entries: 262144 (order: 8, 1048576 bytes)              

Inode-cache hash table entries: 131072 (order: 7, 524288 bytes)                

Memory: 1664MB 256MB = 1920MB total                                            

Memory: 1935728k/1935728k available, 161424k reserved, 262144K highmem         

Virtual kernel memory layout:                                                  

    vector  : 0xffff0000 - 0xffff1000   (   4 kB)                              

    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)                              

    DMA     : 0xf4600000 - 0xffe00000   ( 184 MB)                              

    vmalloc : 0xea800000 - 0xf2000000   ( 120 MB)                              

    lowmem  : 0x80000000 - 0xea000000   (1696 MB)                              

    pkmap   : 0x7fe00000 - 0x80000000   (   2 MB)                              

    modules : 0x7f000000 - 0x7fe00000   (  14 MB)                              

      .init : 0x80008000 - 0x8003e000   ( 216 kB)                              

      .text : 0x8003e000 - 0x80b0e5b8   (11074 kB)                             

      .data : 0x80b10000 - 0x80b7c1f0   ( 433 kB)                              

       .bss : 0x80b7c214 - 0x80bf0690   ( 466 kB)                              

SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=4, Nodes=1        

Preemptible hierarchical RCU implementation.                                   

NR_IRQS:624                                                                    

MXC GPIO hardware                                                              

sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms       

arm_max_freq=1GHz                                                              

MXC_Early serial console at MMIO 0x21f0000 (options '115200')                  

bootconsole [ttymxc3] enabled                                                  

Console: colour dummy device 80x30                                             

Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)                       

pid_max: default: 32768 minimum: 301                                           

Mount-cache hash table entries: 512                                            

CPU: Testing write buffer coherency: ok                                        

hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available   

CPU1: Booted secondary processor                                               

CPU2: Booted secondary processor                                               

CPU3: Booted secondary processor                                               

Brought up 4 CPUs                                                              

SMP: Total of 4 processors activated (6324.22 BogoMIPS).                       

devtmpfs: initialized                                                          

print_constraints: dummy:                                                      

NET: Registered protocol family 16                                             

print_constraints: vddpu: 725 <--> 1300 mV at 1150 mV fast normal              

print_constraints: vddcore: 725 <--> 1300 mV1150 mV fast normal                

print_constraints: vddsoc: 725 <--> 1300 mV at 1200 mV fast normal             

print_constraints: vdd2p5: 2000 <--> 2775 mV at 2400 mV fast normal            

print_constraints: vdd1p1: 800 <--> 1400 mV at 1100 mV fast normal             

print_constraints: vdd3p0: 2625 <--> 3400 mV at 3000 mV fast normal            

hw-breakpoint: found 6 breakpoint and 1 watchpoint registers.                  

hw-breakpoint: 1 breakpoint(s) reserved for watchpoint single-step.            

hw-breakpoint: maximum watchpoint size is 4 bytes.                             

L310 cache controller enabled                                                  

l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x02070000, Cache size: 1048576 B 

bio: create slab <bio-0> at 0                                                  

mxs-dma mxs-dma-apbh: initialized                                              

print_constraints: VA: 2800 mV                                                 

print_constraints: VD: 2800 mV                                                 

print_constraints: VLS: 2800 mV                                                

print_constraints: VLC: 2800 mV                                                

print_constraints: vmmc: 3300 mV                                               

SCSI subsystem initialized                                                     

spi_imx imx6q-ecspi.0: probed                                                  

usbcore: registered new interface driver usbfs                                 

usbcore: registered new interface driver hub                                   

usbcore: registered new device driver usb                                      

Freescale USB OTG Driver loaded, $Revision: 1.55 $                             

mc_pfuze 1-0008: ID: 0,Full lay: 1 ,Metal lay: 2                               

mc_pfuze 1-0008: FAB: 0 ,FIN: 0                                                

print_constraints: SW1A: 300 <--> 1875 mV at 1375 mV                           

print_constraints: SW1B: 300 <--> 1875 mV at 300 mV                            

print_constraints: SW1C: 300 <--> 1875 mV at 1375 mV                           

print_constraints: SW2: 800 <--> 3950 mV at 3000 mV                            

print_constraints: SW3A: 400 <--> 1975 mV at 1500 mV                           

print_constraints: SW3B: 400 <--> 1975 mV at 1500 mV                           

print_constraints: SW4: 800 <--> 3950 mV at 3300 mV                            

print_constraints: SWBST: 5000 <--> 5150 mV at 5000 mV                         

print_constraints: VSNVS: 1200 <--> 3000 mV at 1800 mV                         

print_constraints: VREFDDR: at 750 mV                                          

print_constraints: VGEN1: 800 <--> 1550 mV at 800 mV                           

print_constraints: VGEN2: 800 <--> 1550 mV at 1500 mV                          

print_constraints: VGEN3: 1800 <--> 3300 mV at 1800 mV                         

print_constraints: VGEN4: 1800 <--> 3300 mV at 1800 mV                         

print_constraints: VGEN5: 1800 <--> 3300 mV at 2500 mV                         

print_constraints: VGEN6: 1800 <--> 3300 mV at 2800 mV                         

pca953x 2-0030: failed reading register                                        

pca953x 2-0030: failed writing register                                        

pca953x 2-0030: failed writing register                                        

pca953x 2-0030: failed writing register                                        

pca953x 2-0030: failed writing register                                        

pca953x 2-0030: failed writing register                                        

pca953x 2-0030: failed writing register                                        

pca953x 2-0030: failed writing register                                        

pca953x 2-0030: failed writing register                                        

pca953x 2-0032: failed reading register                                        

pca953x 2-0032: failed writing register                                        

pca953x 2-0032: failed writing register                                        

pca953x 2-0032: failed writing register                                        

pca953x 2-0032: failed writing register                                        

pca953x 2-0032: failed writing register                                        

pca953x 2-0032: failed writing register                                        

pca953x 2-0032: failed writing register                                        

pca953x 2-0032: failed writing register                                        

pca953x 2-0034: failed reading register                                        

pca953x 2-0034: failed writing register                                        

pca953x 2-0034: failed writing register                                        

pca953x 2-0034: failed writing register                                        

pca953x 2-0034: failed writing register                                        

pca953x 2-0034: failed writing register                                        

pca953x 2-0034: failed writing register                                        

pca953x 2-0034: failed writing register                                        

pca953x 2-0034: failed writing register                                        

imx-ipuv3 imx-ipuv3.0: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)          

imx-ipuv3 imx-ipuv3.1: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)          

mxc_mipi_csi2 mxc_mipi_csi2: i.MX MIPI CSI2 driver probed                      

mxc_mipi_csi2 mxc_mipi_csi2: i.MX MIPI CSI2 dphy version is 0x3130302a         

MIPI CSI2 driver module loaded                                                 

Advanced Linux Sound Architecture Driver Version 1.0.24.                       

Bluetooth: Core ver 2.16                                                       

NET: Registered protocol family 31                                             

Bluetooth: HCI device and connection manager initialized                       

Bluetooth: HCI socket layer initialized                                        

Bluetooth: L2CAP socket layer initialized                                      

Bluetooth: SCO socket layer initialized                                        

cfg80211: Calling CRDA to update world regulatory domain                       

i2c-core: driver [max17135] using legacy suspend method                        

i2c-core: driver [max17135] using legacy resume method                         

Switching to clocksource mxc_timer1                                            

NET: Registered protocol family 2                                              

IP route cache hash table entries: 65536 (order: 6, 262144 bytes)              

TCP established hash table entries: 262144 (order: 9, 2097152 bytes)           

TCP bind hash table entries: 65536 (order: 7, 786432 bytes)                    

TCP: Hash tables configured (established 262144 bind 65536)                    

TCP reno registered                                                            

UDP hash table entries: 1024 (order: 3, 32768 bytes)                           

UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes)                      

NET: Registered protocol family 1                                              

RPC: Registered named UNIX socket transport module.                            

RPC: Registered udp transport module.                                          

RPC: Registered tcp transport module.                                          

RPC: Registered tcp NFSv4.1 backchannel transport module.                      

Static Power Management for Freescale i.MX6                                    

wait mode is enabled for i.MX6                                                 

cpaddr = ea880000 suspend_iram_base=ea8fc000                                   

PM driver module loaded                                                        

IMX usb wakeup probe                                                           

add wake up source irq 75                                                      

IMX usb wakeup probe                                                           

cpu regulator mode:ldo_enable                                                  

i.MXC CPU frequency driver                                                     

highmem bounce pool size: 64 pages                                             

JFFS2 version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.                           

msgmni has been set to 3268                                                    

alg: No test for stdrng (krng)                                                 

io scheduler noop registered                                                   

io scheduler deadline registered                                               

io scheduler cfq registered (default)                                          

mxc_mipi_dsi mxc_mipi_dsi: i.MX MIPI DSI driver probed                         

MIPI DSI driver module loaded                                                  

mxc_sdc_fb mxc_sdc_fb.0: register mxc display driver ldb                       

_regulator_get: get() with no identifier                                       

imx-ipuv3 imx-ipuv3.1: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)   

Console: switching to colour frame buffer device 128x48                        

mxc_sdc_fb mxc_sdc_fb.1: register mxc display driver ldb                       

mxc_sdc_fb mxc_sdc_fb.2: register mxc display driver lcd                       

imx-sdma imx-sdma: loaded firmware 1.1                                         

imx-sdma imx-sdma: initialized                                                 

Serial: IMX driver                                                             

imx-uart.1: ttymxc1 at MMIO 0x21e8000 (irq = 59) is a IMX                      

imx-uart.2: ttymxc2 at MMIO 0x21ec000 (irq = 60) is a IMX                      

imx-uart.3: ttymxc3 at MMIO 0x21f0000 (irq = 61) is a IMX                      

console [ttymxc3] enabled, bootconsole disabled                                

console [ttymxc3] enabled, bootconsole disabled                                

loop: module loaded                                                            

No sata disk.                                                                  

No NAND device found.                                                          

Chip scan failed                                                               

GPMI NAND driver registered. (IMX)                                             

vcan: Virtual CAN interface driver                                             

CAN device driver interface                                                    

flexcan netdevice driver                                                       

flexcan imx6q-flexcan.1: device registered (reg_base=ea9b8000, irq=143)        

FEC Ethernet Driver                                                            

fec_enet_mii_bus: probed                                                       

ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver                     

fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller                    

fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1             

fsl-ehci fsl-ehci.0: irq 75, io base 0x02184000                                

fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00                                

hub 1-0:1.0: USB hub found                                                     

hub 1-0:1.0: 1 port detected                                                   

add wake up source irq 72                                                      

pca953x 2-0032: failed writing register                                        

fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller                    

fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 2             

fsl-ehci fsl-ehci.1: irq 72, io base 0x02184200                                

fsl-ehci fsl-ehci.1: USB 2.0 started, EHCI 1.00                                

hub 2-0:1.0: USB hub found                                                     

hub 2-0:1.0: 1 port detected                                                   

Initializing USB Mass Storage driver...                                        

usbcore: registered new interface driver usb-storage                           

USB Mass Storage support registered.                                           

ARC USBOTG Device Controller driver (1 August 2005)                            

mousedev: PS/2 mouse device common for all mice                                

input: gpio-keys as /devices/platform/gpio-keys/input/input0                   

egalax_ts 1-0004: egalax_ts: failed to read firmware version                   

egalax_ts: probe of 1-0004 failed with error -5                                

i2c-core: driver [isl29023] using legacy suspend method                        

i2c-core: driver [isl29023] using legacy resume method                         

snvs_rtc snvs_rtc.0: rtc core: registered snvs_rtc as rtc0                     

i2c /dev entries driver                                                        

Linux video capture interface: v2.00                                           

mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video16           

mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video17           

mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video18           

mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video19           

mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video20           

mag3110 2-000e: check mag3110 chip ID                                          

mag3110 2-000e: read chip ID 0xfffffffb is not equal to 0xc4!                  

mag3110: probe of 2-000e failed with error -22                                 

i2c-core: driver [mag3110] using legacy suspend method                         

i2c-core: driver [mag3110] using legacy resume method                          

mma8451 2-001c: read chip ID 0x1 is not equal to 0x1a or 0x2a!                 

mma8451: probe of 2-001c failed with error -22                                 

imx2-wdt imx2-wdt.0: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=1)    

Bluetooth: Virtual HCI driver ver 1.3                                          

Bluetooth: HCI UART driver ver 2.2                                             

Bluetooth: HCIATH3K protocol initialized                                       

Bluetooth: Generic Bluetooth USB driver ver 0.6                                

usbcore: registered new interface driver btusb                                 

sdhci: Secure Digital Host Controller Interface driver                         

sdhci: Copyright(c) Pierre Ossman                                              

mmc0: SDHCI controller on platform [sdhci-esdhc-imx.2] using DMA               

mmc1: no vmmc regulator found                                                  

mmc1: SDHCI controller on platform [sdhci-esdhc-imx.0] using DMA               

mxc_vdoa mxc_vdoa: i.MX Video Data Order Adapter(VDOA) driver probed           

VPU initialized                                                                

mxc_asrc registered                                                            

Galcore version 4.6.9.6622                                                     

Thermal calibration data is 0x5a05027d                                         

Thermal sensor with ratio = 187                                                

Anatop Thermal registered as thermal_zone0                                     

anatop_thermal_probe: default cooling device is cpufreq!                       

mmc0: new high speed SDHC card at address 0007                                 

mmcblk0: mmc0:0007 SD4GB 3.67 GiB                                              

mmcblk0: p1 p2                                                                

caam caam.0: device ID = 0x0a16010000000000                                    

caam caam.0: job rings = 2, qi = 0                                             

alg: No test for authenc(hmac(md5),cbc(aes)) (authenc-hmac-md5-cbc-aes-caam)   

caam caam.0: authenc-hmac-md5-cbc-aes-caam                                     

alg: No test for authenc(hmac(sha1),cbc(aes)) (authenc-hmac-sha1-cbc-aes-caam) 

caam caam.0: authenc-hmac-sha1-cbc-aes-caam                                    

alg: No test for authenc(hmac(sha224),cbc(aes)) (authenc-hmac-sha224-cbc-aes-ca)

caam caam.0: authenc-hmac-sha224-cbc-aes-caam                                  

alg: No test for authenc(hmac(sha256),cbc(aes)) (authenc-hmac-sha256-cbc-aes-ca)

caam caam.0: authenc-hmac-sha256-cbc-aes-caam                                  

alg: No test for authenc(hmac(md5),cbc(des3_ede)) (authenc-hmac-md5-cbc-des3_ed)

caam caam.0: authenc-hmac-md5-cbc-des3_ede-caam                                

alg: No test for authenc(hmac(sha1),cbc(des3_ede)) (authenc-hmac-sha1-cbc-des3_)

caam caam.0: authenc-hmac-sha1-cbc-des3_ede-caam                               

alg: No test for authenc(hmac(sha224),cbc(des3_ede)) (authenc-hmac-sha224-cbc-d)

caam caam.0: authenc-hmac-sha224-cbc-des3_ede-caam                             

alg: No test for authenc(hmac(sha256),cbc(des3_ede)) (authenc-hmac-sha256-cbc-d)

caam caam.0: authenc-hmac-sha256-cbc-des3_ede-caam                             

alg: No test for authenc(hmac(md5),cbc(des)) (authenc-hmac-md5-cbc-des-caam)   

caam caam.0: authenc-hmac-md5-cbc-des-caam                                     

alg: No test for authenc(hmac(sha1),cbc(des)) (authenc-hmac-sha1-cbc-des-caam) 

caam caam.0: authenc-hmac-sha1-cbc-des-caam                                    

alg: No test for authenc(hmac(sha224),cbc(des)) (authenc-hmac-sha224-cbc-des-ca)

caam caam.0: authenc-hmac-sha224-cbc-des-caam                                  

alg: No test for authenc(hmac(sha256),cbc(des)) (authenc-hmac-sha256-cbc-des-ca)

caam caam.0: authenc-hmac-sha256-cbc-des-caam                                  

caam caam.0: cbc-aes-caam                                                      

caam caam.0: ecb-aes-caam                                                      

caam caam.0: cbc-3des-caam                                                     

caam caam.0: cbc-des-caam                                                      

platform caam_jr.0: registering rng-caam                                       

platform caam_sm.0: caam_sm_test: 8-byte key test match OK                     

platform caam_sm.0: caam_sm_test: 16-byte key test match OK                    

platform caam_sm.0: caam_sm_test: 32-byte key test match OK                    

platform caam_secvio.0: security violation service handlers armed              

usbcore: registered new interface driver usbhid                                

usbhid: USB HID core driver                                                    

usbcore: registered new interface driver snd-usb-audio                         

mxc_hdmi_soc mxc_hdmi_soc.0: MXC HDMI Audio                                    

mxc_spdif mxc_spdif.0: MXC SPDIF Audio                                         

Cirrus Logic CS42888 ALSA SoC Codec Driver                                     

cs42888 1-0048: found device at i2c address 48                                 

cs42888 1-0048: hardware revision 4                                            

i2c-core: driver [cs42888] using legacy suspend method                         

i2c-core: driver [cs42888] using legacy resume method                          

imx-hdmi-soc-dai imx-hdmi-soc-dai.0: Failed: Load HDMI-video first.            

imx_3stack asoc driver                                                         

asoc: CS42888 <-> imx-esai.0 mapping ok                                        

asoc: CS42888_ASRC <-> imx-esai.0 mapping ok                                   

asoc: mxc-spdif <-> imx-spdif-dai.0 mapping ok                                 

Initialize HDMI-audio failed. Load HDMI-video first!                           

ALSA device list:                                                              

  #0: cs42888-audio                                                            

  #1: imx-spdif                                                                

NET: Registered protocol family 26                                             

TCP cubic registered                                                           

NET: Registered protocol family 17                                             

can: controller area network core (rev 20090105 abi 8)                         

NET: Registered protocol family 29                                             

can: raw protocol (rev 20090105)                                               

can: broadcast manager protocol (rev 20090105 t)                               

Bluetooth: RFCOMM TTY layer initialized                                        

Bluetooth: RFCOMM socket layer initialized                                     

Bluetooth: RFCOMM ver 1.11                                                     

Bluetooth: BNEP (Ethernet Emulation) ver 1.3                                   

Bluetooth: BNEP filters: protocol multicast                                    

Bluetooth: HIDP (Human Interface Emulation) ver 1.2                            

lib80211: common routines for IEEE802.11 drivers                               

VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4        

Bus freq driver module loaded                                                  

Bus freq driver Enabled                                                        

mxc_dvfs_core_probe                                                            

DVFS driver module loaded                                                      

regulator_init_complete: VGEN6: incomplete constraints, leaving on             

regulator_init_complete: VGEN5: incomplete constraints, leaving on             

regulator_init_complete: VGEN4: incomplete constraints, leaving on             

regulator_init_complete: VGEN2: incomplete constraints, leaving on             

snvs_rtc snvs_rtc.0: setting system clock to 1970-01-01 00:00:00 UTC (0)       

EXT3-fs: barriers not enabled                                                  

kjournald starting.  Commit interval 5 seconds                                 

EXT3-fs (mmcblk0p2): using internal journal                                    

EXT3-fs (mmcblk0p2): recovery complete                                         

EXT3-fs (mmcblk0p2): mounted filesystem with writeback data mode               

VFS: Mounted root (ext3 filesystem) on device 179:2.                           

devtmpfs: mounted                                                              

Freeing init memory: 216K                                                      

INIT: version 2.88 booting                                                     

Starting udev                                                                  

udevd[119]: starting version 182                                               

DBG sensor data is at 7f001cb0                                                 

pca953x 2-0032: failed writing register                                        

                                                                               

udevadm settle - timeout of 3 seconds reached, the event queue contains:       

  /sys/devices/platform/sdhci-esdhc-imx.2/mmc_host/mmc0/mmc0:0007/block/mmcblk0)

  /sys/devices/platform/sdhci-esdhc-imx.2/mmc_host/mmc0/mmc0:0007/block/mmcblk0)

  /sys/devices/platform/sdhci-esdhc-imx.2/mmc_host/mmc0/mmc0:0007/block/mmcblk0)

  /sys/devices/platform/soc-audio.2/sound/card0/controlC0 (1519)               

  /sys/devices/platform/soc-audio.3/sound/card1/controlC1 (1522)               

  /sys/devices/virtual/block/loop0 (1538)                                      

  /sys/devices/virtual/block/loop1 (1539)                                      

  /sys/devices/virtual/block/loop2 (1540)                                      

  /sys/devices/virtual/block/loop3 (1541)                                      

  /sys/devices/virtual/block/loop4 (1542)                                      

  /sys/devices/virtual/block/loop5 (1543)                                      

  /sys/devices/virtual/block/loop6 (1544)                                      

  /sys/devices/virtual/block/loop7 (1545)                                      

  /sys/devices/platform/soc-audio.2/sound/card0 (1566)                         

  /sys/devices/platform/soc-audio.3/sound/card1 (1567)                         

Starting Bootlog daemon: bootlogd.                                             

ALSA: Restoring mixer settings...                                              

No state is present for card cs42888audio                                      

Found hardware: "cs42888-audio" "" "" "" ""                                    

Hardware is initialized using a generic method                                 

No state is present for card cs42888audio                                      

No state is present for card imxspdif                                          

Found hardware: "imx-spdif" "" "" "" ""                                        

Hardware is initialized using a generic method                                 

No state is present for card imxspdif                                          

Configuring network interfaces... eth0: Freescale FEC PHY driver [Generic PHY] )

udhcpc (v1.21.1) started                                                       

Sending discover...                                                            

Sending discover...                                                            

PHY: 1:01 - Link is Up - 1000/Full                                             

Sending discover...                                                            

No lease, failing                                                              

Starting rpcbind daemon...rpcbind: cannot create socket for udp6               

rpcbind: cannot create socket for tcp6                                         

done.                                                                          

Wed Oct  8 15:38:00 UTC 2014                                                   

INIT: Entering runlevel: 5                                                     

Starting Xserver                                                               

Starting system message bus: dbus.                                             

Starting Connection Manager                                                    

Starting Dropbear SSH server: dropbear.                                        

Starting advanced power management daemon: apmd.                               

apmd[446]: apmd 3.2.1 interfacing with apm driver 1.13 and APM BIOS 1.2        

creating NFS state directory: done                                             

NFS daemon support not enabled in kernel                                       

Starting syslogd/klogd: done                                                   

* Starting Avahi mDNS/DNS-SD Daemon: avahi-daemon                             

[drm] Initialized drm 1.1.0 20060810                                           

[drm] Initialized vivante 1.0.0 20120216 on minor 0                            

   ...done.                                                                    

Starting Telephony daemon                                                      

Starting Linux NFC daemon                                                      

Starting OProfileUI server                                                     

Running local boot scripts (/etc/rc.local).                                    

Stopping Bootlog daemon: bootlogd.                                             

                                                                               

Poky (Yocto Project Reference Distro) 1.5.3 imx6qsabreauto /dev/ttymxc3

Labels (4)
0 Kudos
Reply
3 Replies

4,151 Views
inhojeon
Contributor III

It is IC Malfuction.

Plz, purchase IC via MAXIM directly.

0 Kudos
Reply

4,151 Views
danielhaap
Contributor I

Hi,

I was also running into this issue. I am using U-Boot 2914.07-rc4 and I found a problem there. In mx6qsabreauto.c the function mx6sabre_rev() was returning the wrong revision to the Linux kernel. My board is based on Revision D which is not known by U-Boot. So U-Boot is returning Revision A per default. Try to change like:

reg = reg >> 8 & 0x0F;

switch (reg) {

    case 0x01:

   ret = BOARD_REV_A;
   break;

    case 0x02:

    default:

   ret = BOARD_REV_B;
   break;

    }

Now the Linux kernel will use PAD configuration of revision B. This helps for me.

BR,

Daniel

0 Kudos
Reply

4,151 Views
igorpadykov
NXP Employee
NXP Employee

Hi controlx

seems max7310 just uses linux gpio expander driver pca953x.

Errors may occur since it is not fully compatible with pca953x

(some registers may be absent), however one can safely ignore them.

Best regards

igor

0 Kudos
Reply