parrallel ipu handling

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

parrallel ipu handling

Jump to solution
1,252 Views
smspatrick
Contributor III

For a videofilter I use two ipu instances, both with its own handle, refering to IPUV3 Library. In OP_NORMAL_MODE it's too slow, so i set up streaming mode according to the User's Guide. Both for themself are working fine, but together they nagging around:

mxc_ipu_hl_lib.c:947 ipu is busy
mxc_ipu mxc_ipu: handler already installed on irq 0

mxc_ipu_hl_lib.c:2779 Ioctl IPU_REGISTER_GENERIC_ISR 0 failed!

So i checked the mxc_ipu_hl_lib.c and every call of mxc_ipu_lib_task_init() refers to the same irq channel.

So: How I work around that and why use handle ipu instances when they in the end are referring to the same processes?

It's urgent, so a simple and cheap solution would be appreciate.

Here are some of the inits:

...

filter->ipu1->mode = OP_STREAM_MODE;

...

init_return = mxc_ipu_lib_task_init(  filter->ipu1->input,           //input parameter

                                                           NULL,                            //overlay parameter

                                                           filter->ipu1->output,       //output parameter

                                                           filter->ipu1->mode,         //ipu mode refer to header file

                                                           filter->ipu1->handle);      //allocate for init, provide some info after task init function

for the second ipu all the same.


Labels (4)
Tags (2)
0 Kudos
1 Solution
813 Views
rogerio_silva
NXP Employee
NXP Employee

Hi Patrick,

According to the ipu_lib user guide, there are 3 time-sharing tasks in the IPU hardware; they are ENC, VF and PP. You can't process 2 same tasks at the same time (e.g. 2 ENC, 2VF or 2 PP).

You can use the gstreamer ipu color space conversion plugin (mfw_gst_ipu_csc.c) as example of ipu usage on video applications.

Rgds

Rogerio

View solution in original post

0 Kudos
2 Replies
814 Views
rogerio_silva
NXP Employee
NXP Employee

Hi Patrick,

According to the ipu_lib user guide, there are 3 time-sharing tasks in the IPU hardware; they are ENC, VF and PP. You can't process 2 same tasks at the same time (e.g. 2 ENC, 2VF or 2 PP).

You can use the gstreamer ipu color space conversion plugin (mfw_gst_ipu_csc.c) as example of ipu usage on video applications.

Rgds

Rogerio

0 Kudos
813 Views
smspatrick
Contributor III

Hi Rogerio,

the Plugin only handles one ipu-instance and even this not very well, when it won't get conformant gstreamer buffers, since then it use a memcpy on both sides.

The soultion is the triplet of [ 1. task_init() 2. task_update()  3.task_uninit() ] two times in a parallel process, so that the interrupt works on that process and use a flag or semaphore for the main-thread to see when its done. This works very well.

0 Kudos