For a videofilter I use two ipu instances, both with its own handle, refering to IPUV3 Library. In OP_NORMAL_MODE it's too slow, so i set up streaming mode according to the User's Guide. Both for themself are working fine, but together they nagging around:
mxc_ipu_hl_lib.c:947 ipu is busy
mxc_ipu mxc_ipu: handler already installed on irq 0
mxc_ipu_hl_lib.c:2779 Ioctl IPU_REGISTER_GENERIC_ISR 0 failed!
So i checked the mxc_ipu_hl_lib.c and every call of mxc_ipu_lib_task_init() refers to the same irq channel.
So: How I work around that and why use handle ipu instances when they in the end are referring to the same processes?
It's urgent, so a simple and cheap solution would be appreciate.
Here are some of the inits:
...
filter->ipu1->mode = OP_STREAM_MODE;
...
init_return = mxc_ipu_lib_task_init( filter->ipu1->input, //input parameter
NULL, //overlay parameter
filter->ipu1->output, //output parameter
filter->ipu1->mode, //ipu mode refer to header file
filter->ipu1->handle); //allocate for init, provide some info after task init function
for the second ipu all the same.
Solved! Go to Solution.
Hi Patrick,
According to the ipu_lib user guide, there are 3 time-sharing tasks in the IPU hardware; they are ENC, VF and PP. You can't process 2 same tasks at the same time (e.g. 2 ENC, 2VF or 2 PP).
You can use the gstreamer ipu color space conversion plugin (mfw_gst_ipu_csc.c) as example of ipu usage on video applications.
Rgds
Rogerio
Hi Patrick,
According to the ipu_lib user guide, there are 3 time-sharing tasks in the IPU hardware; they are ENC, VF and PP. You can't process 2 same tasks at the same time (e.g. 2 ENC, 2VF or 2 PP).
You can use the gstreamer ipu color space conversion plugin (mfw_gst_ipu_csc.c) as example of ipu usage on video applications.
Rgds
Rogerio
Hi Rogerio,
the Plugin only handles one ipu-instance and even this not very well, when it won't get conformant gstreamer buffers, since then it use a memcpy on both sides.
The soultion is the triplet of [ 1. task_init() 2. task_update() 3.task_uninit() ] two times in a parallel process, so that the interrupt works on that process and use a flag or semaphore for the main-thread to see when its done. This works very well.