pads in i.MX8 QM MEK board dont work as expected

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

pads in i.MX8 QM MEK board dont work as expected

939 Views
nxf40256
NXP Employee
NXP Employee

I encountered some problems when using some pads in IMX8QM MEK board as below:

#define SC_P_USDHC2_DATA0                        238  /*!< CONN.USDHC2.DATA0, DMA.UART4.RX, LSIO.GPIO5.IO26 */

#define SC_P_USDHC2_DATA1                        239  /*!< CONN.USDHC2.DATA1, DMA.UART4.TX, LSIO.GPIO5.IO27 */

#define SC_P_USDHC2_DATA2                        240  /*!< CONN.USDHC2.DATA2, DMA.UART4.CTS_B, LSIO.GPIO5.IO28 */

#define SC_P_USDHC2_DATA3                        241  /*!< CONN.USDHC2.DATA3, DMA.UART4.RTS_B, LSIO.GPIO5.IO29 */

When i configured those pads to UART mode but there is no UART signal comes out

When i tried configuring those pads to GPIO (GPIO5), i couldn't control the signal either. I did not observe the signal change when set the out put value from 0 to 1 and vice versa.

Note that our application running on M4, and those pads are assigned to M4 partition, core A35 does not run, only core M4 is running

0 Kudos
Reply
1 Reply

789 Views
art
NXP Employee
NXP Employee

Please refer to the M4 core software examples, included into the MCUXpresso SDK for the i.MX8QM MEK board. The SDK can be configured and downloaded from here:

https://mcuxpresso.nxp.com/en/select

Best Regards,
Artur

0 Kudos
Reply