Hi all,
I am trying to connect ov5642 camera to i.MX6Q-based custom board (3.14.28 kernel).
I successfully boot kernel with camera ov5642 is found message,
but when I try gst-launch-1.0 imxv4l2videosrc device=/dev/video0 ! imxipuvideotransform ! imxipuvideosink I get:
Setting pipeline to PAUSED ...
Pipeline is live and does not need PREROLL ...
Setting pipeline to PLAYING ...
New clock: GstSystemClock
ERROR: from element /GstPipeline:pipeline0/GstImxV4l2VideoSrc:imxv4l2videosrc0: Internal data flow error.
Additional debug info:
/home/i_nikolaenko/devel/freescale/fsl-community-bsp/build-rootfs/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer1.0/1.4.5-r0/gstreamer-1.4.5/libs/gst/base/gstbasesrc.c(2933): gst_base_src_loop (): /GstPipeline:pipeline0/GstImxV4l2VideoSrc:imxv4l2videosrc0:
streaming task paused, reason error (-5)
Execution ended after 0:00:10.037558668
Setting pipeline to PAUSED ...
Setting pipeline to READY ...
Setting pipeline to NULL ...
Freeing pipeline ...
GST_DEBUG=2,*imx*:9 gst-launch-1.0 imxv4l2videosrc device=/dev/video0 ! imxipuvideotransform ! imxipuvideosink shows next error message:
New clock: GstSystemClock
0:00:01.620390667 715 0xbf70f0 DEBUG imxv4l2bufferpool v4l2_buffer_pool.c:292:gst_imx_v4l2_buffer_pool_start:<imxv4l2bufferpool0> start
0:00:01.620532667 715 0xbf70f0 DEBUG imxv4l2bufferpool v4l2_buffer_pool.c:148:gst_imx_v4l2_buffer_pool_alloc_buffer:<imxv4l2bufferpool0> alloc 0 0xbff650
0:00:01.620788000 715 0xbf70f0 DEBUG imxv4l2bufferpool v4l2_buffer_pool.c:276:gst_imx_v4l2_buffer_pool_release_buffer:<imxv4l2bufferpool0> qbuf 0 0xbff650
0:00:01.620883000 715 0xbf70f0 DEBUG imxv4l2bufferpool v4l2_buffer_pool.c:148:gst_imx_v4l2_buffer_pool_alloc_buffer:<imxv4l2bufferpool0> alloc 1 0xbff6f0
0:00:01.620995000 715 0xbf70f0 DEBUG imxv4l2bufferpool v4l2_buffer_pool.c:276:gst_imx_v4l2_buffer_pool_release_buffer:<imxv4l2bufferpool0> qbuf 1 0xbff6f0
0:00:01.621070000 715 0xbf70f0 DEBUG imxv4l2bufferpool v4l2_buffer_pool.c:148:gst_imx_v4l2_buffer_pool_alloc_buffer:<imxv4l2bufferpool0> alloc 2 0x76008828
0:00:01.621168667 715 0xbf70f0 DEBUG imxv4l2bufferpool v4l2_buffer_pool.c:276:gst_imx_v4l2_buffer_pool_release_buffer:<imxv4l2bufferpool0> qbuf 2 0x76008828
0:00:01.621250000 715 0xbf70f0 DEBUG imxv4l2bufferpool v4l2_buffer_pool.c:148:gst_imx_v4l2_buffer_pool_alloc_buffer:<imxv4l2bufferpool0> alloc 3 0x760088c8
0:00:01.621362333 715 0xbf70f0 DEBUG imxv4l2bufferpool v4l2_buffer_pool.c:276:gst_imx_v4l2_buffer_pool_release_buffer:<imxv4l2bufferpool0> qbuf 3 0x760088c8
0:00:01.621439667 715 0xbf70f0 DEBUG imxv4l2bufferpool v4l2_buffer_pool.c:148:gst_imx_v4l2_buffer_pool_alloc_buffer:<imxv4l2bufferpool0> alloc 4 0x76008968
0:00:01.621540667 715 0xbf70f0 DEBUG imxv4l2bufferpool v4l2_buffer_pool.c:276:gst_imx_v4l2_buffer_pool_release_buffer:<imxv4l2bufferpool0> qbuf 4 0x76008968
0:00:01.621617333 715 0xbf70f0 DEBUG imxv4l2bufferpool v4l2_buffer_pool.c:148:gst_imx_v4l2_buffer_pool_alloc_buffer:<imxv4l2bufferpool0> alloc 5 0x76008a08
0:00:01.621723000 715 0xbf70f0 DEBUG imxv4l2bufferpool v4l2_buffer_pool.c:276:gst_imx_v4l2_buffer_pool_release_buffer:<imxv4l2bufferpool0> qbuf 5 0x76008a08
0:00:11.626324334 715 0xbf70f0 ERROR imxv4l2bufferpool v4l2_buffer_pool.c:238:gst_imx_v4l2_buffer_pool_acquire_buffer:<imxv4l2bufferpool0> VIDIOC_DQBUF failed: Timer expired
0:00:11.626649668 715 0xbf70f0 WARN basesrc gstbasesrc.c:2933:gst_base_src_loop:<imxv4l2videosrc0> error: Internal data flow error.
0:00:11.626860001 715 0xbf70f0 WARN basesrc gstbasesrc.c:2933:gst_base_src_loop:<imxv4l2videosrc0> error: streaming task paused, reason error (-5)
ERROR: from element /GstPipeline:pipeline0/GstImxV4l2VideoSrc:imxv4l2videosrc0: Internal data flow error.
Please help me to find the way to solve this problem!
Savvy blog post . Speaking of which , if your company has been searching for a a form , my family filled a sample form here Gst secure execution nxp form Fill Online, Printable, Fillable, Blank - PDFfiller
I've got both cameras working at the imx_3.10.53_1.1.1_ga kernel with the next devicetree entries:
v4l2_cap_0 {
compatible = "fsl,imx6q-v4l2-capture";
ipu_id = <0>;
csi_id = <0>;
mclk_source = <0>;
status = "okay";
};
v4l2_cap_1 {
compatible = "fsl,imx6q-v4l2-capture";
ipu_id = <0>;
csi_id = <1>;
mclk_source = <0>;
mipi_camera = <1>;
status = "okay";
};
&i2c1 {
clock-frequency = <100000>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_i2c1_2>;
status = "okay";
ov5642: ov5642@3d {
compatible = "ovti,ov5642";
reg = <0x3d>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_ipu1_2>;
clocks = <&clks 201>;
clock-names = "csi_mclk";
DOVDD-supply = <®_1p8v>;
AVDD-supply = <®_2p5v>;
DVDD-supply = <®_1p8v>;
pwn-gpios = <&gpio3 12 1>;
rst-gpios = <&gpio5 0 0>;
ipu_id = <0>;
csi_id = <0>;
mclk = <24000000>;
mclk_source = <0>;
};
ov5640_mipi: ov5640_mipi@3e {
compatible = "ovti,ov5640_mipi";
reg = <0x3e>;
clocks = <&clks 201>;
clock-names = "csi_mclk";
DOVDD-supply = <®_1p8v>;
AVDD-supply = <®_2p5v>;
DVDD-supply = <®_1p8v>;
pwn-gpios = <&gpio3 8 1>;
rst-gpios = <&gpio3 7 0>;
ipu_id = <0>;
csi_id = <1>;
mclk = <24000000>;
mclk_source = <0>;
};
};
&mipi_csi {
ipu_id = <0>;
csi_id = <1>;
v_channel = <1>;
lanes = <2>;
status = "okay";
};
But the question is why cameras don't work properly at the imx_3.14.28 kernel? Is it possible to get them both working at the same i2c bus at the 3.14.28 kernel?
Hi
Can you try following pipeline?
gst-launch imxv4l2src ! imxv4l2sink
Thanks
Saurabh
Hi Saurabh,
There is the result of gst-launch-1.0 imxv4l2src ! imxv4l2sink:
ERROR: pipeline could not be constructed: no element "imxv4l2src".
Same error for "imxv4l2sink".
There is my gst-imx plugins:
root@imx6qsabresd:~# gst-inspect-1.0 | grep imx
imxv4l2videosrc: imxv4l2videosrc: V4L2 CSI Video Source
imxvpu: imxvpudec: Freescale VPU video decoder
imxvpu: imxvpuenc_h263: Freescale VPU h.263 video encoder
imxvpu: imxvpuenc_h264: Freescale VPU h.264 video encoder
imxvpu: imxvpuenc_mpeg4: Freescale VPU MPEG-4 video encoder
imxvpu: imxvpuenc_mjpeg: Freescale VPU motion JPEG video encoder
imxpxp: imxpxpvideosink: Freescale PxP video sink
imxpxp: imxpxpvideotransform: Freescale PxP video transform
imxipu: imxipuvideotransform: Freescale IPU video transform
imxipu: imxipuvideosink: Freescale IPU video sink
imxipu: imxipucompositor: Freescale IPU video compositor
imxeglvivsink: imxeglvivsink: Freescale EGL video sink
imxg2d: imxg2dvideosink: Freescale G2D video sink
imxg2d: imxg2dvideotransform: Freescale G2D video transform
imxg2d: imxg2dcompositor: Freescale G2D video compositor
imxaudio: imxuniaudiodec: Freescale i.MX uniaudio decoder
imxaudio: imxmp3audioenc: Freescale i.MX MP3 encoder
Thanks
I've got the same error.
I did some research and came up with interesting results:
(I have both cameras at one i2c bus)
1. I have only one camera was found by the imx_3.14.28_1.0.0_ga kernel - with an i2c address of 0x3c. No matter ov5640_mipi or ov5642. But works fine only ov5640_mipi.
2. I have both cameras were found by the imx_3.10.53_1.1.1_ga kernel, but works fine only ov5642!!!
So, there is no gstreamer error, no pinmux error. The same Devicetree file in both cases.
Does anyone have this cameras working simultaneously with the 3.14.28 kernel?