optee-os-tadevkit-3.21.0.imx-r0 do_compile: oe_runmake failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

optee-os-tadevkit-3.21.0.imx-r0 do_compile: oe_runmake failed

454件の閲覧回数
RevathyR
Contributor II

Hi,

Im trying to build a imx-image-full image.With bitbake imx-image-full command I'm gettng the following error.

"ERROR: optee-os-tadevkit-3.21.0.imx-r0 do_compile: oe_runmake failed
ERROR: optee-os-tadevkit-3.21.0.imx-r0 do_compile: ExecutionError('/nxp_sdk/build/tmp/work/imx8mp_lpddr4_evk-poky-linux/optee-os-tadevkit/3.21.0.imx-r0/temp/run.do_compile.2814741', 1, None, None)
ERROR: Logfile of failure stored in: /nxp_sdk/build/tmp/work/imx8mp_lpddr4_evk-poky-linux/optee-os-tadevkit/3.21.0.imx-r0/temp/log.do_compile.2814741
ERROR: Task (/nxp_sdk/sources/meta-imx/meta-bsp/recipes-security/optee/optee-os-tadevkit_3.21.0.imx.bb:do_compile) failed with exit code '1'
ERROR: optee-os-3.21.0.imx-r0 do_compile: oe_runmake failed
ERROR: optee-os-3.21.0.imx-r0 do_compile: ExecutionError('/nxp_sdk/build/tmp/work/imx8mp_lpddr4_evk-poky-linux/optee-os/3.21.0.imx-r0/temp/run.do_compile.2815846', 1, None, None)
ERROR: Logfile of failure stored in: /nxp_sdk/build/tmp/work/imx8mp_lpddr4_evk-poky-linux/optee-os/3.21.0.imx-r0/temp/log.do_compile.2815846
ERROR: Task (/nxp_sdk/sources/meta-imx/meta-bsp/recipes-security/optee/optee-os_3.21.0.imx.bb:do_compile) failed with exit code '1'"

I have tried cleaning and rebuilding this optee-os with the following commands

  • bitbake optee-os -c cleansstate
  • bitbake optee-os -c compile


I have checked online for solutions but nothing worked.

Please help me resolve the issue at the earliest.

0 件の賞賛
返信
5 返答(返信)

422件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

Hi, 

Which BSP are you building? 

Are the host packages and Host machine as required by Yocto user guide? 

To check the log.do_compile.2814741 for more information.

 

Regards

Harvey

 

0 件の賞賛
返信

420件の閲覧回数
RevathyR
Contributor II

@Harvey021 

Yes the host packages and host machine are as required by Yocto user guide document.

In the log file also the same is given and lots of logs are generated.

0 件の賞賛
返信

414件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

What about your PC host configured? like the Cores, RAM ...etc. 

Can also have a try to restart a new build and just run bitbake optee-os, see how it is going.

 

Regards

Harvey

0 件の賞賛
返信

398件の閲覧回数
RevathyR
Contributor II

@Harvey021 

Thanks for the reply.

The system has the required RAM and cores.We run this in a server.

I have cleared the build and initiated it again.

will update once its done.

 

0 件の賞賛
返信

426件の閲覧回数
RevathyR
Contributor II

Kindly help on this issue.

0 件の賞賛
返信