Hi ,
I am using imx6 sabresd board as my development platform, using android 4.0 as my operating system. I've added some code, now my board can recognize fat32 format ssd, and can read and write properly. Now I need to used ntfs format but the code does not support.
I usd the patch(0004-ntfs_support.patch ) on HDMI Dongle Reference Design Release
adn used the folder (cp folder external/ntfs-3g) on i.MX6 OTT TVBox HW/SW Reference Design Release (ICS4.0.4_1.0.0-alpha)
but my board can not recongnize ntfs foramt ssd.
Does anyone know if this knowledge, or give me some advice. Thank you very much for any help
regards
已解决! 转到解答。
Please delete your corrent "ntfs-3g" folder and unzip a new folder here.
Please don't run "sk@ubuntu:~/myandroid/external/ntfs-3g$ ./configure " at any time, it is for Linux, not for Android, this command will modify some head files for Linux build, so it will fail to build the code in Android.
I attached the build steps again, after finished building the sabresd image, please follow them one by one, don't skip any line or add any line, thanks!
$ export ARCH=arm
$ export CROSS_COMPILE=~/myandroid/prebuilt/linux-x86/toolchain/arm-eabi-4.4.3/bin/arm-eabi-
$ cd ~/myandroid
$ source build/envsetup.sh
$ lunch sabresd_6dq-user
$ cd external/ntfs-3g
$ mm
Also attached the workable "ntfs-3g.tar.gz" here, hope there will be no more stange things happen in your side again.
when i compile all projects. it is error :
external/ntfs-3g/src/ntfs-3g.c:69:23: error: sys/xattr.h: No such file or directory
external/ntfs-3g/src/ntfs-3g.c: In function 'ntfs_fuse_getattr':
external/ntfs-3g/src/ntfs-3g.c:858: error: 'struct stat' has no member named 'st_atim'
external/ntfs-3g/src/ntfs-3g.c:859: error: 'struct stat' has no member named 'st_ctim'
external/ntfs-3g/src/ntfs-3g.c:860: error: 'struct stat' has no member named 'st_mtim'
It was answered in https://community.freescale.com/docs/DOC-94561.
To support NTFS, except the "external\ntfs-3g", "system\vold" should also be updated.
Hi li :
i know why it happen. because when i copy the ntfs-3g to /external/. i read the README.and do the follow operation according to the README.
cd external/ntfs-3g
./configure
make
cd /myandroid
make
now i had obtain the system.ing and boot.img .i will used the ntfs format ssd.and test whether it works. when i open my terminal .I put the Log on attachment.
d--------- system system 1970-01-01 00:00 sata
d---rwxr-x system sdcard_rw 1970-01-02 00:00 sdcard
this is my change :
1. | system/vold/Andrido.mk |
Fat.cpp \ |
+ Ntfs.cpp \
Loop.cpp \ |
2. | add /sys/vold/Ntfs.cpp file |
3. | add /sys/vold/Ntfs.h file |
4. | change system/vold/Volume.cpp |
5. | change device/fsl/imx6/imx6/mk |
+ | PRODUCT_PACKAGES += \ |
+ | ntfs-3g \ |
+ | ntfsfix |
6. | kerenl_imx/arch/arm/configs/imx6_android_defconfig |
+CONFIG_FUSE_FS=y
7. | add the /external/ntfs-3g file |
You had used the wrong way to build the source code, the readme file is not for Android.
In Android, you should use the followed commands:
$ export ARCH=arm
$ export CROSS_COMPILE=~/myandroid/prebuilt/linux-x86/toolchain/arm-eabi-4.4.3/bin/arm-eabi-
$ cd ~/myandroid
$ source build/envsetup.sh
$ lunch sabresd_6dq-user
$ cd external/ntfs-3g
$ mm
Hi li,
sk@ubuntu:~/myandroid/external/ntfs-3g$ mm
============================================
PLATFORM_VERSION_CODENAME=REL
PLATFORM_VERSION=4.0.4
TARGET_PRODUCT=sabresd_6dq
TARGET_BUILD_VARIANT=user
TARGET_BUILD_TYPE=release
TARGET_BUILD_APPS=
TARGET_ARCH=arm
TARGET_ARCH_VARIANT=armv7-a-neon
HOST_ARCH=x86
HOST_OS=linux
HOST_BUILD_TYPE=release
BUILD_ID=UNKNOWN
BUILD_NUMBER=eng.sk.20130626.020656
============================================
No private recovery resources for TARGET_DEVICE sabresd_6dq
make: Entering directory `/home/sk/myandroid'
make: Nothing to be done for `all_modules'.
make: Leaving directory `/home/sk/myandroid'
Hi li:
I deleted my out/target/product/sabresd_6dq directory and recompile generated sabresd_6dq/system.img file. Then I went to / external/ntfs-3g this directory, I do the command output:
sk@ubuntu:~/myandroid/external/ntfs-3g$ ./configure
sk@ubuntu:~/myandroid/external/ntfs-3g$ mm
============================================
PLATFORM_VERSION_CODENAME=REL
PLATFORM_VERSION=4.0.4
TARGET_PRODUCT=sabresd_6dq
TARGET_BUILD_VARIANT=eng
TARGET_BUILD_TYPE=release
TARGET_BUILD_APPS=
TARGET_ARCH=arm
TARGET_ARCH_VARIANT=armv7-a-neon
HOST_ARCH=x86
HOST_OS=linux
HOST_BUILD_TYPE=release
BUILD_ID=UNKNOWN
BUILD_NUMBER=eng.sk.20130627.025131
============================================
No private recovery resources for TARGET_DEVICE sabresd_6dq
make: Entering directory `/home/sk/myandroid'
target thumb C: libfuse <= external/ntfs-3g/libfuse-lite/fuse.c
In file included from external/ntfs-3g/libfuse-lite/fuse.c:9:
external/ntfs-3g/config.h:49:1: warning: "HAVE_ENDIAN_H" redefined
In file included from <command-line>:0:
./system/core/include/arch/linux-arm/AndroidConfig.h:165:1: warning: this is the location of the previous definition
external/ntfs-3g/libfuse-lite/fuse.c: In function 'fuse_lib_setattr':
external/ntfs-3g/libfuse-lite/fuse.c:1204: error: 'struct stat' has no member named 'st_atim'
external/ntfs-3g/libfuse-lite/fuse.c:1209: error: 'struct stat' has no member named 'st_mtim'
external/ntfs-3g/libfuse-lite/fuse.c:1218: error: 'struct stat' has no member named 'st_atim'
external/ntfs-3g/libfuse-lite/fuse.c:1220: error: 'struct stat' has no member named 'st_mtim'
external/ntfs-3g/libfuse-lite/fuse.c: In function 'fuse_lib_readdir':
external/ntfs-3g/libfuse-lite/fuse.c:1909: warning: comparison between signed and unsigned integer expressions
external/ntfs-3g/libfuse-lite/fuse.c: In function 'locks_insert':
external/ntfs-3g/libfuse-lite/fuse.c:2170: warning: comparison is always true due to limited range of data type
external/ntfs-3g/libfuse-lite/fuse.c: In function 'lock_to_flock':
external/ntfs-3g/libfuse-lite/fuse.c:2250: warning: comparison is always false due to limited range of data type
make: *** [out/target/product/sabresd_6dq/obj/STATIC_LIBRARIES/libfuse_intermediates/libfuse-lite/fuse.o] Error 1
make: Leaving directory `/home/sk/myandroid'
sk@ubuntu:~/myandroid/external/ntfs-3g$
Please delete your corrent "ntfs-3g" folder and unzip a new folder here.
Please don't run "sk@ubuntu:~/myandroid/external/ntfs-3g$ ./configure " at any time, it is for Linux, not for Android, this command will modify some head files for Linux build, so it will fail to build the code in Android.
I attached the build steps again, after finished building the sabresd image, please follow them one by one, don't skip any line or add any line, thanks!
$ export ARCH=arm
$ export CROSS_COMPILE=~/myandroid/prebuilt/linux-x86/toolchain/arm-eabi-4.4.3/bin/arm-eabi-
$ cd ~/myandroid
$ source build/envsetup.sh
$ lunch sabresd_6dq-user
$ cd external/ntfs-3g
$ mm
Also attached the workable "ntfs-3g.tar.gz" here, hope there will be no more stange things happen in your side again.
Hi ,
i have do it .I have compiled the Android BSP code a long time ago. it has been generated system.img
when i used the same operation on the /myandroid/external/hostapd. the same error is appear. where am i wrong?
i have compilde the android bsp code long long ago. i could found everything on the /out/target/program/sabresd/. it is ok.
please tell me the wrong.