nativesdk-qtbase-6.4.3-r0 do_compile: ExecutionError

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

nativesdk-qtbase-6.4.3-r0 do_compile: ExecutionError

1,391 Views
darsh_kapoor
Contributor I

ERROR: nativesdk-qtbase-6.4.3-r0 do_compile: ExecutionError('/home/xrda3/iMX8_bsp/iMX8m_mini_Yocto/build-xwayland-imx8mm/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-qtbase/6.4.3-r0/temp/run.do_compile.16948', 1, None, None)
ERROR: Logfile of failure stored in: /home/xrda3/iMX8_bsp/iMX8m_mini_Yocto/build-xwayland-imx8mm/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-qtbase/6.4.3-r0/temp/log.do_compile.16948

 fatal error: bits/floatn-32.h: No such file or directory
| 23 | #include <bits/floatn-32.h>
| | ^~~~~~~~~~~~~~~~~~
| compilation terminated.
| ninja: build stopped: subcommand failed.
| WARNING: exit code 1 from a shell command.
ERROR: Task (virtual:nativesdk:/home/xrda3/iMX8_bsp/iMX8m_mini_Yocto/sources/meta-qt6/recipes-qt/qt6/qtbase_git.bb:do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 3908 tasks of which 3902 didn't need to be rerun and 1 failed.

Summary: 1 task failed:
virtual:nativesdk:/home/xrda3/iMX8_bsp/iMX8m_mini_Yocto/sources/meta-qt6/recipes-qt/qt6/qtbase_git.bb:do_compile
Summary: There were 25 WARNING messages.
Summary: There was 1 ERROR message, returning a non-zero exit code.

0 Kudos
Reply
2 Replies

1,358 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @darsh_kapoor 

Please try to clean all of this package and then rebuild it.

Best Regards

Zhiming

0 Kudos
Reply

1,304 Views
darsh_kapoor
Contributor I

Thanks it worked

0 Kudos
Reply