Hi All,
I have the following two questions regarding imx7 chipsets
1) Is it possible to use mxsldr and mxsboot tools to provision a bare board with u-boot , kernel and rootfs ? Is the two tools supported for imx7 boards ?
2) Is is possible to download download u-boot, kernel and rootfs to QSPI flash devices if the mxsldr and mxsboot tools are supported for the imx7 processors.
Thanks in advance,
Sonu Abraham
Hi Sonu
unfortunately mxsldr and mxsboot tools are not suppoted by nxp,
for image programming is used mfg tool utility found on
In general yes, it is possible to download download u-boot, kernel and rootfs to QSPI flash
if its size allows for it.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------