mxc_v4l2_capture.out : capture 2592x1944 frame

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mxc_v4l2_capture.out : capture 2592x1944 frame

1,989 Views
anjojohn
Contributor IV

Hi All,

I have been trying to capture high resolution images from mx6 dualite with ov5640 mipi camera using imx-test application. Each time i try to capture images above 640x480, the image is corrupted and can't be viewed with any raw players.

I had to use mxc_v4l2_capture since Gstreamer imxv4l2videosrc plugin only support resolution upto 1920x1080. 

Below is the command i used for 640x480 capture

mxc_v4l2_capture.out -iw 640 -ih 480 -ow 640 -oh 480 -f UYVY -c 5 still.yuv

for any other higher resolution, the image is corrupted

i tried these 

mxc_v4l2_capture.out -iw 2592 -ih 1944 -ow 2592 -oh 1944 -f UYVY -c 5 -m 1 still.yuv

log of this command

in_width = 2592, in_height = 1944
out_width = 2592, out_height = 1944
top = 0, left = 0
sensor chip is ov5640_mipi_camera
sensor supported frame size:
640x480
320x240
720x480
720x576
1280x720
1920x1080
2592x1944
176x144
1024x768
sensor frame format: UYVY
sensor frame format: UYVY
sensor frame format: UYVY
sensor frame format: UYVY
sensor frame format: UYVY
sensor frame format: UYVY
sensor frame format: UYVY
sensor frame format: UYVY
sensor frame format: UYVY
Width = 2592 Height = 1944 Image size = 10077696
pixelformat: UYVY
UYVY
imx-ipuv3 2400000.ipu: IC output size(1944) cannot exceed 1024
imx-ipuv3 2400000.ipu: failed to calculate prpenc height scaling coefficients
imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x00100000
buf.index 2
buf.index 0
buf.index 1

i also tried setting the -i (input mode) to 0 and 1 and it didn't help either.

Is there any issue with mxc_v4l2_capture with higher resolution? Any help is appreciated

With Regards

John

0 Kudos
Reply
3 Replies

1,138 Views
joanxie
NXP TechSupport
NXP TechSupport

how about try to use gstreamer 1.0?

gst-inspect-1.0 imxv4l2src

   Capabilities:

     video/x-raw

                 format: YUY2

                 width: 640

                 height: 480

             framerate: { 15/1, 30/1 }

     video/x-raw

                 format: YUY2

                 width: 320

                 height: 240

             framerate: { 15/1, 30/1 }

     video/x-raw

                 format: YUY2

                 width: 720

                 height: { 576, 480 }

             framerate: { 15/1, 30/1 }

     video/x-raw

                 format: YUY2

                 width: 1280

                 height: 720

             framerate: { 15/1, 30/1 }

     video/x-raw

                 format: YUY2

                 width: 1920

                 height: 1080

             framerate: 15/1

     video/x-raw

                 format: YUY2

                 width: 2592

                 height: 1944

             framerate: 15/1

     video/x-raw

                 format: YUY2

                 width: 176

                 height: 144

             framerate: { 15/1, 30/1 }

     video/x-raw

                 format: YUY2

               width: 1024

                 height: 768

             framerate: { 15/1, 30/1 }

gst-launch-1.0 -v imxv4l2src device=/dev/video0 ! "video/x-raw, format=(string)YUY2, width=(int)2592, height=(int)1944, framerate=(fraction)15/1" ! videoconvert ! x264enc ! avimux ! filesink location=still.yuv

0 Kudos
Reply

1,138 Views
anjojohn
Contributor IV

Hi Joan,

which version of Gstreamer Freescale plugins are you using. I am using gstreamer-1.4.5. The camera source plugin in my version is "imxv4l2videosrc" and the resolutions are configured with capture-mode parameter. 

0 Kudos
Reply

1,138 Views
joanxie
NXP TechSupport
NXP TechSupport

my gstreamer is older version, no problem, you can use the mode your src plugins shows. the command is the same like I sent to you, just change the plugins refer to your gstreamer

0 Kudos
Reply