mxc_v4l2_capture driver and IPU colorspace conversion

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mxc_v4l2_capture driver and IPU colorspace conversion

ソリューションへジャンプ
660件の閲覧回数
jamiew
Contributor III

Is it possible to get the IPU to do colour space conversion using the mxc_v4l2_capture driver?

I would like to end up with a buffer containing an I420 frame given the capture device produces UYVY.

I've been looking at csc_ex1.c but it seems I would have to do some seemingly unnecessary copies.

Thanks

Jamie

ラベル(3)
タグ(3)
0 件の賞賛
1 解決策
461件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jamie

I am afraid mxc_v4l2_capture can not do colour space conversion,

so some code modifications are needed.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
1 返信
462件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jamie

I am afraid mxc_v4l2_capture can not do colour space conversion,

so some code modifications are needed.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛