Dear community,
I recently tried to create an image for a SABRE Platform board based on an existing working image. But when I tried to compile an new kernel for the image, the kernel instantly reboots when calling mxc_iomux_v3_setup_multiple_pads(mx6q_sabresd_pads,ARRAY_SIZE(mx6q_sabresd_pads)) in mx6_sabresd_board_init of file board_mx6q_sabresd.c.
Removal of the call to mxc_iomux... makes the kernel boot without further problems, but the touchpad is not working, of course.
For kernel compilation I used the package provided by freescale (L3.0.35_4.0.0_ER_SOURCE) with all the patches applied. The configuration of my kernel is based on the configuration of the working kernel, nothing was added or removed yet, so I expect it to work, which is not the case.
The working kernel is of version 3.0.35, which is the kernel I want to use.
Any help or insight is highly appreciated.
Kind regards,
Patrick
GCC Version: 4.7.3
Kernel config: see attachment
Original Attachment has been moved to: config.zip
解決済! 解決策の投稿を見る。
Do you run on FSL sabresd board? What's the board version?
If the reboot issue is caused by mxc_iomux_v3_setup_multiple_pads(), you can find out which iomux setting cause the issue by modifing the parameter in mxc_iomux_v3_setup_multiple_pads().
Do you run on FSL sabresd board? What's the board version?
If the reboot issue is caused by mxc_iomux_v3_setup_multiple_pads(), you can find out which iomux setting cause the issue by modifing the parameter in mxc_iomux_v3_setup_multiple_pads().
Thanks,
yes, it is a sabresd board, I don't know which version however.
Your method worked, just commented out some lines and get the kernel working to an acceptable degree. I am still wondering why this occurs, as the kernel versions are identical, and the configuration untouched. Could be a compiler problem, but I doubt it.