mx53 lvds and hdmi dual display

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

mx53 lvds and hdmi dual display

1,275 次查看
zhangenvi
Contributor I

all,

   lvds and hdmi dual displays, Input Parallel Display Ports is all di0. lvds and hdmi will not display together. And video of lvds is faintness. And lvds is conneted at channel 0 output lvds port. how to solve it? Thanks!

标记 (1)
0 项奖励
5 回复数

865 次查看
zhangenvi
Contributor I
u-boot boot args set HDMI,LVDS(XGA) not used.you can select one of them
0 项奖励

865 次查看
guaguann
Contributor I

In this case, connect both two displays to DI0 and share the same configuration of IPU.

 

And make sure using the same format and resolution for these two displays. MX53 supports that.  

zhang envi said:



Nan SHENG said:

I'm wondering if you want to use the parellel interface or lvds/hdmi? If you want to display dual display the inputs from lvds and hdmi, do you want to display the same content on the two displays or display independently?

 

yes,want to display the same content on the two displays,  both are connected at di0.

0 项奖励

865 次查看
zhangenvi
Contributor I


Nan SHENG said:

I'm wondering if you want to use the parellel interface or lvds/hdmi? If you want to display dual display the inputs from lvds and hdmi, do you want to display the same content on the two displays or display independently?

 

yes,want to display the same content on the two displays,  both are connected at di0.

0 项奖励

865 次查看
guaguann
Contributor I

I'm wondering if you want to use the parellel interface or lvds/hdmi? If you want to display dual display the inputs from lvds and hdmi, do you want to display the same content on the two displays or display independently?

0 项奖励

865 次查看
Yanfei_Sun
Contributor IV

you have to enable IPU di1 display and connect LVDS to it by setting the LVDS register if you want to show independent contents on the two displays.

if you just want to duplicate the content on the secondary display, it is feasible to use di0 only.

0 项奖励