Hi,
I have an ili9326 based LCD+ads7843 SPI touchscreen. I could get the touchscreen to work with
2.6.35 kernel; but not the SPI touchscreen controller. Is SPI on SSP2 working with 2.6.35 kernel,
or do I need 3.x kernel for that? I ask because 3.x doesn't have lcdif.c/h interface and I cannot figure
out how to integrate the driver I was using with 2.6.35 kernel in 3.7.
Thanks!
Thanks Otavio, will take a look at that.
@Fabio LCD interface is is supported, but only in dotclock mode right now :smileysad:
In 2.6.35, all modes are supported. I will try to stick with 2.6.35 I think.
No; SPI is broken in 2.6.35 for i.MX23. If you fix it please send us the fix :-) 2.6.31 is the last known to work from FSL kernels.
We've included the touchscreen support for i.MX28 (backported from 3.9) onto 3.8 at Freescale/linux-mainline · GitHub; you may want to give it a try.