moving console to microusb on imx6ull EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

moving console to microusb on imx6ull EVK

304 Views
asurti9
Contributor III

Hello community,

Is there a possibility of moving console (UART) to microusb port? Such that there is dual functionality on USB port?

Thanks!

Tags (3)
0 Kudos
Reply
2 Replies

255 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

i.MX 6ULL Applications Processors contains two high speed (HS) USB 2.0 OTG (Up to 480 Mbps) controllers, with two integrated HS USB Phy. On the EVK board, J1101 is a Type-A connector for USB host port, J1102 is a Micro-B connector for USB OTG port. The OTG port J1102 is also used for downloading the boot image by UUU Tool in Serial Download Mode.

0 Kudos
Reply

257 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

No, for the i.MX6ULL recommend to use the UART to debug, you can see that in our EVK we use the UART TO USB to debug easily.

0 Kudos
Reply