moving console to microusb on imx6ull EVK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

moving console to microusb on imx6ull EVK

226 次查看
asurti9
Contributor III

Hello community,

Is there a possibility of moving console (UART) to microusb port? Such that there is dual functionality on USB port?

Thanks!

标记 (3)
0 项奖励
回复
2 回复数

177 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

i.MX 6ULL Applications Processors contains two high speed (HS) USB 2.0 OTG (Up to 480 Mbps) controllers, with two integrated HS USB Phy. On the EVK board, J1101 is a Type-A connector for USB host port, J1102 is a Micro-B connector for USB OTG port. The OTG port J1102 is also used for downloading the boot image by UUU Tool in Serial Download Mode.

0 项奖励
回复

179 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

No, for the i.MX6ULL recommend to use the UART to debug, you can see that in our EVK we use the UART TO USB to debug easily.

0 项奖励
回复